<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: K64 144-pin RMII_MODE bit does not get set</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K64-144-pin-RMII-MODE-bit-does-not-get-set/m-p/679993#M41848</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Fang Li.&lt;BR /&gt;This customer board uses exact Ethernet schematic&amp;nbsp;from FRDM-K64F board. The difference is that we&amp;nbsp;used 144-pin package instead of 100-pin.&lt;BR /&gt;Here is the schematic of how we do connect PHY;&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/24937iB538263F9E265863/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;BR /&gt;And like I said, for the sample code Keil uVision 5, RMII_MODE bit does not get set, while in Freedom board everything works.&lt;BR /&gt;&lt;BR /&gt;Aleksey&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 07 Jul 2017 21:56:56 GMT</pubDate>
    <dc:creator>alekseystarovoy</dc:creator>
    <dc:date>2017-07-07T21:56:56Z</dc:date>
    <item>
      <title>K64 144-pin RMII_MODE bit does not get set</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K64-144-pin-RMII-MODE-bit-does-not-get-set/m-p/679991#M41846</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We do use MK64FX512VLQ12 MCU in our system, which is 144 pin package, and we need to have Ethernet on it.&lt;BR /&gt;We made routing based on FRDM-K64F board, i.e. we used all of the same external components on the Ethernet side, except we had to adjust pin mapping.&lt;/P&gt;&lt;P&gt;From the schematic stand point it all looks great; however, we have problem. Looks like the PHY is sending messages to the MCU, but there is no communication from MCU to the PHY. Also, RMII_MODE bit does not get set while code runnig. However, when same code is used on the FRDM board, RMII_MODE bit get set and everything works as it should. Now, my question is, do we need to do something special to have RMII_MODE bit to be set on 144 package? Because in compare to the 100 pin package here we have all MII lines available.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 01 Jul 2017 00:17:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K64-144-pin-RMII-MODE-bit-does-not-get-set/m-p/679991#M41846</guid>
      <dc:creator>alekseystarovoy</dc:creator>
      <dc:date>2017-07-01T00:17:45Z</dc:date>
    </item>
    <item>
      <title>Re: K64 144-pin RMII_MODE bit does not get set</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K64-144-pin-RMII-MODE-bit-does-not-get-set/m-p/679992#M41847</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;PRE&gt;&lt;SPAN style="font-family: arial,helvetica,sans-serif;"&gt;Please let me know if the customer board has the same &lt;/SPAN&gt;&lt;SPAN style="font-family: arial,helvetica,sans-serif;"&gt;Ethernet PHY with FRDM-K64F board? T&lt;/SPAN&gt;&lt;SPAN style="font-family: arial,helvetica,sans-serif;"&gt;he FRDM-K64F board is using RMII Ethernet
interface, the 50MHz external clock output from the KSZ8081 Ethernet PHY. And the K64 MCG is in PEE mode, the PLL reference clock is external
50MHz clock. Customer could check the EXTAL0 (PTA18) pin if there with 50MHz clock available. &lt;/SPAN&gt;&lt;PRE&gt;&lt;SPAN style="font-family: arial,helvetica,sans-serif;"&gt;As for the software config, customer should check the pin muxing register if the pins with correct function. &lt;/SPAN&gt;&lt;/PRE&gt;&lt;/PRE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Jul 2017 06:35:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K64-144-pin-RMII-MODE-bit-does-not-get-set/m-p/679992#M41847</guid>
      <dc:creator>fangli</dc:creator>
      <dc:date>2017-07-07T06:35:10Z</dc:date>
    </item>
    <item>
      <title>Re: K64 144-pin RMII_MODE bit does not get set</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K64-144-pin-RMII-MODE-bit-does-not-get-set/m-p/679993#M41848</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Fang Li.&lt;BR /&gt;This customer board uses exact Ethernet schematic&amp;nbsp;from FRDM-K64F board. The difference is that we&amp;nbsp;used 144-pin package instead of 100-pin.&lt;BR /&gt;Here is the schematic of how we do connect PHY;&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/24937iB538263F9E265863/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;BR /&gt;And like I said, for the sample code Keil uVision 5, RMII_MODE bit does not get set, while in Freedom board everything works.&lt;BR /&gt;&lt;BR /&gt;Aleksey&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Jul 2017 21:56:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K64-144-pin-RMII-MODE-bit-does-not-get-set/m-p/679993#M41848</guid>
      <dc:creator>alekseystarovoy</dc:creator>
      <dc:date>2017-07-07T21:56:56Z</dc:date>
    </item>
    <item>
      <title>Re: K64 144-pin RMII_MODE bit does not get set</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K64-144-pin-RMII-MODE-bit-does-not-get-set/m-p/679994#M41849</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;PRE class="" data-fulltext="" data-placeholder="Tradução" dir="ltr" style="color: #212121; background-color: #ffffff; border: none; font-size: 16px !important; padding: 0px 0.14em 0px 0px;"&gt;&lt;SPAN lang="en"&gt;Hello Aleksey Starovoytov. I'm having the same problem, I wonder if you can solve it?&lt;/SPAN&gt;&lt;/PRE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Oct 2017 13:31:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K64-144-pin-RMII-MODE-bit-does-not-get-set/m-p/679994#M41849</guid>
      <dc:creator>danilolima</dc:creator>
      <dc:date>2017-10-19T13:31:56Z</dc:date>
    </item>
  </channel>
</rss>