<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Flash loader S/W for TWRK20D72M in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flash-loader-S-W-for-TWRK20D72M/m-p/678154#M41760</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I expect that IAR doesn't give this tool integrated because they don't want foreign binaries to be loadable. If you have a license you can ask IAR support to be sure.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Usually your debugger manufacturer will include a binary programming utility with the tool (eg. P&amp;amp;E or Segger) and this is often the easiest to use and most reliable method.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;KDS has it built in but I never managed to get it to work (one may need a master's degree in Eclipse to get some of that stuff to operate). You could get hold of the older &lt;STRONG&gt;CodeWarrior 10 for Kinetis&lt;/STRONG&gt; since it has a nice flash utility built in that is much easier to use &lt;EM&gt;and works surprisingly well&lt;/EM&gt;. Since both CW and KDS will gradually be dumped, also look at the new MCUXpresso V10 because I expect that that will have such a tool integrated into it (unless the developer's forgot that engineers need to be able to do things like this). It is NXP's flag-ship development environment (which I haven't actually used yet) and presumably be the best maintained - at least until the next round of take-overs and strategy changes (RIP Interniche, MQX, CW7, CW10, KDS, PE, etc.....).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 12 May 2017 13:59:24 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2017-05-12T13:59:24Z</dc:date>
    <item>
      <title>Flash loader S/W for TWRK20D72M</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flash-loader-S-W-for-TWRK20D72M/m-p/678153#M41759</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am having Binary file(.bin) of one Application.I want to flash it on MCU. but in IAR , I am not finding Option for direct binary flash.Any one has Idea of Flashloader for K20 TWR EVM. I have Tried Kinetics Flashtool. But it is not Getting Connected.i want Flash utility for this board.please provide me link for same .&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 May 2017 12:05:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flash-loader-S-W-for-TWRK20D72M/m-p/678153#M41759</guid>
      <dc:creator>palakpatel</dc:creator>
      <dc:date>2017-05-12T12:05:09Z</dc:date>
    </item>
    <item>
      <title>Re: Flash loader S/W for TWRK20D72M</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flash-loader-S-W-for-TWRK20D72M/m-p/678154#M41760</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I expect that IAR doesn't give this tool integrated because they don't want foreign binaries to be loadable. If you have a license you can ask IAR support to be sure.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Usually your debugger manufacturer will include a binary programming utility with the tool (eg. P&amp;amp;E or Segger) and this is often the easiest to use and most reliable method.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;KDS has it built in but I never managed to get it to work (one may need a master's degree in Eclipse to get some of that stuff to operate). You could get hold of the older &lt;STRONG&gt;CodeWarrior 10 for Kinetis&lt;/STRONG&gt; since it has a nice flash utility built in that is much easier to use &lt;EM&gt;and works surprisingly well&lt;/EM&gt;. Since both CW and KDS will gradually be dumped, also look at the new MCUXpresso V10 because I expect that that will have such a tool integrated into it (unless the developer's forgot that engineers need to be able to do things like this). It is NXP's flag-ship development environment (which I haven't actually used yet) and presumably be the best maintained - at least until the next round of take-overs and strategy changes (RIP Interniche, MQX, CW7, CW10, KDS, PE, etc.....).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 May 2017 13:59:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flash-loader-S-W-for-TWRK20D72M/m-p/678154#M41760</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2017-05-12T13:59:24Z</dc:date>
    </item>
  </channel>
</rss>