<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 K51 as USB Device: how to NAK a USB IN</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K51-as-USB-Device-how-to-NAK-a-USB-IN/m-p/676494#M41607</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;USB 2.0 allows a Device to NAK a USB In request if it has no data to send. &amp;nbsp;This is normal. &amp;nbsp;We were using this on code that was originally developed on a TI Stellaris processor, then ported to the K51 when TI suddenly discontinued the Stellaris line.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Reviewing the K51 Sub-Family Reference Manual, I find no reference whatsoever to forcing a NAK condition. &amp;nbsp;Reviewing the USB code, I find no reference whatsoever to NAK in Device mode.&lt;BR /&gt;&lt;BR /&gt;How do I force a NAK if I have nothing to send?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 28 Jun 2017 16:40:44 GMT</pubDate>
    <dc:creator>johnstrohm</dc:creator>
    <dc:date>2017-06-28T16:40:44Z</dc:date>
    <item>
      <title>K51 as USB Device: how to NAK a USB IN</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K51-as-USB-Device-how-to-NAK-a-USB-IN/m-p/676494#M41607</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;USB 2.0 allows a Device to NAK a USB In request if it has no data to send. &amp;nbsp;This is normal. &amp;nbsp;We were using this on code that was originally developed on a TI Stellaris processor, then ported to the K51 when TI suddenly discontinued the Stellaris line.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Reviewing the K51 Sub-Family Reference Manual, I find no reference whatsoever to forcing a NAK condition. &amp;nbsp;Reviewing the USB code, I find no reference whatsoever to NAK in Device mode.&lt;BR /&gt;&lt;BR /&gt;How do I force a NAK if I have nothing to send?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Jun 2017 16:40:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K51-as-USB-Device-how-to-NAK-a-USB-IN/m-p/676494#M41607</guid>
      <dc:creator>johnstrohm</dc:creator>
      <dc:date>2017-06-28T16:40:44Z</dc:date>
    </item>
    <item>
      <title>Re: K51 as USB Device: how to NAK a USB IN</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K51-as-USB-Device-how-to-NAK-a-USB-IN/m-p/676495#M41608</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;An endpoint automatically NAKs when it has no data waiting to be sent (in its BD). Therefore there is nothing that needs to be done/forced.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Jun 2017 20:29:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K51-as-USB-Device-how-to-NAK-a-USB-IN/m-p/676495#M41608</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2017-06-28T20:29:54Z</dc:date>
    </item>
  </channel>
</rss>