<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: MKV10Z64 - VLPS - high current draw</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKV10Z64-VLPS-high-current-draw/m-p/675908#M41567</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Test the same project and same MCU with two FRDM-KV10Z boards, get different current in VLPS. &lt;BR /&gt;Compare hardware of the FRDM-KV10Z, find the J12 will lead the current leakage. After cut the trace of J12 at bottom side, the current in VLPS of my FRDM-KV10Z board down to about 40μA.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/19929i9C096899A3D79341/image-size/large?v=v2&amp;amp;px=999" title="Isolation UART SWD_DIO.png" alt="Isolation UART SWD_DIO.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Test the same project and same MCU with two FRDM-KV10Z boards but using different firmware applications for onboard OpenSDA, get different current in VLPS. &lt;BR /&gt;Compare firmware application of onboard OpenSDA, find different J-Link firmware will set different voltage to UART1_TX_TGTMCU_R. When use newest Board-Specific Firmwares'19_OpenSDA_FRDM-KV10Z.bin', the PTB17/UART0_TX current leakage occurs.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Conclusion:&lt;BR /&gt;We think it meet the 'Internal pull-up/down case' in &lt;A href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fprocessors.wiki.ti.com%2Findex.php%2FOptimizing_IO_Power_Consumption" rel="nofollow" target="_blank"&gt;Optimizing IO Power Consumption&lt;/A&gt;. Customer should avoid this.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/19968iF8D0E50B3F3D15F8/image-size/large?v=v2&amp;amp;px=999" title="Fig3_internalpullupdowncell.JPG" alt="Fig3_internalpullupdowncell.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 08 Jun 2017 00:53:06 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2017-06-08T00:53:06Z</dc:date>
    <item>
      <title>MKV10Z64 - VLPS - high current draw</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKV10Z64-VLPS-high-current-draw/m-p/675907#M41566</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Greetings. I am using the above MCU in a device I am developing. Sleep current in VLPS is ~380uA (confirmed that this is the draw of the MCU alone). Per the datasheet, it should be much much lower. I am using the functions per SDK2.2 to enter VLPS, I am seeing a drop from run time draw (~2mA) to this sleep current draw, so I know that the MCU is entering a lower power state, but I cannot achieve the numbers I expect. All un-used pins are pulled low using internal pull downs and driven low (excluding the JTAG lines - although I suppose I could add them to the list too). Any ideas about what else I should check? Is something defaulted to on (via SDK2.2 or otherwise) that I should be disabling? I believe the core clock is disabled in VLPS so no value in dropping clock speed when sleeping, correct?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help is appreciated!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Chris&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 May 2017 15:07:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKV10Z64-VLPS-high-current-draw/m-p/675907#M41566</guid>
      <dc:creator>chrisphelan</dc:creator>
      <dc:date>2017-05-11T15:07:07Z</dc:date>
    </item>
    <item>
      <title>Re: MKV10Z64 - VLPS - high current draw</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKV10Z64-VLPS-high-current-draw/m-p/675908#M41567</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Test the same project and same MCU with two FRDM-KV10Z boards, get different current in VLPS. &lt;BR /&gt;Compare hardware of the FRDM-KV10Z, find the J12 will lead the current leakage. After cut the trace of J12 at bottom side, the current in VLPS of my FRDM-KV10Z board down to about 40μA.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/19929i9C096899A3D79341/image-size/large?v=v2&amp;amp;px=999" title="Isolation UART SWD_DIO.png" alt="Isolation UART SWD_DIO.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Test the same project and same MCU with two FRDM-KV10Z boards but using different firmware applications for onboard OpenSDA, get different current in VLPS. &lt;BR /&gt;Compare firmware application of onboard OpenSDA, find different J-Link firmware will set different voltage to UART1_TX_TGTMCU_R. When use newest Board-Specific Firmwares'19_OpenSDA_FRDM-KV10Z.bin', the PTB17/UART0_TX current leakage occurs.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Conclusion:&lt;BR /&gt;We think it meet the 'Internal pull-up/down case' in &lt;A href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fprocessors.wiki.ti.com%2Findex.php%2FOptimizing_IO_Power_Consumption" rel="nofollow" target="_blank"&gt;Optimizing IO Power Consumption&lt;/A&gt;. Customer should avoid this.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/19968iF8D0E50B3F3D15F8/image-size/large?v=v2&amp;amp;px=999" title="Fig3_internalpullupdowncell.JPG" alt="Fig3_internalpullupdowncell.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Jun 2017 00:53:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKV10Z64-VLPS-high-current-draw/m-p/675908#M41567</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2017-06-08T00:53:06Z</dc:date>
    </item>
  </channel>
</rss>