<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックI m working on FRDM-KE06Z brd. I have written a simple code to configure SPI0 as master and to transfer 1 byte of data to the spi data buffer. I m not getting any output for the SPI0(none of the signals are coming out when probed). codeattched. plz help</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/I-m-working-on-FRDM-KE06Z-brd-I-have-written-a-simple-code-to/m-p/675508#M41531</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Code is attached&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-337609"&gt;SPI.c.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-337609"&gt;main.c.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 19 Jul 2017 10:39:32 GMT</pubDate>
    <dc:creator>lajithacs</dc:creator>
    <dc:date>2017-07-19T10:39:32Z</dc:date>
    <item>
      <title>I m working on FRDM-KE06Z brd. I have written a simple code to configure SPI0 as master and to transfer 1 byte of data to the spi data buffer. I m not getting any output for the SPI0(none of the signals are coming out when probed). codeattched. plz help</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/I-m-working-on-FRDM-KE06Z-brd-I-have-written-a-simple-code-to/m-p/675508#M41531</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Code is attached&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-337609"&gt;SPI.c.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-337609"&gt;main.c.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Jul 2017 10:39:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/I-m-working-on-FRDM-KE06Z-brd-I-have-written-a-simple-code-to/m-p/675508#M41531</guid>
      <dc:creator>lajithacs</dc:creator>
      <dc:date>2017-07-19T10:39:32Z</dc:date>
    </item>
    <item>
      <title>Re: I m working on FRDM-KE06Z brd. I have written a simple code to configure SPI0 as master and to transfer 1 byte of data to the spi data buffer. I m not getting any output for the SPI0(none of the signals are coming out when probed). codeattched. plz he</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/I-m-working-on-FRDM-KE06Z-brd-I-have-written-a-simple-code-to/m-p/675509#M41532</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;The initialization of SPI0 module pins and clock seems right. One problem can with the comparison in&amp;nbsp;&lt;EM&gt;register_write()&lt;/EM&gt;&lt;/P&gt;&lt;PRE class="language-none line-numbers"&gt;&lt;CODE&gt;if(SPI0_S == 0x20)‍‍‍‍&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;Instead of this comparison, try:&lt;/P&gt;&lt;PRE class="language-none line-numbers"&gt;&lt;CODE&gt;if((SPI0_S &amp;amp; 0x20) == 0x20)‍&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;(Because other bits in &lt;EM&gt;SPI0_S&amp;nbsp;&lt;/EM&gt;like &lt;EM&gt;SPRF&lt;/EM&gt;, &lt;EM&gt;SPMF&amp;nbsp;&lt;/EM&gt;can also be 1. Then SPI0_S may not be 0x20 always)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Good luck&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Jul 2017 17:09:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/I-m-working-on-FRDM-KE06Z-brd-I-have-written-a-simple-code-to/m-p/675509#M41532</guid>
      <dc:creator>visakhanc</dc:creator>
      <dc:date>2017-07-19T17:09:57Z</dc:date>
    </item>
    <item>
      <title>Re: I m working on FRDM-KE06Z brd. I have written a simple code to configure SPI0 as master and to transfer 1 byte of data to the spi data buffer. I m not getting any output for the SPI0(none of the signals are coming out when probed). codeattched. plz he</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/I-m-working-on-FRDM-KE06Z-brd-I-have-written-a-simple-code-to/m-p/675510#M41533</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Vishakhan C. SPI0&amp;nbsp;working fine now!!!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Jul 2017 06:22:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/I-m-working-on-FRDM-KE06Z-brd-I-have-written-a-simple-code-to/m-p/675510#M41533</guid>
      <dc:creator>lajithacs</dc:creator>
      <dc:date>2017-07-20T06:22:25Z</dc:date>
    </item>
    <item>
      <title>Re: I m working on FRDM-KE06Z brd. I have written a simple code to configure SPI0 as master and to transfer 1 byte of data to the spi data buffer. I m not getting any output for the SPI0(none of the signals are coming out when probed). codeattched. plz he</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/I-m-working-on-FRDM-KE06Z-brd-I-have-written-a-simple-code-to/m-p/675511#M41534</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good to know it helped you!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Jul 2017 06:53:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/I-m-working-on-FRDM-KE06Z-brd-I-have-written-a-simple-code-to/m-p/675511#M41534</guid>
      <dc:creator>visakhanc</dc:creator>
      <dc:date>2017-07-20T06:53:22Z</dc:date>
    </item>
  </channel>
</rss>