<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: Can't find I2S MCLK source options in K22F documentation</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-find-I2S-MCLK-source-options-in-K22F-documentation/m-p/674209#M41447</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Scott,&lt;/P&gt;&lt;P&gt;See the chapter '5.7.9 I2S/SAI clocking' in &lt;A href="http://www.nxp.com/docs/en/reference-manual/K22P64M120SF5V2RM.pdf"&gt;K22P64M120SF5V2RM&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="5.7.9 I2S SAI clocking.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/24737i696B683C11B9A038/image-size/large?v=v2&amp;amp;px=999" role="button" title="5.7.9 I2S SAI clocking.png" alt="5.7.9 I2S SAI clocking.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 27 Jun 2017 06:55:20 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2017-06-27T06:55:20Z</dc:date>
    <item>
      <title>Can't find I2S MCLK source options in K22F documentation</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-find-I2S-MCLK-source-options-in-K22F-documentation/m-p/674208#M41446</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The MK22FN1M0AVLH12 reference manual's section on the I2S module master clock says to see the chip-specific configuration information for the definitions of the input options used by I2Sx_TCR2[MSEL] and I2Sx_MCR[MICS]. &amp;nbsp;I can't find those definitions in the chip-specific information - just the rather unhelpful statement that "The MCLK Input Clock Select bit of the MCLK Control Register (MCR[MICS]) selects the clock input to the I2S/SAI module’s MCLK divider."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Where are these clock source options listed?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Scott&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Jun 2017 18:27:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-find-I2S-MCLK-source-options-in-K22F-documentation/m-p/674208#M41446</guid>
      <dc:creator>scottm</dc:creator>
      <dc:date>2017-06-26T18:27:07Z</dc:date>
    </item>
    <item>
      <title>Re: Can't find I2S MCLK source options in K22F documentation</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-find-I2S-MCLK-source-options-in-K22F-documentation/m-p/674209#M41447</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Scott,&lt;/P&gt;&lt;P&gt;See the chapter '5.7.9 I2S/SAI clocking' in &lt;A href="http://www.nxp.com/docs/en/reference-manual/K22P64M120SF5V2RM.pdf"&gt;K22P64M120SF5V2RM&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="5.7.9 I2S SAI clocking.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/24737i696B683C11B9A038/image-size/large?v=v2&amp;amp;px=999" role="button" title="5.7.9 I2S SAI clocking.png" alt="5.7.9 I2S SAI clocking.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Jun 2017 06:55:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-find-I2S-MCLK-source-options-in-K22F-documentation/m-p/674209#M41447</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2017-06-27T06:55:20Z</dc:date>
    </item>
    <item>
      <title>Re: Can't find I2S MCLK source options in K22F documentation</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-find-I2S-MCLK-source-options-in-K22F-documentation/m-p/674210#M41448</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks. &amp;nbsp;I was confused because 3.9.6.2 is&amp;nbsp;&lt;EM&gt;also&lt;/EM&gt; entitled "I2S/SAI clocking" and there's no indication there that more information is to be found elsewhere. &amp;nbsp;It would be great if someday all of the reference manuals had hyperlinks between sections whenever the relevant information is spread out.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Scott&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Jun 2017 18:11:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-find-I2S-MCLK-source-options-in-K22F-documentation/m-p/674210#M41448</guid>
      <dc:creator>scottm</dc:creator>
      <dc:date>2017-06-27T18:11:49Z</dc:date>
    </item>
  </channel>
</rss>