<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックCan Run Spi Flash Memory IC with SD_Card component in MCUonelipse ?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-Run-Spi-Flash-Memory-IC-with-SD-Card-component-in/m-p/223084#M4143</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all&lt;/P&gt;&lt;P&gt;I use KL25Z board, with have SPI Flash Memory ( Do not install ). I use Fat_FileSystem component for Professor Expert from website MCUonelipse , and memory require of Fat_FileSystem is SD Card .&lt;/P&gt;&lt;P&gt;. So i I attend that :&lt;/P&gt;&lt;P&gt;1. Add SD_Card component for Professor Expert from MCUonelipse in Fat_FileSystem .&lt;/P&gt;&lt;P&gt;2. install IC Flash memory in KL25Zboard.&lt;/P&gt;&lt;P&gt;3. The Pin which connect to SD_Card, i will use to connect to IC Flash memory&lt;/P&gt;&lt;P&gt;4. And i will run function : SD_Card read from SD_Card component .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does IC Flash Memory can replace SD_Card ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Phuong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 11 Feb 2014 06:30:42 GMT</pubDate>
    <dc:creator>afdasdfas</dc:creator>
    <dc:date>2014-02-11T06:30:42Z</dc:date>
    <item>
      <title>Can Run Spi Flash Memory IC with SD_Card component in MCUonelipse ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-Run-Spi-Flash-Memory-IC-with-SD-Card-component-in/m-p/223084#M4143</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all&lt;/P&gt;&lt;P&gt;I use KL25Z board, with have SPI Flash Memory ( Do not install ). I use Fat_FileSystem component for Professor Expert from website MCUonelipse , and memory require of Fat_FileSystem is SD Card .&lt;/P&gt;&lt;P&gt;. So i I attend that :&lt;/P&gt;&lt;P&gt;1. Add SD_Card component for Professor Expert from MCUonelipse in Fat_FileSystem .&lt;/P&gt;&lt;P&gt;2. install IC Flash memory in KL25Zboard.&lt;/P&gt;&lt;P&gt;3. The Pin which connect to SD_Card, i will use to connect to IC Flash memory&lt;/P&gt;&lt;P&gt;4. And i will run function : SD_Card read from SD_Card component .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does IC Flash Memory can replace SD_Card ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Phuong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Feb 2014 06:30:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-Run-Spi-Flash-Memory-IC-with-SD-Card-component-in/m-p/223084#M4143</guid>
      <dc:creator>afdasdfas</dc:creator>
      <dc:date>2014-02-11T06:30:42Z</dc:date>
    </item>
    <item>
      <title>Re: Can Run Spi Flash Memory IC with SD_Card component in MCUonelipse ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-Run-Spi-Flash-Memory-IC-with-SD-Card-component-in/m-p/223085#M4144</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Phuong,&lt;/P&gt;&lt;P&gt;That unpopulated EEPROM is not connected to the KL25Z: it is connected to the pins of the K20 (OpenSDA chip). So for sure you would need to make hardware modifications to access it from the KL25Z.&lt;/P&gt;&lt;P&gt;But more important: an EEPROM or external FLASH chip has a completly different protocol and command set compared to an SD card. So you cannot swap in an EEPROM instead of an SD card without software/driver modifications. Yes, it is very possible to implement a FatFS driver using an external EEPROM, and the FatFS driver API supports multiple 'memory' types. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Feb 2014 07:28:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-Run-Spi-Flash-Memory-IC-with-SD-Card-component-in/m-p/223085#M4144</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2014-02-11T07:28:03Z</dc:date>
    </item>
    <item>
      <title>Re: Can Run Spi Flash Memory IC with SD_Card component in MCUonelipse ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-Run-Spi-Flash-Memory-IC-with-SD-Card-component-in/m-p/223086#M4145</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Erich&lt;/P&gt;&lt;P&gt;Yes. I have a mistake, Flash IC is not connected to MCU&amp;nbsp; MKL25Z of board. now i change to use SD card for FATFS .Thank you.&lt;/P&gt;&lt;P&gt;Phuong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Feb 2014 08:30:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-Run-Spi-Flash-Memory-IC-with-SD-Card-component-in/m-p/223086#M4145</guid>
      <dc:creator>afdasdfas</dc:creator>
      <dc:date>2014-02-11T08:30:46Z</dc:date>
    </item>
  </channel>
</rss>