<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: K60 clock running at half speed.  Why?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-clock-running-at-half-speed-Why/m-p/155831#M414</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I resolved the problem.&amp;nbsp; A hardware layout problem on the board resulted in a 25 Mhz clock instead of 50 Mhz.&amp;nbsp; This has been fixed with cuts/jumpers.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 06 Nov 2012 18:02:45 GMT</pubDate>
    <dc:creator>PhilH</dc:creator>
    <dc:date>2012-11-06T18:02:45Z</dc:date>
    <item>
      <title>K60 clock running at half speed.  Why?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-clock-running-at-half-speed-Why/m-p/155829#M412</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to port to a new development board. It has a K60 chip and is using a 50Mhz external clock input.&amp;nbsp; I started with the 3.8.1 release and just compiled the libraries in debug mode and tried one of the examples.&amp;nbsp; It hung in the clock setup code.&amp;nbsp; Since all my previous experience is with 3.8.0, I downloaded the older release and tried that.&amp;nbsp; That code comes up and runs (does not get hung in the clock setup code).&amp;nbsp; I tried to configure UART5 as that is wired through a MAX232 chip for serial access.&amp;nbsp; I was getting garbage characters on both input and output but it did get an interrupt when I typed a char into hyperterminal.&amp;nbsp; I tried a small loop of "_time_delay(1000); printf("x");"&amp;nbsp; and found it was taking twice as long to output the garbage char.&amp;nbsp; This led me to think the clock was running slow by 2 x so I tried to connect at 4800 baud (instead of the configured by me of 9600) and success.&amp;nbsp; I can now talk correctly to a serial port.&amp;nbsp; The question is why is the clock running 2x slow?&amp;nbsp; This is the same exact startup code as run on the&amp;nbsp; TOWER hardware platform which also has a 50 Mhz input clock. Anyone have a clue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Phil H.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Oct 2012 05:47:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-clock-running-at-half-speed-Why/m-p/155829#M412</guid>
      <dc:creator>PhilH</dc:creator>
      <dc:date>2012-10-29T05:47:30Z</dc:date>
    </item>
    <item>
      <title>Re: K60 clock running at half speed.  Why?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-clock-running-at-half-speed-Why/m-p/155830#M413</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Not sure what your problem is specifically. But UART 0 &amp;amp; 1 use the system clock and the others use the bus clock. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Nov 2012 16:52:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-clock-running-at-half-speed-Why/m-p/155830#M413</guid>
      <dc:creator>crezyoz</dc:creator>
      <dc:date>2012-11-06T16:52:56Z</dc:date>
    </item>
    <item>
      <title>Re: K60 clock running at half speed.  Why?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-clock-running-at-half-speed-Why/m-p/155831#M414</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I resolved the problem.&amp;nbsp; A hardware layout problem on the board resulted in a 25 Mhz clock instead of 50 Mhz.&amp;nbsp; This has been fixed with cuts/jumpers.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Nov 2012 18:02:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-clock-running-at-half-speed-Why/m-p/155831#M414</guid>
      <dc:creator>PhilH</dc:creator>
      <dc:date>2012-11-06T18:02:45Z</dc:date>
    </item>
  </channel>
</rss>