<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic KL16z don't work in run mode in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL16z-don-t-work-in-run-mode/m-p/673426#M41376</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am developing a program using a kinetis kl16z128. It's works correctly when in "debug mode", but in "run mode", does not boot. It's like if I was&amp;nbsp;not power up or its in reset.&lt;/P&gt;&lt;P&gt;When I click "resume" in debug mode it works correctly. I disconnect the USBDM and reset the board, the programm load do not boot, notinhg works.&lt;/P&gt;&lt;P&gt;I am using CodeWarrior 10.7 and USBDM.&lt;/P&gt;&lt;P&gt;Does anyone know what this problem is?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 03 Jun 2017 17:10:12 GMT</pubDate>
    <dc:creator>carlosalexandre</dc:creator>
    <dc:date>2017-06-03T17:10:12Z</dc:date>
    <item>
      <title>KL16z don't work in run mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL16z-don-t-work-in-run-mode/m-p/673426#M41376</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am developing a program using a kinetis kl16z128. It's works correctly when in "debug mode", but in "run mode", does not boot. It's like if I was&amp;nbsp;not power up or its in reset.&lt;/P&gt;&lt;P&gt;When I click "resume" in debug mode it works correctly. I disconnect the USBDM and reset the board, the programm load do not boot, notinhg works.&lt;/P&gt;&lt;P&gt;I am using CodeWarrior 10.7 and USBDM.&lt;/P&gt;&lt;P&gt;Does anyone know what this problem is?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 03 Jun 2017 17:10:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL16z-don-t-work-in-run-mode/m-p/673426#M41376</guid>
      <dc:creator>carlosalexandre</dc:creator>
      <dc:date>2017-06-03T17:10:12Z</dc:date>
    </item>
    <item>
      <title>Re: KL16z don't work in run mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL16z-don-t-work-in-run-mode/m-p/673427#M41377</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Carlos Alexandre Ferri,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;&amp;nbsp; 1. Make sure you download the code in the flash, not the RAM.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; After you download the code to the flash, power off and power on the board again, to check whether your application code works or not?&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; I don't have the USBDM on my side, so I don't know whether it caused by your USBDM.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;&amp;nbsp; 2.&amp;nbsp; &amp;nbsp; Check the following properties&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/19662i35F04BB305E8FC63/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Make sure your are select the ewl, not ewl_hosted.&lt;/P&gt;&lt;P&gt;&amp;nbsp;3. If you are still not OK,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Check whether your USBDM can download the .bin, .hex directly, without the IDE.&lt;/P&gt;&lt;P&gt;&amp;nbsp; Then, you can generate the .hex or .bin to download directly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Jun 2017 05:28:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL16z-don-t-work-in-run-mode/m-p/673427#M41377</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2017-06-05T05:28:49Z</dc:date>
    </item>
    <item>
      <title>Re: KL16z don't work in run mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL16z-don-t-work-in-run-mode/m-p/673428#M41378</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kerry,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you so much for help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My project was set&amp;nbsp;"ewl_hosted", when I change to "ewl", &amp;nbsp;it worked right.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Alexandre&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Jun 2017 13:57:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL16z-don-t-work-in-run-mode/m-p/673428#M41378</guid>
      <dc:creator>carlosalexandre</dc:creator>
      <dc:date>2017-06-05T13:57:10Z</dc:date>
    </item>
  </channel>
</rss>