<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to use PWT to capture the pulse width with KE06 in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-use-PWT-to-capture-the-pulse-width-with-KE06/m-p/672104#M41287</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;Zhong,&lt;/P&gt;&lt;P&gt;Normally the user can calculate the frequency of input pulse by reading PPW and NPW. &lt;BR /&gt;If the pulse width which you want to measure is larger than 'Max pulse width', that may cause the problem.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/25629i679E700EE128E75D/image-size/large?v=v2&amp;amp;px=999" title="Max pulse width.png" alt="Max pulse width.png" /&gt;&lt;/span&gt;&lt;BR /&gt;You can connect a higher frequency signal to test whether the PWT can measure correct width. &lt;BR /&gt;For example:&lt;/P&gt;&lt;P&gt;Enable the Bus clock output on PTH2. (SIM_SOPT0[CLKOE]=1)&lt;/P&gt;&lt;P&gt;And enable bus clock output via an optional prescaler. (SIM_SOPT0[BUSREF]=100)&lt;/P&gt;&lt;P&gt;And then connect PTH2 to PTD5(as PWT input).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 19 Jul 2017 08:16:09 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2017-07-19T08:16:09Z</dc:date>
    <item>
      <title>How to use PWT to capture the pulse width with KE06</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-use-PWT-to-capture-the-pulse-width-with-KE06/m-p/672103#M41286</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a&amp;nbsp; FRDM-KE06Z. I hope to use PWT to capture the pulse width. The attached is my KDS project with PE.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I use GPIO( as BusTx) to send a pulse series on pin PTD0, connected pin PTD5( as PWT input).&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;PWT is configured &amp;nbsp;as "The first falling edge starts the pulse width measurement, and on all the subsequent rising and falling edges, the pulse width is captured.", &amp;nbsp;PWT Clock is set to 24Mhz, enable PWT to generate interrupt when PWTRDY is set and enable PWT to generate interrupt when PWTOV is set.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When the program is running, and press sw2 button (sand a frame), I can see the signal on pin PTD5(PWT input pin). But PWT do not take the any data for pulse width. In fact, I can check the PWT overflow interrupt was taken place, and if I let the PTD5 as float, PWT can capture a pulse data to print in random.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could you advise me the solution for it?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Many thanks!&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Robert&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-337658"&gt;ke06PWT.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Jul 2017 04:00:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-use-PWT-to-capture-the-pulse-width-with-KE06/m-p/672103#M41286</guid>
      <dc:creator>zhongshen</dc:creator>
      <dc:date>2017-07-18T04:00:10Z</dc:date>
    </item>
    <item>
      <title>Re: How to use PWT to capture the pulse width with KE06</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-use-PWT-to-capture-the-pulse-width-with-KE06/m-p/672104#M41287</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;Zhong,&lt;/P&gt;&lt;P&gt;Normally the user can calculate the frequency of input pulse by reading PPW and NPW. &lt;BR /&gt;If the pulse width which you want to measure is larger than 'Max pulse width', that may cause the problem.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/25629i679E700EE128E75D/image-size/large?v=v2&amp;amp;px=999" title="Max pulse width.png" alt="Max pulse width.png" /&gt;&lt;/span&gt;&lt;BR /&gt;You can connect a higher frequency signal to test whether the PWT can measure correct width. &lt;BR /&gt;For example:&lt;/P&gt;&lt;P&gt;Enable the Bus clock output on PTH2. (SIM_SOPT0[CLKOE]=1)&lt;/P&gt;&lt;P&gt;And enable bus clock output via an optional prescaler. (SIM_SOPT0[BUSREF]=100)&lt;/P&gt;&lt;P&gt;And then connect PTH2 to PTD5(as PWT input).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Jul 2017 08:16:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-use-PWT-to-capture-the-pulse-width-with-KE06/m-p/672104#M41287</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2017-07-19T08:16:09Z</dc:date>
    </item>
    <item>
      <title>Re: How to use PWT to capture the pulse width with KE06</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-use-PWT-to-capture-the-pulse-width-with-KE06/m-p/672105#M41288</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Robin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for you reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I known the PWT to measure fast frequency. In my project, created tx frame on PTD0 in about 27kbps, which can see on the scope and connect to PWT input (PTD5), the problem I met is PWT can take interrupt on overflow, but it cannot capture any pulse width, as like as PWT input does not connect anything.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I guess that maybe PE configuration has bug? Please give me a fevor &amp;nbsp;to check.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Jul 2017 09:46:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-use-PWT-to-capture-the-pulse-width-with-KE06/m-p/672105#M41288</guid>
      <dc:creator>zhongshen</dc:creator>
      <dc:date>2017-07-19T09:46:12Z</dc:date>
    </item>
    <item>
      <title>Re: How to use PWT to capture the pulse width with KE06</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-use-PWT-to-capture-the-pulse-width-with-KE06/m-p/672106#M41289</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Test with the FRDM-KE06Z REV A1 board. Press the SW2 and wait the code stop at the breakpoiont.&lt;/P&gt;&lt;P&gt;Not sure if these results meet your needs.&lt;/P&gt;&lt;P&gt;But the PWT seems works and catched &lt;SPAN style="color: #ff0000;"&gt;first Positive pulse&lt;/SPAN&gt; and &lt;SPAN style="color: #3366ff;"&gt;second Negative pulse.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/26643i7A67A8E1084B03AB/image-size/large?v=v2&amp;amp;px=999" title="imageFile.png" alt="imageFile.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;intervel_time[0] catch the &lt;SPAN style="color: #ff0000;"&gt;NegativeWidth&lt;/SPAN&gt;, and it meet the data: &lt;SPAN style="color: #ff0000;"&gt;0xfcb/24MHz=168.46us&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/26683i1C16B8BCFDC4AEAF/image-size/large?v=v2&amp;amp;px=999" title="intervel_time[0].png" alt="intervel_time[0].png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3366ff;"&gt;intervel_time[1]&lt;/SPAN&gt; catch the &lt;SPAN style="color: #3366ff;"&gt;PositiveWidth&lt;/SPAN&gt;, and it meet the data: &lt;SPAN style="color: #3366ff;"&gt;0x1da/24MHz=19.75us&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/26713i26C5048C230D7E01/image-size/large?v=v2&amp;amp;px=999" title="intervel_time[1].png" alt="intervel_time[1].png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Jul 2017 08:22:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-use-PWT-to-capture-the-pulse-width-with-KE06/m-p/672106#M41289</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2017-07-24T08:22:40Z</dc:date>
    </item>
  </channel>
</rss>