<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Using QSPI in K81 in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-QSPI-in-K81/m-p/671669#M41249</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to use QSPI in K81 (TWR_K81F150M). And importing the example "qspi_polling_transfer", without modifying any code, it always fail, printing "The data is wrong".&lt;/P&gt;&lt;P&gt;Same occurs with example "qspi_edma_transfer".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Checking the memory monitor, in each write, the first 2 bytes is always "CCCC". For example, writing&lt;/P&gt;&lt;P&gt;uint32_t data[4] containing numbers 1, 2, 3, 4 in memory 0x6800 0000 will lead to:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;memory addr &amp;nbsp;- &amp;nbsp; values&lt;/P&gt;&lt;P&gt;0x6800 0000 &amp;nbsp;- CCCC0000 00010000 00020000&lt;/P&gt;&lt;P&gt;0x6800 000C &amp;nbsp;- &amp;nbsp;00030000 &amp;nbsp;00040000 00000000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;where, I think, it should be:&lt;/P&gt;&lt;P&gt;0x6800 0000 &amp;nbsp;- 00000001 00000002 00000003&lt;/P&gt;&lt;P&gt;0x6800 000C &amp;nbsp;- &amp;nbsp;00000004 &amp;nbsp;00000000 00000000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any idea?&lt;/P&gt;&lt;P&gt;Thanks :smileygrin:!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 23 Jun 2017 18:16:48 GMT</pubDate>
    <dc:creator>alysonrosa</dc:creator>
    <dc:date>2017-06-23T18:16:48Z</dc:date>
    <item>
      <title>Using QSPI in K81</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-QSPI-in-K81/m-p/671669#M41249</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to use QSPI in K81 (TWR_K81F150M). And importing the example "qspi_polling_transfer", without modifying any code, it always fail, printing "The data is wrong".&lt;/P&gt;&lt;P&gt;Same occurs with example "qspi_edma_transfer".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Checking the memory monitor, in each write, the first 2 bytes is always "CCCC". For example, writing&lt;/P&gt;&lt;P&gt;uint32_t data[4] containing numbers 1, 2, 3, 4 in memory 0x6800 0000 will lead to:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;memory addr &amp;nbsp;- &amp;nbsp; values&lt;/P&gt;&lt;P&gt;0x6800 0000 &amp;nbsp;- CCCC0000 00010000 00020000&lt;/P&gt;&lt;P&gt;0x6800 000C &amp;nbsp;- &amp;nbsp;00030000 &amp;nbsp;00040000 00000000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;where, I think, it should be:&lt;/P&gt;&lt;P&gt;0x6800 0000 &amp;nbsp;- 00000001 00000002 00000003&lt;/P&gt;&lt;P&gt;0x6800 000C &amp;nbsp;- &amp;nbsp;00000004 &amp;nbsp;00000000 00000000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any idea?&lt;/P&gt;&lt;P&gt;Thanks :smileygrin:!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Jun 2017 18:16:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-QSPI-in-K81/m-p/671669#M41249</guid>
      <dc:creator>alysonrosa</dc:creator>
      <dc:date>2017-06-23T18:16:48Z</dc:date>
    </item>
    <item>
      <title>Re: Using QSPI in K81</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-QSPI-in-K81/m-p/671670#M41250</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alyson Rosa,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tested this code example in my side (using MCUXpresso IDE and SDK 2.2) and I couldn't see any problem in its functionality. The board doesn't require any special setting in its jumpers but just to discard, please verify this. Also, K81 doesn't have SDK downloable package, so are you using a K80 package?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Jorge Alcala&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Jul 2017 00:45:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-QSPI-in-K81/m-p/671670#M41250</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2017-07-19T00:45:51Z</dc:date>
    </item>
    <item>
      <title>Re: Using QSPI in K81</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-QSPI-in-K81/m-p/671671#M41251</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jorge,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you share the code? Or at least the LookUp Table (LUT) for this flash?&lt;/P&gt;&lt;P&gt;I'm using SDK from K82 package.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Jul 2017 17:46:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-QSPI-in-K81/m-p/671671#M41251</guid>
      <dc:creator>alysonrosa</dc:creator>
      <dc:date>2017-07-19T17:46:00Z</dc:date>
    </item>
    <item>
      <title>Re: Using QSPI in K81</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-QSPI-in-K81/m-p/671672#M41252</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alyson Rosa&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry for the late reply, I am using the same code example and SDK package as you, qspi_edma_transfer and K82 SDK 2.2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Jorge Alcala&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Aug 2017 16:32:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-QSPI-in-K81/m-p/671672#M41252</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2017-08-18T16:32:19Z</dc:date>
    </item>
  </channel>
</rss>