<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: KE06 &amp; KE02 question in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE06-KE02-question/m-p/671617#M41248</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello steven qing,&lt;/P&gt;&lt;P&gt;&amp;nbsp;1. KE02 and KE06 is nearly pin to pin compatible in the same package.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Take 64 LQFP package as an example, just pin 13 have difference, KE02 is vss, ke06 is PTI4.&lt;/P&gt;&lt;P&gt;&amp;nbsp; So, when you design the hardware, you need to check the package, then compare KE06 with KE02.&lt;/P&gt;&lt;P&gt;&amp;nbsp; 64LQPF package, except pin13, other pin are the same in hardware.&lt;/P&gt;&lt;P&gt;2. module difference.&lt;/P&gt;&lt;P&gt;&amp;nbsp; CPU frequency: KE06 48Mhz, KE02, 40Mhz or 20Mhz.&lt;/P&gt;&lt;P&gt;&amp;nbsp;flash size, KE06 can up to 128KB, KE02 can up to 64KB.&lt;/P&gt;&lt;P&gt;&amp;nbsp;ram size: KE06 can up to 16KB, KE02 can up to 4KB.&lt;/P&gt;&lt;P&gt;&amp;nbsp;EEPROM, KE06 don't have it, KE02 have 256Byte.&lt;/P&gt;&lt;P&gt;&amp;nbsp;I2C, KE06 have two I2C, KE02 just one.&lt;/P&gt;&lt;P&gt;CAN:KE06 one module, KE02 none.&lt;/P&gt;&lt;P&gt;PWT:KE06 one mdoule, KE02 none.&lt;/P&gt;&lt;P&gt;Just these difference, so the software need to take care about it. Especially the core frequency, FLL factor, KE06 is 1280, ke02 is 1024.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 26 Jun 2017 09:13:46 GMT</pubDate>
    <dc:creator>kerryzhou</dc:creator>
    <dc:date>2017-06-26T09:13:46Z</dc:date>
    <item>
      <title>KE06 &amp; KE02 question</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE06-KE02-question/m-p/671616#M41247</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Expert:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I use the KE06 to design a product, now,I plan to use the KE02 to replace KE06.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So I have questions below:&lt;BR /&gt;(1)hardware:except the hardware sources are different,is the same the other design?Is there any document about this?&lt;BR /&gt;(2)software:whese content will I need modify?Is there any document about this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your support.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Jun 2017 03:11:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE06-KE02-question/m-p/671616#M41247</guid>
      <dc:creator>stevenqing</dc:creator>
      <dc:date>2017-06-23T03:11:57Z</dc:date>
    </item>
    <item>
      <title>Re: KE06 &amp; KE02 question</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE06-KE02-question/m-p/671617#M41248</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello steven qing,&lt;/P&gt;&lt;P&gt;&amp;nbsp;1. KE02 and KE06 is nearly pin to pin compatible in the same package.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Take 64 LQFP package as an example, just pin 13 have difference, KE02 is vss, ke06 is PTI4.&lt;/P&gt;&lt;P&gt;&amp;nbsp; So, when you design the hardware, you need to check the package, then compare KE06 with KE02.&lt;/P&gt;&lt;P&gt;&amp;nbsp; 64LQPF package, except pin13, other pin are the same in hardware.&lt;/P&gt;&lt;P&gt;2. module difference.&lt;/P&gt;&lt;P&gt;&amp;nbsp; CPU frequency: KE06 48Mhz, KE02, 40Mhz or 20Mhz.&lt;/P&gt;&lt;P&gt;&amp;nbsp;flash size, KE06 can up to 128KB, KE02 can up to 64KB.&lt;/P&gt;&lt;P&gt;&amp;nbsp;ram size: KE06 can up to 16KB, KE02 can up to 4KB.&lt;/P&gt;&lt;P&gt;&amp;nbsp;EEPROM, KE06 don't have it, KE02 have 256Byte.&lt;/P&gt;&lt;P&gt;&amp;nbsp;I2C, KE06 have two I2C, KE02 just one.&lt;/P&gt;&lt;P&gt;CAN:KE06 one module, KE02 none.&lt;/P&gt;&lt;P&gt;PWT:KE06 one mdoule, KE02 none.&lt;/P&gt;&lt;P&gt;Just these difference, so the software need to take care about it. Especially the core frequency, FLL factor, KE06 is 1280, ke02 is 1024.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Jun 2017 09:13:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE06-KE02-question/m-p/671617#M41248</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2017-06-26T09:13:46Z</dc:date>
    </item>
  </channel>
</rss>