<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 KW41z hardware flow control(RTS, CTS)</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW41z-hardware-flow-control-RTS-CTS/m-p/670109#M41151</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear sir,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Currently the UART of KW41Z is 2 wire UART(TX, RX). Does KW41Z support RTS, CTS? How do I implement it ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Sean&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 14 Jul 2017 08:38:55 GMT</pubDate>
    <dc:creator>seanwu</dc:creator>
    <dc:date>2017-07-14T08:38:55Z</dc:date>
    <item>
      <title>KW41z hardware flow control(RTS, CTS)</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW41z-hardware-flow-control-RTS-CTS/m-p/670109#M41151</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear sir,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Currently the UART of KW41Z is 2 wire UART(TX, RX). Does KW41Z support RTS, CTS? How do I implement it ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Sean&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Jul 2017 08:38:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW41z-hardware-flow-control-RTS-CTS/m-p/670109#M41151</guid>
      <dc:creator>seanwu</dc:creator>
      <dc:date>2017-07-14T08:38:55Z</dc:date>
    </item>
    <item>
      <title>Re: KW41z hardware flow control(RTS, CTS)</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW41z-hardware-flow-control-RTS-CTS/m-p/670110#M41152</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello seanwu,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The LPUART module from the KW41Z supports hardware flow control and is configured through the&amp;nbsp;LPUARTx_MODIR register. Please refer to chapter&amp;nbsp;&lt;STRONG&gt;38.2.6 LPUART Modem IrDA Register&lt;/STRONG&gt; in the reference manual for information on this functionality.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The current MCUXpresso SDK for&amp;nbsp;KW41Z is based on KSDK 2.2 and the LPUART drivers for this version don't support hardware flow control. This functionality will be supported in KSDK 2.3.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Additionaly, you need to configure the pin mux to the corresponding LPUART RTS/CTS signals.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Gerardo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Aug 2017 00:58:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW41z-hardware-flow-control-RTS-CTS/m-p/670110#M41152</guid>
      <dc:creator>gerardo_rodriguez</dc:creator>
      <dc:date>2017-08-01T00:58:50Z</dc:date>
    </item>
  </channel>
</rss>