<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: KE04 SWD Interface Question</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE04-SWD-Interface-Question/m-p/670028#M41150</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello JIM MORRIS,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; k10 have some difference with the KE series, especially the SWD_CLK pin. K series have the internal pull down, but the KE series don't have it.&lt;/P&gt;&lt;P&gt;&amp;nbsp; For other external resistors, in the application, to work stably, it is better to add the according external resistors.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;If you still have question, please let me know!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 26 Jun 2017 03:22:59 GMT</pubDate>
    <dc:creator>kerryzhou</dc:creator>
    <dc:date>2017-06-26T03:22:59Z</dc:date>
    <item>
      <title>KE04 SWD Interface Question</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE04-SWD-Interface-Question/m-p/670025#M41147</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I just finished a design using a&amp;nbsp;Kinetis KE04 series part (MKE04Z8VTG4), and came across this footnote in section 9.2 (Debug port pin descriptions) of the KE04 reference manual for this part:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. The pad library of this device does not support on-chip pull down; the SWD_CLK pin supports only pulp controlled by PTAPE0, external pulldown resistor is required to fully support the SWD protocol.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yet I have looked at the schematics for the&amp;nbsp;&lt;SPAN style="color: #4a4a4d; background-color: #ffffff; font-size: 16px;"&gt;FRDM-KE04Z board with the 24 pin version of this chip on it, and do not see any pulldown in the circuit on the SWD_CLK line of the device.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #4a4a4d; background-color: #ffffff; font-size: 16px;"&gt;Can anyone comment on this, as I have a completed set of gerber files for my PCB, but don't want to pull the trigger on an order until I know whether I need to add a pulldown resistor on this signal. Right now I just have RESET (PTA5), SWD_DIO (PTA4), and SWD_CLK (PTA0) going to the respective pins on a Mini-10 ARM header, along with GND and VCC.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #4a4a4d; background-color: #ffffff; font-size: 16px;"&gt;Thanks!&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #4a4a4d; background-color: #ffffff; font-size: 16px;"&gt;Jim&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Jun 2017 19:54:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE04-SWD-Interface-Question/m-p/670025#M41147</guid>
      <dc:creator>jimmorris</dc:creator>
      <dc:date>2017-06-21T19:54:18Z</dc:date>
    </item>
    <item>
      <title>Re: KE04 SWD Interface Question</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE04-SWD-Interface-Question/m-p/670026#M41148</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello JIM Morris,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Normally, in the new KE04 design, customer should:&lt;BR /&gt;1. SWD_DIO add 4.7K to 10K external pullup resistor, internal pull up is weak, it is better to add external pull up.&lt;BR /&gt;2. SWD_CLK add external pulldown resistor resistor, because the pin don't have the internal pull down. &lt;BR /&gt;3. Reset_b pin, 4.7K to 10K external pullup resistor, and 0.1uf capacitor to ground.&lt;BR /&gt;4, NMI pin, external 4.7k to 10K pull up.&lt;BR /&gt;You said FRDM-KE04 don't have the exteral pull down in the SWD_CLK pin, you will find, actually, the SWD_CLK also add to the 74LVC125ADB chip which is connect to the on board opensdsa.&lt;BR /&gt;Anyway, to work stably, I suggest you do like the above 4 items which I mentioned.&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;If you still have question about it, please let me know!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Jun 2017 02:11:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE04-SWD-Interface-Question/m-p/670026#M41148</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2017-06-23T02:11:56Z</dc:date>
    </item>
    <item>
      <title>Re: KE04 SWD Interface Question</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE04-SWD-Interface-Question/m-p/670027#M41149</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the tips. &amp;nbsp;I guess I didn't look closely enough at the FRDM-KE04 schematic to catch some of that. &amp;nbsp;My other Kinetis designs have been with the K10 series, and I didn't have to use any external resistors with that device, or at least I got away without using any.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Jun 2017 12:49:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE04-SWD-Interface-Question/m-p/670027#M41149</guid>
      <dc:creator>jimmorris</dc:creator>
      <dc:date>2017-06-23T12:49:14Z</dc:date>
    </item>
    <item>
      <title>Re: KE04 SWD Interface Question</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE04-SWD-Interface-Question/m-p/670028#M41150</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello JIM MORRIS,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; k10 have some difference with the KE series, especially the SWD_CLK pin. K series have the internal pull down, but the KE series don't have it.&lt;/P&gt;&lt;P&gt;&amp;nbsp; For other external resistors, in the application, to work stably, it is better to add the according external resistors.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;If you still have question, please let me know!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Jun 2017 03:22:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE04-SWD-Interface-Question/m-p/670028#M41150</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2017-06-26T03:22:59Z</dc:date>
    </item>
  </channel>
</rss>