<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: K64F: ADC 16 bits range</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K64F-ADC-16-bits-range/m-p/669942#M41146</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Cesar Hoyos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It depends in your VDD, VDDA, VSS, VSSA and VREF voltages. For example if you supply VDD with 3.3V, VDDA must be 3.3V (+/- 0.1V) and then VREFH could be up to 3.3V, so your range is between VREFL and 3.3V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this help you.&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Jorge Alcala&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 09 Jun 2017 01:31:28 GMT</pubDate>
    <dc:creator>jorge_a_vazquez</dc:creator>
    <dc:date>2017-06-09T01:31:28Z</dc:date>
    <item>
      <title>K64F: ADC 16 bits range</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K64F-ADC-16-bits-range/m-p/669941#M41145</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello there,&lt;/P&gt;&lt;P&gt;I am working with development platform of K64F and I am programming the actions of the ADC for conversion in 16bits, single-ended working.&lt;/P&gt;&lt;P&gt;I have read the reference manual, but I am still not sure if I am right about range.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="tablaTensionesADC.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/20310iDC796BDADF412227/image-size/large?v=v2&amp;amp;px=999" role="button" title="tablaTensionesADC.png" alt="tablaTensionesADC.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Following this, I have assumed that the input voltage range is between 0V and 3'6V.&lt;/P&gt;&lt;P&gt;Could anyone confirm this assumption?&lt;/P&gt;&lt;P&gt;Thanks for your attention,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 May 2017 13:24:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K64F-ADC-16-bits-range/m-p/669941#M41145</guid>
      <dc:creator>cesarhoyos</dc:creator>
      <dc:date>2017-05-31T13:24:09Z</dc:date>
    </item>
    <item>
      <title>Re: K64F: ADC 16 bits range</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K64F-ADC-16-bits-range/m-p/669942#M41146</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Cesar Hoyos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It depends in your VDD, VDDA, VSS, VSSA and VREF voltages. For example if you supply VDD with 3.3V, VDDA must be 3.3V (+/- 0.1V) and then VREFH could be up to 3.3V, so your range is between VREFL and 3.3V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this help you.&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Jorge Alcala&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Jun 2017 01:31:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K64F-ADC-16-bits-range/m-p/669942#M41146</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2017-06-09T01:31:28Z</dc:date>
    </item>
  </channel>
</rss>