<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: UART frame error receving from VLPS in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-frame-error-receving-from-VLPS/m-p/668119#M41086</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alessandro Morniroli&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have check your code, I couldn't see any problem in the code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;are there any cases where recovery time from VLPS to RUN is above the max value reported from datasheet,&amp;nbsp;de facto&amp;nbsp;losing the first RX bit?&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;As long as you have mentioned:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;(by the way, I also tried running @ 38400 baudrate but frame errors happen the same but with minor frequency).&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It could be that the problem is related with the first comment of mark in the post &lt;A href="https://community.nxp.com/thread/327741"&gt;Using Kinetis Low Power Stop Modes with unrestricted UART operation - a report&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;where he mentions that there is a problem with the wakeup time and the baud rate limit (where he mentioned that he doesn't see any problem with 57600).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you reduce your baud rate, for example, 9600, do errors still happened?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regardless of this, the problem is related only with the VLPS, as it is taking too much time to wakeup from VLPS to RUN mode, could you try with SMC_SetPowerModeStop (Stop mode), there should be too much difference.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Jorge Alcala&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 28 Jul 2017 21:55:03 GMT</pubDate>
    <dc:creator>jorge_a_vazquez</dc:creator>
    <dc:date>2017-07-28T21:55:03Z</dc:date>
    <item>
      <title>UART frame error receving from VLPS</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-frame-error-receving-from-VLPS/m-p/668117#M41084</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to using VLPS power mode with unrestricted UART operations&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've already read some topics on the community:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/327741" rel="nofollow noopener noreferrer" target="_blank"&gt;Using Kinetis Low Power Stop Modes with unrestricted UART operation - a report&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/442086" rel="nofollow noopener noreferrer" target="_blank"&gt;Deep Sleep and VLPS on MK64FN1M0VLL12&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I understand that the main problem is to stay "alive" (RUN/WAIT or similar) while&amp;nbsp;RX/TX transmissions are active, going to VLPS only when UART peripheral is in "idle" state, waiting for new RX/TX (enabling wakeup from VLPS using RX active edge interrupt).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also understand that&amp;nbsp;the baudrate limit is 57600, since transition from VLPS to RUN on the RX active edge interrupt takes some time (~5uS for my MCU).&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Detecting TX idle status can be done &lt;SPAN&gt;easily&lt;/SPAN&gt;, simply checking UARTx_S1[TC].&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Detecting RX idle status is a bit more difficult (not so difficult indeed).&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Briefly, it should be possible to use UART with unrestricted RX operations acting as follows:&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;- prior to enter VLPS mode, enable UARTx_BDH[RXEDGIE];&lt;BR /&gt;- remain "active" (e.g. RUN or WAIT mode) for RX to be completed;&lt;/P&gt;&lt;P&gt;- detect RX idle status prior to enter VLPS again;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I implemented the following solution, which seems to do the job very well,&amp;nbsp;minimizing the time that MCU stay in RUN/WAIT&amp;nbsp;for allowing RX/TX to complete correctly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;&lt;SPAN class="comment token"&gt;/* Common include. */&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#include &lt;SPAN class="string token"&gt;"fsl_common.h"&lt;/SPAN&gt;&lt;/SPAN&gt;

&lt;SPAN class="property macro token"&gt;#include &lt;SPAN class="string token"&gt;"fsl_clock.h"&lt;/SPAN&gt;&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#include &lt;SPAN class="string token"&gt;"fsl_gpio.h"&lt;/SPAN&gt;&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#include &lt;SPAN class="string token"&gt;"fsl_lptmr.h"&lt;/SPAN&gt;&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#include &lt;SPAN class="string token"&gt;"fsl_port.h"&lt;/SPAN&gt;&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#include &lt;SPAN class="string token"&gt;"fsl_pit.h"&lt;/SPAN&gt;&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#include &lt;SPAN class="string token"&gt;"fsl_ftm.h"&lt;/SPAN&gt;&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#include &lt;SPAN class="string token"&gt;"fsl_smc.h"&lt;/SPAN&gt;&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#include &lt;SPAN class="string token"&gt;"fsl_uart.h"&lt;/SPAN&gt;&lt;/SPAN&gt;

&lt;SPAN class="comment token"&gt;/**
 * Struct used for saving 'is busy' flag about RX/TX channels.
 */&lt;/SPAN&gt;
&lt;SPAN class="keyword token"&gt;static&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;union&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; uint8_t raw&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;/**&amp;lt; Raw data. */&lt;/SPAN&gt;

&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="keyword token"&gt;struct&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; uint8_t rx&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;:&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;/**&amp;lt; RX channel flag. */&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; uint8_t tx&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;:&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;/**&amp;lt; TX channel flag. */&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; uint8_t spare &lt;SPAN class="punctuation token"&gt;:&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;6&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;/**&amp;lt; Not used.&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; */&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt; bit&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt; tsgIsBusy&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

&lt;SPAN class="comment token"&gt;/**
 * Variable used for storing received input.
 */&lt;/SPAN&gt;
&lt;SPAN class="keyword token"&gt;static&lt;/SPAN&gt; uint8_t u8sgInput&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

&lt;SPAN class="comment token"&gt;/**
 * UART2 ISR handler.
 */&lt;/SPAN&gt;
&lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt;
UART2_RX_TX_IRQHandler &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; uint32_t u32lSr &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;/* Get UART status register. */&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; u32lSr &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; UART_GetStatusFlags &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;UART2&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;/* TX completed? */&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="keyword token"&gt;if&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;u32lSr &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt; UART_S1_TC_MASK&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;/* Clear TX 'is busy' flag. */&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; tsgIsBusy&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;bit&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;tx &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;

&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;/* RX active edge interrupt? */&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="keyword token"&gt;if&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;u32lSr &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt; kUART_RxActiveEdgeFlag&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;/* Set RX 'is busy' flag. */&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; tsgIsBusy&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;bit&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;rx &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;/* Disable RX active edge interrupt (for minimizing ISR overhead). */&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; UART_DisableInterrupts &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;UART2&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; kUART_RxActiveEdgeInterruptEnable&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;/* Clear RXEDGIF flag. */&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; UART2&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;S2 &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; UART_S2_RXEDGIF_MASK&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;

&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;/* RX data received? */&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="keyword token"&gt;if&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;u32lSr &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt; kUART_RxDataRegFullFlag&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;/* Just read the byte received from UART_D register. */&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; u8sgInput &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; UART_ReadByte &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;UART2&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;/* Clear RXEDGIF flag (just in case). */&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; UART2&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;S2 &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; UART_S2_RXEDGIF_MASK&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;

&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;/* RX idle? */&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="keyword token"&gt;if&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;u32lSr &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt; kUART_IdleLineFlag&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;/* Clear RX 'is busy' flag. */&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; tsgIsBusy&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;bit&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;rx &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;/*
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; * UART_D still not read?
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; *
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; * Please note that interrupt may be delayed and executed when IDLE
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; * interrupt has been already triggered.
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; */&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="keyword token"&gt;if&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;!&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;u32lSr &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt; kUART_RxDataRegFullFlag&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;/* Read data from UART_D for enabling IDLE interrupt again. */&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; UART_ReadByte &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;UART2&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;

&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;/* Enable RX active edge interrupt again. */&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; UART_EnableInterrupts&amp;nbsp; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;UART2&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; kUART_RxActiveEdgeInterruptEnable&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;

&lt;SPAN class="comment token"&gt;/**
 * UART2 error ISR handler.
 */&lt;/SPAN&gt;
&lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt;
UART2_ERR_IRQHandler &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; uint32_t u32lSr &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;/* Get UART status register. */&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; u32lSr &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; UART_GetStatusFlags &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;UART2&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;/* Clear UART status register. */&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; UART_ClearStatusFlags &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;UART2&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; u32lSr&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;


&lt;SPAN class="comment token"&gt;/**
 * Main routine.
 *
 * @return Never.
 */&lt;/SPAN&gt;
&lt;SPAN class="keyword token"&gt;int&lt;/SPAN&gt;
main &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="keyword token"&gt;const&lt;/SPAN&gt; mcg_config_t tlConfig &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;mcgMode&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; kMCG_ModeFEI&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;irclkEnableMode &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;ircs&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; kMCG_IrcSlow&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;fcrdiv&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;frdiv&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;dmx32&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; kMCG_Dmx32Fine&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;pll0Config&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;drs&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; kMCG_DrsMidHigh
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="keyword token"&gt;const&lt;/SPAN&gt; gpio_pin_config_t tlLedPinConfig &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;pinDirection &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; kGPIO_DigitalOutput&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;outputLogic&amp;nbsp; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="keyword token"&gt;const&lt;/SPAN&gt; uart_config_t tlUartConfig &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;baudRate_Bps&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;57600&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;parityMode&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; kUART_ParityDisabled&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;txFifoWatermark &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;rxFifoWatermark &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;enableTx&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;enableRx&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; uint32_t u32lMask&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SMC_SetPowerModeProtection &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;SMC&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; kSMC_AllowPowerModeVlp&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CLOCK_SetSimSafeDivs &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CLOCK_SetMcgConfig &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;tlConfig&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SystemCoreClockUpdate &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CLOCK_EnableClock &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;kCLOCK_PortA&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CLOCK_EnableClock &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;kCLOCK_PortD&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORT_SetPinMux &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;PORTA&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; kPORT_MuxAsGpio&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORT_SetPinMux &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;PORTD&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;6&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; kPORT_MuxAlt3&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORT_SetPinMux &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;PORTD&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;7&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; kPORT_MuxAlt3&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; GPIO_PinInit &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;GPIOA&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;tlLedPinConfig&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; UART_Init &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;UART2&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;tlUartConfig&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; CLOCK_GetBusClkFreq &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; UART2&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;PFIFO &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;~&lt;/SPAN&gt;UART_PFIFO_RXFE_MASK &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;~&lt;/SPAN&gt;UART_PFIFO_TXFE_MASK&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;/* Idle character bit count starts after stop bit. */&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; UART2&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;C1 &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; UART_C1_ILT_MASK&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; UART2&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;PFIFO &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;~&lt;/SPAN&gt;UART_PFIFO_RXFE_MASK &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;~&lt;/SPAN&gt;UART_PFIFO_TXFE_MASK&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; UART_EnableInterrupts &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;UART2&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; kUART_RxDataRegFullInterruptEnable &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; kUART_RxOverrunInterruptEnable&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; kUART_NoiseErrorInterruptEnable&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; kUART_FramingErrorInterruptEnable&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; kUART_ParityErrorInterruptEnable&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; kUART_IdleLineInterruptEnable&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; kUART_RxActiveEdgeInterruptEnable&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; NVIC_SetPriority &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;UART2_ERR_IRQn&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="number token"&gt;8&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; NVIC_SetPriority &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;UART2_RX_TX_IRQn&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;10&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; NVIC_EnableIRQ &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;UART2_ERR_IRQn&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; NVIC_EnableIRQ &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;UART2_RX_TX_IRQn&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="keyword token"&gt;while&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;true&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; u32lMask &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; DisableGlobalIRQ &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;/* RX/TX active? */&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="keyword token"&gt;if&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;tsgIsBusy&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;raw&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; GPIO_SetPinsOutput &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;GPIOA&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;lt;&amp;lt;&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;/* Stay in wait power mode. */&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SMC_SetPowerModeWait &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;SMC&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="keyword token"&gt;else&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; GPIO_ClearPinsOutput &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;GPIOA&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;lt;&amp;lt;&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;/* RX/TX idle: just enter VLPS. */&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SMC_SetPowerModeVlps &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;SMC&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;

&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; EnableGlobalIRQ &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;u32lMask&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;

&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="keyword token"&gt;return&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;
‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;BR /&gt;So, each time a byte is received, the UART ISR should trigger three times:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- the first one, because of RxD Pin Active Edge Interrupt Flag (incoming RX -&amp;gt; start bit);&lt;BR /&gt;- the second one, because of Receive Data Register Full Flag interrupt (byte received);&lt;/P&gt;&lt;P&gt;- the third one, because of Idle Line Flag (10 consecutive 1's recognized after the previous stop bit);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So far all right: PTA1 stay 'high' in wait mode and 'low' in vlps mode. I checked with an oscilloscope and PTA1 stay high synchronously with RX traffic (10bit transmission + 1 bit for IDLE detection).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Let's come to problems.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I ported the implementation in my project. The same project may be executed on two different boards, which mount two different MCU:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- MK22FN512VLH12 (mask 0N50M)&lt;BR /&gt;- MK22FX512VMC12 (mask 3N03G)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My project, after system initialization, goes to SLEEP using VLPS as power mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;While it's in sleep, it'is receving asynchronously data from&amp;nbsp;a BT controller (TI CC2564) @ 57600 baudrate.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;All seems to work properly, except that randomly UART RX receive frame errors.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I exclude a problem with TI CC2564 because using WAIT power mode instead of VLPS frame errors are never received.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;There is also a big difference between the two MCU. For example, in 12h runtime the following frame errors were reported:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-&amp;nbsp;&lt;SPAN&gt;MK22FN512VLH12&amp;nbsp; -&amp;gt; 3638&lt;BR /&gt;-&amp;nbsp;MK22FX512VMC12 -&amp;gt; 293&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;The main difference is that FN is configured for run @ 72MHz (because of maximum core clock speed is 80MHz from datasheet), while FX @ 98MHz. Source clock for UARTs on both FN/FX boards is the bus clock (core clock divide by 2, so FN @ 36Mhz and FX @ 49MHz). Both boards operate using&amp;nbsp;FLL Engaged External (FEE): external crystal is 32KHz.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;From datasheet, the recovery time from VLPS -&amp;gt; RUN is:&lt;BR /&gt;&lt;BR /&gt;-&amp;nbsp;&lt;SPAN&gt;MK22FN512VLH12&amp;nbsp; -&amp;gt;&amp;nbsp;5.7us&lt;BR /&gt;-&amp;nbsp;MK22FX512VMC12 -&amp;gt; 4.4us&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;Both of them are below the half of baud period, so receiving data @ 57600 should not be a problem (by the way, I also tried running @ 38400 baudrate but frame errors happen the same but with minor frequency).&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;My questions are:&lt;BR /&gt;&lt;BR /&gt;1) what could cause these frame errors?&lt;BR /&gt;2) why&amp;nbsp;there is a so big difference with frame errors received between FN/FX?&lt;BR /&gt;3) are there any cases where recovery time from VLPS to RUN is above the max value reported from datasheet,&amp;nbsp;de facto&amp;nbsp;losing the first RX bit?&lt;BR /&gt;4) are there any cases where RX active edge interrupt may not be recognized if it happens &lt;SPAN&gt;synchronously&lt;SPAN&gt;&amp;nbsp;with the execution of WFI instruction?&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Any help / advice is welcome: these frame errors sometime force my system&amp;nbsp;to re-initialize the whole BT stack because it stucks.&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;&lt;BR /&gt;Alessandro&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Jul 2017 14:07:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-frame-error-receving-from-VLPS/m-p/668117#M41084</guid>
      <dc:creator>alessandromorni</dc:creator>
      <dc:date>2017-07-13T14:07:25Z</dc:date>
    </item>
    <item>
      <title>Re: UART frame error receving from VLPS</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-frame-error-receving-from-VLPS/m-p/668118#M41085</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;nothing at all? I'm still groping around in the dark, a&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;ny help / advice is welcome.&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Alessandro&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Jul 2017 12:20:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-frame-error-receving-from-VLPS/m-p/668118#M41085</guid>
      <dc:creator>alessandromorni</dc:creator>
      <dc:date>2017-07-27T12:20:38Z</dc:date>
    </item>
    <item>
      <title>Re: UART frame error receving from VLPS</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-frame-error-receving-from-VLPS/m-p/668119#M41086</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alessandro Morniroli&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have check your code, I couldn't see any problem in the code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;are there any cases where recovery time from VLPS to RUN is above the max value reported from datasheet,&amp;nbsp;de facto&amp;nbsp;losing the first RX bit?&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;As long as you have mentioned:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;(by the way, I also tried running @ 38400 baudrate but frame errors happen the same but with minor frequency).&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It could be that the problem is related with the first comment of mark in the post &lt;A href="https://community.nxp.com/thread/327741"&gt;Using Kinetis Low Power Stop Modes with unrestricted UART operation - a report&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;where he mentions that there is a problem with the wakeup time and the baud rate limit (where he mentioned that he doesn't see any problem with 57600).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you reduce your baud rate, for example, 9600, do errors still happened?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regardless of this, the problem is related only with the VLPS, as it is taking too much time to wakeup from VLPS to RUN mode, could you try with SMC_SetPowerModeStop (Stop mode), there should be too much difference.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Jorge Alcala&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Jul 2017 21:55:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-frame-error-receving-from-VLPS/m-p/668119#M41086</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2017-07-28T21:55:03Z</dc:date>
    </item>
    <item>
      <title>Re: UART frame error receving from VLPS</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-frame-error-receving-from-VLPS/m-p/668120#M41087</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thank you for the support.&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It could be that the problem is related with the first comment of mark in the post &lt;A _jive_internal="true" data-containerid="2019" data-containertype="14" data-content-finding="Community" data-objectid="327741" data-objecttype="1" href="https://community.nxp.com/thread/327741"&gt;Using Kinetis Low Power Stop Modes with unrestricted UART operation - a report&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;where he mentions that there is a problem with the wakeup time and the baud rate limit (where he mentioned that he doesn't see any problem with 57600).&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you reduce your baud rate, for example, 9600, do errors still happened?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;BR /&gt;I think that's correct: in fact the first byte @115200bps (in VLPS) is always lost because of frame error. I've tried also with 9600 and 19200, but errors still happen randomically.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;Jorge Antonio Alcala Vazquez ha scritto:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regardless of this, the problem is related only with the VLPS, as it is taking too much time to wakeup from VLPS to RUN mode, could you try with SMC_SetPowerModeStop (Stop mode), there should be too much difference.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Unfortunately, STOP mode is not allowed by our applications because of power consumption&lt;BR /&gt;&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/6825i68F1AFDC0FE5B9A8/image-size/large?v=v2&amp;amp;px=999" title="power.png" alt="power.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Aug 2017 07:11:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-frame-error-receving-from-VLPS/m-p/668120#M41087</guid>
      <dc:creator>alessandromorni</dc:creator>
      <dc:date>2017-08-01T07:11:52Z</dc:date>
    </item>
    <item>
      <title>Re: UART frame error receving from VLPS</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-frame-error-receving-from-VLPS/m-p/668121#M41088</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On the K64 with external oscillator it is quite fast/repeatable to wake from VLPS mode and so 57600Baud is reliable.&lt;/P&gt;&lt;P&gt;However it is dependent on clocks and clock sources, as well as exact parts used and there can be a spread in the time taken.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If possible to control the data used on the UART (protocol) one could always send some dummy characters that are just there to wake up the processor and allow it enough time to get back to a stable state before the message is interpreted.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Aug 2017 15:58:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-frame-error-receving-from-VLPS/m-p/668121#M41088</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2017-08-01T15:58:43Z</dc:date>
    </item>
  </channel>
</rss>