<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックAbsolute Placement in FlexNVM</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Absolute-Placement-in-FlexNVM/m-p/222512#M4099</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Using a TWRK40X256 with FlexNVM, set as data flash and EEPROM, I have a constant array that needs to be stored in FlexNVM at address 0x10008000.&amp;nbsp; I am able to place the array at the desired location and it downloads properly to that location.&amp;nbsp; However I also get a duplicate copy at address 0x10000000, which I do not want as that address is reserved for other data.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Why do I get this duplicate load at the start of FlexNVM?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 11 Jan 2013 16:15:19 GMT</pubDate>
    <dc:creator>nickg</dc:creator>
    <dc:date>2013-01-11T16:15:19Z</dc:date>
    <item>
      <title>Absolute Placement in FlexNVM</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Absolute-Placement-in-FlexNVM/m-p/222512#M4099</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Using a TWRK40X256 with FlexNVM, set as data flash and EEPROM, I have a constant array that needs to be stored in FlexNVM at address 0x10008000.&amp;nbsp; I am able to place the array at the desired location and it downloads properly to that location.&amp;nbsp; However I also get a duplicate copy at address 0x10000000, which I do not want as that address is reserved for other data.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Why do I get this duplicate load at the start of FlexNVM?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Jan 2013 16:15:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Absolute-Placement-in-FlexNVM/m-p/222512#M4099</guid>
      <dc:creator>nickg</dc:creator>
      <dc:date>2013-01-11T16:15:19Z</dc:date>
    </item>
    <item>
      <title>Re: Absolute Placement in FlexNVM</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Absolute-Placement-in-FlexNVM/m-p/222513#M4100</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Maybe it's because of the fact that when you use eeprom, FlexNVM becomes partially an EEPROM Backup (written in the documentation that this backup space should be more than 16x bigger than the eeprom area&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Jan 2013 12:52:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Absolute-Placement-in-FlexNVM/m-p/222513#M4100</guid>
      <dc:creator>mathieunavarro</dc:creator>
      <dc:date>2013-01-15T12:52:04Z</dc:date>
    </item>
    <item>
      <title>Re: Absolute Placement in FlexNVM</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Absolute-Placement-in-FlexNVM/m-p/222514#M4101</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Nick, was this assumption helpful for you to move on with your project? Let us know! :smileywink:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Jan 2013 23:10:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Absolute-Placement-in-FlexNVM/m-p/222514#M4101</guid>
      <dc:creator>Monica</dc:creator>
      <dc:date>2013-01-29T23:10:46Z</dc:date>
    </item>
  </channel>
</rss>