<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Is the SPI program provided by the FRDM-K66's SDK supposed to work?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-the-SPI-program-provided-by-the-FRDM-K66-s-SDK-supposed-to/m-p/665595#M40909</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Besides, I am&amp;nbsp;wondering if the issue would not come from the GPIO configuration in&amp;nbsp;BOARD_InitBootPins() function.&lt;/P&gt;&lt;P&gt;Because both channel are using&amp;nbsp;PCS0 as chip select.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 24 Jul 2017 08:47:36 GMT</pubDate>
    <dc:creator>benjaminheder</dc:creator>
    <dc:date>2017-07-24T08:47:36Z</dc:date>
    <item>
      <title>Is the SPI program provided by the FRDM-K66's SDK supposed to work?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-the-SPI-program-provided-by-the-FRDM-K66-s-SDK-supposed-to/m-p/665590#M40904</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working with MCUXpresso and I have an issue with the SPI program "dspi_interrupt_transfer" provided by the FRDM-K66's SDK.&lt;BR /&gt;Actually when I debug it and try to look inside the SPI0 and SPI1 registers these ones remain disabled in Memory -&amp;gt; Monitors Window.&lt;/P&gt;&lt;P&gt;Then I try with the SPI program&amp;nbsp;&lt;SPAN&gt;"dspi_polling_transfer" and once again it doesn't work.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Is there a bug in DSPI SDK examples?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Do you have any solution for this problem because&amp;nbsp;I run out of idea.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Best Regards&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Ben&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Jul 2017 08:38:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-the-SPI-program-provided-by-the-FRDM-K66-s-SDK-supposed-to/m-p/665590#M40904</guid>
      <dc:creator>benjaminheder</dc:creator>
      <dc:date>2017-07-12T08:38:55Z</dc:date>
    </item>
    <item>
      <title>Re: Is the SPI program provided by the FRDM-K66's SDK supposed to work?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-the-SPI-program-provided-by-the-FRDM-K66-s-SDK-supposed-to/m-p/665591#M40905</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Benjamin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As I have not FRDM-K66 board, I use FRDM-K64F to have a test for the exmple dspi_interrupt_transfer with the MCUExpresso tools and SDK, the example use SPI0 as master spi, use spi1 slave spi.&lt;/P&gt;&lt;P&gt;I can see the spi register value as the following screenshot.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/26303i7FEF234E4F7E69F0/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Jul 2017 03:33:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-the-SPI-program-provided-by-the-FRDM-K66-s-SDK-supposed-to/m-p/665591#M40905</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2017-07-18T03:33:34Z</dc:date>
    </item>
    <item>
      <title>Re: Is the SPI program provided by the FRDM-K66's SDK supposed to work?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-the-SPI-program-provided-by-the-FRDM-K66-s-SDK-supposed-to/m-p/665592#M40906</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Xiangjun,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help.&lt;/P&gt;&lt;P&gt;However it doesn't help me. It seems to be an IDE issue.&lt;/P&gt;&lt;P&gt;A new release of MCUXpresso has been brought and now allows to monitor only SPI0 (master).&lt;BR /&gt;But I&amp;nbsp;still can't monitor SPI1 (slave) with my own program and the SDK example.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this issue coming from the founder?&lt;/P&gt;&lt;P&gt;Do I have to connect SCK, CS, MISO, MOSI between both channels or it is not important?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ben&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Jul 2017 09:34:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-the-SPI-program-provided-by-the-FRDM-K66-s-SDK-supposed-to/m-p/665592#M40906</guid>
      <dc:creator>benjaminheder</dc:creator>
      <dc:date>2017-07-19T09:34:20Z</dc:date>
    </item>
    <item>
      <title>Re: Is the SPI program provided by the FRDM-K66's SDK supposed to work?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-the-SPI-program-provided-by-the-FRDM-K66-s-SDK-supposed-to/m-p/665593#M40907</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Benjamin,&lt;/P&gt;&lt;P&gt;If you can watch the SPI0 register, can not watch the SPI1 register, i think it is debugger issue of the MCUExpresso, it is not related whether you connect the SPI signals between SPI0 and SPI1.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Jul 2017 03:32:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-the-SPI-program-provided-by-the-FRDM-K66-s-SDK-supposed-to/m-p/665593#M40907</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2017-07-20T03:32:20Z</dc:date>
    </item>
    <item>
      <title>Re: Is the SPI program provided by the FRDM-K66's SDK supposed to work?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-the-SPI-program-provided-by-the-FRDM-K66-s-SDK-supposed-to/m-p/665594#M40908</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Xiangjun,&lt;/P&gt;&lt;P&gt;Thank you for these informations.&lt;/P&gt;&lt;P&gt;Do you know when this problem will be resolved on MCUXpresso?&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Ben&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Jul 2017 08:16:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-the-SPI-program-provided-by-the-FRDM-K66-s-SDK-supposed-to/m-p/665594#M40908</guid>
      <dc:creator>benjaminheder</dc:creator>
      <dc:date>2017-07-24T08:16:56Z</dc:date>
    </item>
    <item>
      <title>Re: Is the SPI program provided by the FRDM-K66's SDK supposed to work?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-the-SPI-program-provided-by-the-FRDM-K66-s-SDK-supposed-to/m-p/665595#M40909</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Besides, I am&amp;nbsp;wondering if the issue would not come from the GPIO configuration in&amp;nbsp;BOARD_InitBootPins() function.&lt;/P&gt;&lt;P&gt;Because both channel are using&amp;nbsp;PCS0 as chip select.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Jul 2017 08:47:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-the-SPI-program-provided-by-the-FRDM-K66-s-SDK-supposed-to/m-p/665595#M40909</guid>
      <dc:creator>benjaminheder</dc:creator>
      <dc:date>2017-07-24T08:47:36Z</dc:date>
    </item>
    <item>
      <title>Re: Is the SPI program provided by the FRDM-K66's SDK supposed to work?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-the-SPI-program-provided-by-the-FRDM-K66-s-SDK-supposed-to/m-p/665596#M40910</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Benjamin,&lt;/P&gt;&lt;P&gt;I do not think the issue comes from BOARD_InitBootPins() function, it is the debugger issue of MCUExpresso tools, because the MCUExpresso tools supports Kinetis just now.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Jul 2017 03:00:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-the-SPI-program-provided-by-the-FRDM-K66-s-SDK-supposed-to/m-p/665596#M40910</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2017-07-26T03:00:30Z</dc:date>
    </item>
    <item>
      <title>Re: Is the SPI program provided by the FRDM-K66's SDK supposed to work?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-the-SPI-program-provided-by-the-FRDM-K66-s-SDK-supposed-to/m-p/665597#M40911</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks a lot for the answer.&lt;BR /&gt;Maybe you should be able to answer to this question too?&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/457193"&gt;https://community.nxp.com/thread/457193&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Benjamin Heder&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Aug 2017 17:00:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-the-SPI-program-provided-by-the-FRDM-K66-s-SDK-supposed-to/m-p/665597#M40911</guid>
      <dc:creator>benjaminheder</dc:creator>
      <dc:date>2017-08-08T17:00:00Z</dc:date>
    </item>
  </channel>
</rss>