<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックKinetis micro controller internal flash</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-micro-controller-internal-flash/m-p/663986#M40810</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to build infrastructure for write/read small size data (around 1~2 KB) into the internal flash using&amp;nbsp;FRDM-K64F.&lt;/P&gt;&lt;P&gt;The write/read designated flash sectors&amp;nbsp;must not be over written&amp;nbsp;upon the OS&amp;nbsp;&amp;amp;&amp;nbsp;application binary flashing&lt;/P&gt;&lt;P&gt;1. Is there a&amp;nbsp;PC tool that can support flashing specific flash sectors? (for example not flashing the&amp;nbsp;last xx sectors)?&lt;/P&gt;&lt;P&gt;2. Is it possible to manage the internal flash (or part of it - for example the write/read area) as a file system?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks a lot,&lt;/P&gt;&lt;P&gt;Dotan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 29 Sep 2016 12:23:33 GMT</pubDate>
    <dc:creator>dotangoldberg</dc:creator>
    <dc:date>2016-09-29T12:23:33Z</dc:date>
    <item>
      <title>Kinetis micro controller internal flash</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-micro-controller-internal-flash/m-p/663986#M40810</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to build infrastructure for write/read small size data (around 1~2 KB) into the internal flash using&amp;nbsp;FRDM-K64F.&lt;/P&gt;&lt;P&gt;The write/read designated flash sectors&amp;nbsp;must not be over written&amp;nbsp;upon the OS&amp;nbsp;&amp;amp;&amp;nbsp;application binary flashing&lt;/P&gt;&lt;P&gt;1. Is there a&amp;nbsp;PC tool that can support flashing specific flash sectors? (for example not flashing the&amp;nbsp;last xx sectors)?&lt;/P&gt;&lt;P&gt;2. Is it possible to manage the internal flash (or part of it - for example the write/read area) as a file system?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks a lot,&lt;/P&gt;&lt;P&gt;Dotan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Sep 2016 12:23:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-micro-controller-internal-flash/m-p/663986#M40810</guid>
      <dc:creator>dotangoldberg</dc:creator>
      <dc:date>2016-09-29T12:23:33Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis micro controller internal flash</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-micro-controller-internal-flash/m-p/663987#M40811</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi dotan goldberg&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you are using P&amp;amp;Emicro interface to flash your device, you can used the advanced option. it gives you the ability to preserve FLASH ranges.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check the following post as reference.&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://mcuoneclipse.com/2015/04/16/updated-pe-gdb-server-for-eclipse-connectattach-and-advanced-flash-programming/" title="https://mcuoneclipse.com/2015/04/16/updated-pe-gdb-server-for-eclipse-connectattach-and-advanced-flash-programming/"&gt;https://mcuoneclipse.com/2015/04/16/updated-pe-gdb-server-for-eclipse-connectattach-and-advanced-flash-programming/&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this information help you.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jorge Alcala&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Oct 2016 21:15:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-micro-controller-internal-flash/m-p/663987#M40811</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2016-10-05T21:15:54Z</dc:date>
    </item>
  </channel>
</rss>