<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックQspi—flash</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Qspi-flash/m-p/663929#M40806</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;大家好，我想用KL81主控加载程序到Qspi-flash，工程上配置（开发环境：KEIL5.11或者KEIL5.23）寄存器FOPT EQU 0xBD、编写下载，硬件上PTB16~17接上串口，打开KinetisFlashTool工具发现通信不正常，提示：Error: Connect device failed(Error: Initial ping failure: Invalid packet type.).。用同样的方法在GCC开发环境上是可以通信的，并且能下载sb文件到Qspi—flash上去。请问下在KEIL环境上如何下载程序到Qspi-flash上去呢？恳请各位工程师的回答...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 18 Mar 2017 05:43:26 GMT</pubDate>
    <dc:creator>yingwufang</dc:creator>
    <dc:date>2017-03-18T05:43:26Z</dc:date>
    <item>
      <title>Qspi—flash</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Qspi-flash/m-p/663929#M40806</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;大家好，我想用KL81主控加载程序到Qspi-flash，工程上配置（开发环境：KEIL5.11或者KEIL5.23）寄存器FOPT EQU 0xBD、编写下载，硬件上PTB16~17接上串口，打开KinetisFlashTool工具发现通信不正常，提示：Error: Connect device failed(Error: Initial ping failure: Invalid packet type.).。用同样的方法在GCC开发环境上是可以通信的，并且能下载sb文件到Qspi—flash上去。请问下在KEIL环境上如何下载程序到Qspi-flash上去呢？恳请各位工程师的回答...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 18 Mar 2017 05:43:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Qspi-flash/m-p/663929#M40806</guid>
      <dc:creator>yingwufang</dc:creator>
      <dc:date>2017-03-18T05:43:26Z</dc:date>
    </item>
    <item>
      <title>Re: Qspi—flash</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Qspi-flash/m-p/663930#M40807</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi YINGWU FANG,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 从你描述中看，应该还是UART串口链接的问题，按道理如果连接正常是可以的。&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; 不知道你原来的程序配置是从ROM启动还是从FLASH启动，建议你直接按下NMI引脚，然后按下reset， 松开NMI， 松开reset，再试下。&lt;/P&gt;&lt;P&gt;我这边在同一个KL82板子上，试了PTC3，PTC4 以及PTB16，PTB17， 都能够连上。&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/16522iDE82DB69C10DEF4E/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;COM9是PTC3，PTC4， COM8是PTB16，PTB17。&lt;/P&gt;&lt;P&gt;所以还是先把UART连通，检查你的链接。&lt;/P&gt;&lt;P&gt;PTB16接PC TX&lt;/P&gt;&lt;P&gt;PTC17接PC RX。&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Mar 2017 06:39:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Qspi-flash/m-p/663930#M40807</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2017-03-21T06:39:34Z</dc:date>
    </item>
    <item>
      <title>Re: Qspi—flash</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Qspi-flash/m-p/663931#M40808</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI Kerry，&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;     感谢您的回复，此问题已经解决、原因是KEIL的Optimize被设置成 level3导致的。我想再请教您如下几个问题&lt;/P&gt;&lt;P&gt;1.我开发的产品分为boot和APP两个工程，boot放在internal flash，APP放在Qspi-flash，系统启动先在boot运行、检测到APP的存在就运行到Qspi-flash的代码，此种方法是否可行？&lt;/P&gt;&lt;P&gt;2.boot和APP都放在Qspi-flash，boot先通过bootloader装载、APP通过boot对QSPI-flash写的方式来装载（APP绕过bootloader而在boot上装载），系统启动时先在boot运行、检测到APP的存在跳转到APP，此种方法是否可行？&lt;/P&gt;&lt;P&gt;3.boot和APP都放在Qspi-flash，两者都通过bootloader装载，系统启动时先在boot运行、检测到APP的存在跳转到APP，此种方法是否可行？&lt;/P&gt;&lt;P&gt;4.装载程序到Qspi-flash，是不是一定要通过ROM bootloader？&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;   祝：生活愉快&lt;/P&gt;&lt;P&gt;        YINGWU FANG&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Mar 2017 00:54:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Qspi-flash/m-p/663931#M40808</guid>
      <dc:creator>yingwufang</dc:creator>
      <dc:date>2017-03-22T00:54:32Z</dc:date>
    </item>
    <item>
      <title>Re: Qspi—flash</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Qspi-flash/m-p/663932#M40809</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi YINGWU FANG,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; 1.2.3, 从原理上讲是可以实现的，不过目前还没有对应的应用给你参考，需要你自己去研究。&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; 4. 从ROM bootloader启动烧录到Qspi-flash毕竟我们的KBOOT2.0有对应的工具可以帮你烧录，否则就需要你自己想法烧录，然后再跳转了。&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Mar 2017 06:03:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Qspi-flash/m-p/663932#M40809</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2017-03-22T06:03:36Z</dc:date>
    </item>
  </channel>
</rss>