<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: Availability of OpenSDA standard or Example programs</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Availability-of-OpenSDA-standard-or-Example-programs/m-p/222104#M4078</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;pgo, thanks for the observations, we'll be analyzing that over.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 Feb 2013 19:56:54 GMT</pubDate>
    <dc:creator>Monica</dc:creator>
    <dc:date>2013-02-12T19:56:54Z</dc:date>
    <item>
      <title>Availability of OpenSDA standard or Example programs</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Availability-of-OpenSDA-standard-or-Example-programs/m-p/222101#M4075</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anyone know if there has then been any progress is releasing information about coding for the OpenSDA available in the 'Freedom' evaluation boards?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In particular any of the following would be useful:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;OpenSDA standard - A specification of the file format for the .SDA files used and how the information is loaded into the OpenSDA device.&amp;nbsp; Note - this is about the K20 device loaded with the OpenSDA not using the bootloader for the connected target.&lt;/LI&gt;&lt;LI&gt;Example projects.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have been unable to find either of the above but it is possible I'm looking in the wrong places :smileysad:.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Previous posting about this have indicated that the above would be soon available but it has been quite a while and AFAIK they are not available yet.&lt;/P&gt;&lt;P&gt;Looking at the P&amp;amp;E site only has OpenSDA applications.&lt;/P&gt;&lt;P&gt;The material on the ARM website only applies to CMSIS debugger interface and does not appear to cover actual OpenSDA loader.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any information would be appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Jan 2013 06:04:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Availability-of-OpenSDA-standard-or-Example-programs/m-p/222101#M4075</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2013-01-09T06:04:56Z</dc:date>
    </item>
    <item>
      <title>Re: Availability of OpenSDA standard or Example programs</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Availability-of-OpenSDA-standard-or-Example-programs/m-p/222102#M4076</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm afraid sins the OpenSDA application was developed by P&amp;amp;E Micro and therefore their intellectual property, only they can provide information related to that subject.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Feb 2013 22:02:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Availability-of-OpenSDA-standard-or-Example-programs/m-p/222102#M4076</guid>
      <dc:creator>apanecatl</dc:creator>
      <dc:date>2013-02-06T22:02:20Z</dc:date>
    </item>
    <item>
      <title>Re: Availability of OpenSDA standard or Example programs</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Availability-of-OpenSDA-standard-or-Example-programs/m-p/222103#M4077</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pedro,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes there have been a couple of other posting indicating that this is the situation.&amp;nbsp; This is unfortunate and compares poorly with similar ideas from other manufacturers e.g.STMicro.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could I suggest that Freescale change the name of the application as it is in no way "Open".&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Source is not available&lt;/LI&gt;&lt;LI&gt;Official specification of interface is not available.&lt;/LI&gt;&lt;LI&gt;Provided implementations are secured and mass erase disabled.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Not much 'Open' in that list :smileyhappy:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Freescale should also update their documentation which is quite misleading on this aspect.&amp;nbsp; From the OpenSDA USer Guide:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;"OpenSDA is an open-standard serial and debug adapter.&lt;/STRONG&gt;"&amp;nbsp; I'm unsure what this is meant to mean in light of your posting.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The web page also refers to:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;"Open-source data logging application provides an example for customer, partner and enthusiast development on the OpenSDA circuit"&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I have not been able to find this and it seems incompatible with your information.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However there has been some information posted that may allows others to use the implementations provided on the Freedom boards.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/311676"&gt;Basic OpenSDA Project&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is also possible to use alternative (open source) debugger interfaces with the Freedom boards.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/311643"&gt;Re: Replaced Freedom KL25 - now OpenSDA doesn't work&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Feb 2013 06:10:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Availability-of-OpenSDA-standard-or-Example-programs/m-p/222103#M4077</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2013-02-07T06:10:59Z</dc:date>
    </item>
    <item>
      <title>Re: Availability of OpenSDA standard or Example programs</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Availability-of-OpenSDA-standard-or-Example-programs/m-p/222104#M4078</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;pgo, thanks for the observations, we'll be analyzing that over.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Feb 2013 19:56:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Availability-of-OpenSDA-standard-or-Example-programs/m-p/222104#M4078</guid>
      <dc:creator>Monica</dc:creator>
      <dc:date>2013-02-12T19:56:54Z</dc:date>
    </item>
    <item>
      <title>Re: Availability of OpenSDA standard or Example programs</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Availability-of-OpenSDA-standard-or-Example-programs/m-p/222105#M4079</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi pgo,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry about that. Thanks a lot for your efforts on OpenSDA and more related &lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;observations&lt;/SPAN&gt; are hoped in the future.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Aug 2013 11:08:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Availability-of-OpenSDA-standard-or-Example-programs/m-p/222105#M4079</guid>
      <dc:creator>calvinji</dc:creator>
      <dc:date>2013-08-12T11:08:15Z</dc:date>
    </item>
    <item>
      <title>Re: Availability of OpenSDA standard or Example programs</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Availability-of-OpenSDA-standard-or-Example-programs/m-p/222106#M4080</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;See development of OpenSDA v2 in&amp;nbsp;&lt;A class="link-titled" href="https://github.com/mbedmicro/DAPLink" title="https://github.com/mbedmicro/DAPLink"&gt;GitHub - mbedmicro/DAPLink&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 15 Jul 2017 13:31:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Availability-of-OpenSDA-standard-or-Example-programs/m-p/222106#M4080</guid>
      <dc:creator>hmyoong</dc:creator>
      <dc:date>2017-07-15T13:31:01Z</dc:date>
    </item>
  </channel>
</rss>