<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Custom board with kl26z: internal flash programming (128k) via mini usb  in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Custom-board-with-kl26z-internal-flash-programming-128k-via-mini/m-p/663463#M40762</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using a custom board with kl26z and 128k internal flash. I would like to know if&lt;/P&gt;&lt;P&gt;there is a way to program internal flash in production phase without using jtag/swd interface. I thought to use mini usb&lt;/P&gt;&lt;P&gt;connected to PC usb port&amp;nbsp; and to write a program reading&amp;nbsp;&amp;nbsp; flash images data from miniusb serial port and&amp;nbsp; erase /program all internal flash.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 10 Apr 2017 10:05:58 GMT</pubDate>
    <dc:creator>protagora27prot</dc:creator>
    <dc:date>2017-04-10T10:05:58Z</dc:date>
    <item>
      <title>Custom board with kl26z: internal flash programming (128k) via mini usb</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Custom-board-with-kl26z-internal-flash-programming-128k-via-mini/m-p/663463#M40762</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using a custom board with kl26z and 128k internal flash. I would like to know if&lt;/P&gt;&lt;P&gt;there is a way to program internal flash in production phase without using jtag/swd interface. I thought to use mini usb&lt;/P&gt;&lt;P&gt;connected to PC usb port&amp;nbsp; and to write a program reading&amp;nbsp;&amp;nbsp; flash images data from miniusb serial port and&amp;nbsp; erase /program all internal flash.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Apr 2017 10:05:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Custom-board-with-kl26z-internal-flash-programming-128k-via-mini/m-p/663463#M40762</guid>
      <dc:creator>protagora27prot</dc:creator>
      <dc:date>2017-04-10T10:05:58Z</dc:date>
    </item>
    <item>
      <title>Re: Custom board with kl26z: internal flash programming (128k) via mini usb</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Custom-board-with-kl26z-internal-flash-programming-128k-via-mini/m-p/663464#M40763</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If you want to use the USB to program the device, first you need to load on the device a bootloader.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Vicente&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Apr 2017 21:20:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Custom-board-with-kl26z-internal-flash-programming-128k-via-mini/m-p/663464#M40763</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2017-04-11T21:20:35Z</dc:date>
    </item>
    <item>
      <title>Re: Custom board with kl26z: internal flash programming (128k) via mini usb</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Custom-board-with-kl26z-internal-flash-programming-128k-via-mini/m-p/663465#M40764</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;I have almost the same question("I would like to know if there is a way to program internal flash in production phase without using jtag/swd interface."&lt;A _jive_internal="true" data-content-finding="Community" data-userid="263680" data-username="protagora27protagora27" href="https://community.nxp.com/people/protagora27protagora27" style="color: #5e89c1; background-color: #ffffff; border: 0px; font-weight: 600; text-decoration: underline; font-size: 11.9994px;"&gt;protagora27 protagora27&lt;/A&gt;), I also trying to program a custom board with KL27Z256V via USB &lt;STRONG&gt;not&lt;/STRONG&gt; OpenSDA-USB, I also try to connect to the board with "KINETIS FLASH TOOL", but can achieve the connection between PC and board via USB; via OpenSDA-USB the connection was asserted.&lt;/P&gt;&lt;P&gt;I also try with FRDM-KL43&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/26763i40817C4E74BC2E3C/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_6.png" alt="pastedImage_6.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/kerryzhou"&gt;kerryzhou&lt;/A&gt;‌&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Jul 2017 16:00:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Custom-board-with-kl26z-internal-flash-programming-128k-via-mini/m-p/663465#M40764</guid>
      <dc:creator>isaacromero</dc:creator>
      <dc:date>2017-07-21T16:00:41Z</dc:date>
    </item>
    <item>
      <title>Re: Custom board with kl26z: internal flash programming (128k) via mini usb</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Custom-board-with-kl26z-internal-flash-programming-128k-via-mini/m-p/663466#M40765</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Isaac Romero,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Your question is not the same question as the top post, next time you can create your own question post directly.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Because KL26 don't have the ROM bootloader, then the customer need to download the flash bootloader with USB bootloader function in the KL26 at first.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; But you are using KL27 chip, this chip have the on chip ROM bootloader, it already contains the USB ROM bootloader function, so you can use the HID to download the code with the Kinetis flash tool. Your own board can refer to the FRDM-KL43 if you want to download the APP code with USB ROM bootloader.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; If you still have further question, please create the new post and let me know, I will reply you directly in your own post.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Thanks a lot!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Jul 2017 02:09:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Custom-board-with-kl26z-internal-flash-programming-128k-via-mini/m-p/663466#M40765</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2017-07-24T02:09:14Z</dc:date>
    </item>
  </channel>
</rss>