<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Embedded gdbserver for K22 controlled via UART</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Embedded-gdbserver-for-K22-controlled-via-UART/m-p/662801#M40698</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'd like to be able to debug my FreeRTOS app running on a K22, but the connectivity of the K22 is such that the JTAG/SWD are not available. However, a UART is available, so the hope was that a gdbserver could be compiled into the FreeRTOS app and activated with a specific UART sequence, in order to set breakpoints, inspect variables, etc. Does something like this exist for the ARM Cortex M4 that runs on the K22?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 01 Feb 2017 22:22:23 GMT</pubDate>
    <dc:creator>gsosnow</dc:creator>
    <dc:date>2017-02-01T22:22:23Z</dc:date>
    <item>
      <title>Embedded gdbserver for K22 controlled via UART</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Embedded-gdbserver-for-K22-controlled-via-UART/m-p/662801#M40698</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'd like to be able to debug my FreeRTOS app running on a K22, but the connectivity of the K22 is such that the JTAG/SWD are not available. However, a UART is available, so the hope was that a gdbserver could be compiled into the FreeRTOS app and activated with a specific UART sequence, in order to set breakpoints, inspect variables, etc. Does something like this exist for the ARM Cortex M4 that runs on the K22?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Feb 2017 22:22:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Embedded-gdbserver-for-K22-controlled-via-UART/m-p/662801#M40698</guid>
      <dc:creator>gsosnow</dc:creator>
      <dc:date>2017-02-01T22:22:23Z</dc:date>
    </item>
    <item>
      <title>Re: Embedded gdbserver for K22 controlled via UART</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Embedded-gdbserver-for-K22-controlled-via-UART/m-p/662802#M40699</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry we do not have the application &amp;amp; sample as you would like to. Anyway, there has a quite useful reference for this issue you may find at:&lt;A class="link-titled" href="https://mcuoneclipse.com/2016/06/13/adding-freertos-thread-awareness-to-gdb-and-eclipse/" title="https://mcuoneclipse.com/2016/06/13/adding-freertos-thread-awareness-to-gdb-and-eclipse/"&gt;Adding FreeRTOS Thread Awareness to GDB and Eclipse | MCU on Eclipse&lt;/A&gt; . Hope it will be helpful.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Feb 2017 09:06:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Embedded-gdbserver-for-K22-controlled-via-UART/m-p/662802#M40699</guid>
      <dc:creator>miduo</dc:creator>
      <dc:date>2017-02-10T09:06:17Z</dc:date>
    </item>
  </channel>
</rss>