<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックKinetis UART: using DMA and ISR possible?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-UART-using-DMA-and-ISR-possible/m-p/661274#M40601</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Kinetisis K64F. I'd like to send characters out the UART using DMA, and receive using an ISR. I configured a DMA channel to send to the UART (triggered from the URT TRE signal). I set TDMAS, which says "&lt;EM&gt;Configures the transmit data register empty flag, S1[TDRE], to generate interrupt or DMA requests if C2[TIE] is set&lt;/EM&gt;". So I set TIE as well, but now I never get the DMA transfer, but the RX_TX ISR is called repeatedly...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it possible to send with DMA while receiving with an ISR? If so what bits need be set?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance for any help,&lt;BR /&gt;Best Regards, Dave&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 09 Dec 2016 19:32:09 GMT</pubDate>
    <dc:creator>davenadler</dc:creator>
    <dc:date>2016-12-09T19:32:09Z</dc:date>
    <item>
      <title>Kinetis UART: using DMA and ISR possible?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-UART-using-DMA-and-ISR-possible/m-p/661274#M40601</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Kinetisis K64F. I'd like to send characters out the UART using DMA, and receive using an ISR. I configured a DMA channel to send to the UART (triggered from the URT TRE signal). I set TDMAS, which says "&lt;EM&gt;Configures the transmit data register empty flag, S1[TDRE], to generate interrupt or DMA requests if C2[TIE] is set&lt;/EM&gt;". So I set TIE as well, but now I never get the DMA transfer, but the RX_TX ISR is called repeatedly...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it possible to send with DMA while receiving with an ISR? If so what bits need be set?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance for any help,&lt;BR /&gt;Best Regards, Dave&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Dec 2016 19:32:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-UART-using-DMA-and-ISR-possible/m-p/661274#M40601</guid>
      <dc:creator>davenadler</dc:creator>
      <dc:date>2016-12-09T19:32:09Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis UART: using DMA and ISR possible?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-UART-using-DMA-and-ISR-possible/m-p/661275#M40602</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, it works just fine if you set TDMAS as I intended and not TCDMAS as I typed the first time, aaarrggg...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Dec 2016 22:00:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-UART-using-DMA-and-ISR-possible/m-p/661275#M40602</guid>
      <dc:creator>davenadler</dc:creator>
      <dc:date>2016-12-09T22:00:13Z</dc:date>
    </item>
  </channel>
</rss>