<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic GenericSPI: No inherited component assigned in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GenericSPI-No-inherited-component-assigned/m-p/661038#M40582</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to configure the&amp;nbsp;SPI1 bus using the FRDM-K22F. The PE component GenericSPI gives an error when added to the design: No Inherited Component Assigned. The SPI Channel dropdown does not contain any values.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Configuring the SPIMaster_LDD component seems to work fine. I've already configured the SPI1 pins in the PinSettings component.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Why can't I configure the GenericSPI component? Is there something I need to do first?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Feb 2017 21:41:22 GMT</pubDate>
    <dc:creator>asfarley</dc:creator>
    <dc:date>2017-02-22T21:41:22Z</dc:date>
    <item>
      <title>GenericSPI: No inherited component assigned</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GenericSPI-No-inherited-component-assigned/m-p/661038#M40582</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to configure the&amp;nbsp;SPI1 bus using the FRDM-K22F. The PE component GenericSPI gives an error when added to the design: No Inherited Component Assigned. The SPI Channel dropdown does not contain any values.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Configuring the SPIMaster_LDD component seems to work fine. I've already configured the SPI1 pins in the PinSettings component.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Why can't I configure the GenericSPI component? Is there something I need to do first?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Feb 2017 21:41:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/GenericSPI-No-inherited-component-assigned/m-p/661038#M40582</guid>
      <dc:creator>asfarley</dc:creator>
      <dc:date>2017-02-22T21:41:22Z</dc:date>
    </item>
    <item>
      <title>Re: GenericSPI: No inherited component assigned</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GenericSPI-No-inherited-component-assigned/m-p/661039#M40583</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alexander,&lt;/P&gt;&lt;P&gt;The 'GenericSPI' component is for legacy HCS08 and ColdFire devices, and the 'SPI channel' points to their Init_SPIxxx component. So it is not applicable for Kinetis (as the API is different). The documentation for the component was not clear abou this (I appologize!), so I have updated it.&lt;/P&gt;&lt;P&gt;If you want to use a software (bit banging) SPI implementation, you could use the GenericSWSPI too:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/13666iFEF38CD0816B62AA/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Feb 2017 07:16:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/GenericSPI-No-inherited-component-assigned/m-p/661039#M40583</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2017-02-23T07:16:38Z</dc:date>
    </item>
  </channel>
</rss>