<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: ADC0_DP3 drawing more current than ADC1_SE5a in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC0-DP3-drawing-more-current-than-ADC1-SE5a/m-p/660999#M40581</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;Alexander,&lt;/P&gt;&lt;P&gt;Please pay attation to the hardware connected to these two pins on FRDM-K22F board.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/14068iCF911ADBD63C2518/image-size/large?v=v2&amp;amp;px=999" title="ADC1_SE5a.png" alt="ADC1_SE5a.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/14111i57204501768D55BC/image-size/large?v=v2&amp;amp;px=999" title="ADC0_DP3.png" alt="ADC0_DP3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 24 Feb 2017 02:55:08 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2017-02-24T02:55:08Z</dc:date>
    <item>
      <title>ADC0_DP3 drawing more current than ADC1_SE5a</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC0-DP3-drawing-more-current-than-ADC1-SE5a/m-p/660998#M40580</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using a FRDM-K22F with two pins configured as ADC inputs using Processor Expert. I've stuck with the default settings (longest conversion time, low-power not checked, high-speed not checked, single-ended mode, sharing not checked).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm testing a 5V-output sensor through a (50%) resistor divider which should give a voltage swing between 0-2.5V at the ADC input. While ADC1_SE5a seems fine (readings agree with a multimeter, etc) the ADC0_DP3 input seems to be drawing a significant amount of current, despite being configured in the same way as ADC1_SE5a.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When the sensor is outputting 4.7V, the resistor divider gives about 2.3V through the divider if it's not connected to any ADC inputs. If I wire it to ADC1_SE5a, I still get 2.3V when sampling. If I wire the 2.3V node to ADC0_DP3, it gets pulled down to .9V.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It appears that the resistor divider I'm using creates a sensor output impedance which is too high for the &lt;SPAN&gt;ADC0_DP3&amp;nbsp;&lt;/SPAN&gt;input impedance.&amp;nbsp;Why is&amp;nbsp;&lt;SPAN&gt;ADC1_SE5a not having the same issues?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;ADC0_DP3 gives reasonable readings using a low-impedance source (power rails or gnd) so it's not just a conversion/scaling issue. If ADC1 was sampling from more than 1 channel this could be caused by the inrush current when the channel switches but since it's only connected to 1 channel, this probably isn't the explanation.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Feb 2017 21:37:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC0-DP3-drawing-more-current-than-ADC1-SE5a/m-p/660998#M40580</guid>
      <dc:creator>asfarley</dc:creator>
      <dc:date>2017-02-22T21:37:40Z</dc:date>
    </item>
    <item>
      <title>Re: ADC0_DP3 drawing more current than ADC1_SE5a</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC0-DP3-drawing-more-current-than-ADC1-SE5a/m-p/660999#M40581</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;Alexander,&lt;/P&gt;&lt;P&gt;Please pay attation to the hardware connected to these two pins on FRDM-K22F board.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/14068iCF911ADBD63C2518/image-size/large?v=v2&amp;amp;px=999" title="ADC1_SE5a.png" alt="ADC1_SE5a.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/14111i57204501768D55BC/image-size/large?v=v2&amp;amp;px=999" title="ADC0_DP3.png" alt="ADC0_DP3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Feb 2017 02:55:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC0-DP3-drawing-more-current-than-ADC1-SE5a/m-p/660999#M40581</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2017-02-24T02:55:08Z</dc:date>
    </item>
  </channel>
</rss>