<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Programming the flash config field after a SWD mass erase.</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Programming-the-flash-config-field-after-a-SWD-mass-erase/m-p/660499#M40556</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Andrew Parlane,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; The CAUTION is correct, it is not only the MCU feature, it is the flash feature.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; If you want to program the flash, you must erase it at first. If the flash is programmed before, and you don't do the flash erase, just program it directly, your program won't be success.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; The flash configuration filed also meet this requirement. If you want to modify the data, you also need to erase it at first, then write the flash to the data which you want.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;If you still have question, please let me know!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 17 Mar 2017 08:17:11 GMT</pubDate>
    <dc:creator>kerryzhou</dc:creator>
    <dc:date>2017-03-17T08:17:11Z</dc:date>
    <item>
      <title>Programming the flash config field after a SWD mass erase.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Programming-the-flash-config-field-after-a-SWD-mass-erase/m-p/660498#M40555</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm looking specifically at a K66F.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When you use the MDM-AP to mass erase the chip. It erases flash to all 1s, except for the security bit in the flash config field. This is what I see in practice, and what I read in the&amp;nbsp;Production Flash Programming Best Practices for Kinetis K- and L-series MCUs PDF here:&amp;nbsp;&lt;A class="link-titled" href="http://cache.nxp.com/assets/documents/data/en/application-notes/AN4835.pdf" title="http://cache.nxp.com/assets/documents/data/en/application-notes/AN4835.pdf"&gt;http://cache.nxp.com/assets/documents/data/en/application-notes/AN4835.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However in the K66 reference manual in 32.4.12.8 "Program Section command", it states:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;CAUTION&lt;BR /&gt;A flash memory location must be in the erased state before&lt;BR /&gt;being programmed. Cumulative programming of bits (back-to-&lt;BR /&gt;back program operations without an intervening erase) within a&lt;BR /&gt;flash memory location is not allowed. Re-programming of&lt;BR /&gt;existing 0s to 0 is not allowed as this overstresses the device.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So how does this work for the flash config field where the security bit is set to 0 during a mass erase.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do I just ignore this caution for this bit, and issue a program section command as normal? Or is it better to run a sector erase first to actually erase that bit?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When it says reprogramming of existing 0s to 0 is not allowed. Does that mean the program section command will fail (it doesn't in the FCF case, and I haven't tried it in any other cases).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Mar 2017 20:53:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Programming-the-flash-config-field-after-a-SWD-mass-erase/m-p/660498#M40555</guid>
      <dc:creator>andrewparlane2</dc:creator>
      <dc:date>2017-03-16T20:53:42Z</dc:date>
    </item>
    <item>
      <title>Re: Programming the flash config field after a SWD mass erase.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Programming-the-flash-config-field-after-a-SWD-mass-erase/m-p/660499#M40556</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Andrew Parlane,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; The CAUTION is correct, it is not only the MCU feature, it is the flash feature.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; If you want to program the flash, you must erase it at first. If the flash is programmed before, and you don't do the flash erase, just program it directly, your program won't be success.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; The flash configuration filed also meet this requirement. If you want to modify the data, you also need to erase it at first, then write the flash to the data which you want.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;If you still have question, please let me know!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Mar 2017 08:17:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Programming-the-flash-config-field-after-a-SWD-mass-erase/m-p/660499#M40556</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2017-03-17T08:17:11Z</dc:date>
    </item>
  </channel>
</rss>