<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: FRDM-K82 using OpenSDA</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K82-using-OpenSDA/m-p/660319#M40521</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Eric&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, I tried that version.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think that the problem is that the FRDM-K82F (and other FRDM boards) are delivered with mbed bootloaders. These show the disk space (also in DOS) as 96k in size. The P&amp;amp;E MSD + Debug application is 200k in size and so can't be copied (also not in DOS). I do have a suspicion that the SDA files are also code in some way and can only be loaded if the P&amp;amp;E Bootloaer is installed.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I had the same problem with other FRDM boards such as the FRDM-K64F but P&amp;amp;E Micro also has a debug-only ".bin" in the package for that the board which can be loaded and is adequate for some debugging (but misses a VCOM and USB-MSD). Therefore I tend to have multiple boards - one with the mbed (which does VCOM and USB-MSD but can't debug) and one with P&amp;amp;E in case I need to quickly do some low level debugging.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately I don't know where to get a new bootloader that will need to be loaded via JTAG first that will then allow a version to be loaded that will work with Win 10 and also allow debugging.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems that the mbed FRDM-K82F support is very half-hearted - the link on the boot loader leads to a non-existent ARM page - they don't even have anything on the official web site about the board (no new version that corrects the Win 10 issue, whereas FRDM-K22F and FRDM-K64F do) yet the FRDM-K82F, is a year or so old, is delivered with their loader which doesn't actually work (just to copy form Win 7) and doesn't allow corrections....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have installed a secondary boot loader with USB-MSD and CDC so that&amp;nbsp; can basically work but will probably need to fall-back on a HW Jtag method in case of specific debugging requirements - or use the TWR-K82F board instead.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There still seems to be be quite a mess with these tools - each time losing several hours to do a couple of simple checks ;-(&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 03 Feb 2017 19:08:10 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2017-02-03T19:08:10Z</dc:date>
    <item>
      <title>FRDM-K82 using OpenSDA</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K82-using-OpenSDA/m-p/660313#M40515</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="margin: 0cm 0cm 10pt;"&gt;&lt;SPAN style="color: #000000; font-family: Calibri; font-size: medium;"&gt;Few months ego I have seen reports about possible damage when using FRDM-K82F OpenSDA Firmware in windows 10 environment. &lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0cm 0cm 10pt;"&gt;&lt;SPAN style="color: #000000; font-family: Calibri; font-size: medium;"&gt;My question is if the problems still exists or has been solved.&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0cm 0cm 10pt;"&gt;&lt;SPAN style="color: #000000; font-family: Calibri; font-size: medium;"&gt;Tx&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0cm 0cm 10pt;"&gt;&lt;SPAN style="color: #000000; font-family: Calibri; font-size: medium;"&gt;Shaul&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Dec 2016 20:27:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K82-using-OpenSDA/m-p/660313#M40515</guid>
      <dc:creator>shauldorf</dc:creator>
      <dc:date>2016-12-08T20:27:38Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K82 using OpenSDA</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K82-using-OpenSDA/m-p/660314#M40516</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi shaul dorf,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; This issue will be solved in the bootloader reversion opensda v2.2.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Now, you can try to refer to this post:&lt;/P&gt;&lt;P&gt;&lt;A href="https://mcuoneclipse.com/2016/06/26/how-to-recover-the-opensda-v2-x-bootloader/"&gt;https://mcuoneclipse.com/2016/06/26/how-to-recover-the-opensda-v2-x-bootloader/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; And use the beta opensda v2.2 on your side:&lt;/P&gt;&lt;P&gt;&lt;A href="https://developer.mbed.org/questions/68997/How-to-recover-FRDM-K22F/#answer10413"&gt;https://developer.mbed.org/questions/68997/How-to-recover-FRDM-K22F/#answer10413&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Kerry&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Dec 2016 03:23:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K82-using-OpenSDA/m-p/660314#M40516</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2016-12-12T03:23:17Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K82 using OpenSDA</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K82-using-OpenSDA/m-p/660315#M40517</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="margin: 0cm 0cm 10pt;"&gt;Thanks&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Is there any schedule for OpenSDA c2.2 new version&lt;/LI&gt;&lt;LI style="color: #000000; font-size: 11pt;"&gt;What is the status of |PEMicro and J-Link, is it safe to use them?&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Shaul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Dec 2016 16:09:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K82-using-OpenSDA/m-p/660315#M40517</guid>
      <dc:creator>shauldorf</dc:creator>
      <dc:date>2016-12-12T16:09:40Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K82 using OpenSDA</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K82-using-OpenSDA/m-p/660316#M40518</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Shaul dorf,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Please refer to this post:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-330935"&gt;Freedom OpenSDA Firmware Issues Reported on Windows 10&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The schedule is not given out, if I get the update information, will let you know.&lt;/P&gt;&lt;P&gt;You can use the PEMicro and JLINK, it is support the win10 now, but just as suggest, you need to replace the default CMSIS-DAP application with a Segger JLink or P&amp;amp;E OpenSDA application before using a Windows 10 computer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Dec 2016 02:38:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K82-using-OpenSDA/m-p/660316#M40518</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2016-12-13T02:38:38Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K82 using OpenSDA</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K82-using-OpenSDA/m-p/660317#M40519</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am wondering how to use the P&amp;amp;E Micro version so that it would be possible to debug on the FRDM-K82F board?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I try to load the P&amp;amp;E version (the newest is MSD-DEBUG-FRDM-K82F_Pemicro_v118.SDA) it just reports that there is not enough space on the disk to copy it. P&amp;amp;E has just debugger versions (no MSD) for FRDM-K22 and FRDM-K64 which work but not such for the FRDM-K82.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Pre-loaded mbed version allows copying files to the board from Win 7 but loses the file when connected to Win 10. It doesn't support debugging and doesn't offer a VCOM serial port. At mbed there is no mention of support for the board and no new versions found.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any ideas how to work though what looks like a availability of working support?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Feb 2017 16:44:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K82-using-OpenSDA/m-p/660317#M40519</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2017-02-03T16:44:37Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K82 using OpenSDA</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K82-using-OpenSDA/m-p/660318#M40520</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mark,&lt;/P&gt;&lt;P&gt;I don't have a K82F, but are you using the version from 2017_01_31 (&lt;A class="link-titled" href="http://www.pemicro.com/opensda/" title="http://www.pemicro.com/opensda/"&gt;P&amp;amp;E Microcomputer Systems: Over 30 years as an Industry leader in Embedded Systems Development Tools, debug probes, and …&lt;/A&gt;&amp;nbsp;)?:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/12923iD861395F0114C867/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I saw errors about 'not enough space' in combination with virus scanners or some 'MSD indexing devices'. Best if you copy the .SDA file from a DOS prompt.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Feb 2017 16:59:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K82-using-OpenSDA/m-p/660318#M40520</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2017-02-03T16:59:04Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K82 using OpenSDA</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K82-using-OpenSDA/m-p/660319#M40521</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Eric&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, I tried that version.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think that the problem is that the FRDM-K82F (and other FRDM boards) are delivered with mbed bootloaders. These show the disk space (also in DOS) as 96k in size. The P&amp;amp;E MSD + Debug application is 200k in size and so can't be copied (also not in DOS). I do have a suspicion that the SDA files are also code in some way and can only be loaded if the P&amp;amp;E Bootloaer is installed.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I had the same problem with other FRDM boards such as the FRDM-K64F but P&amp;amp;E Micro also has a debug-only ".bin" in the package for that the board which can be loaded and is adequate for some debugging (but misses a VCOM and USB-MSD). Therefore I tend to have multiple boards - one with the mbed (which does VCOM and USB-MSD but can't debug) and one with P&amp;amp;E in case I need to quickly do some low level debugging.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately I don't know where to get a new bootloader that will need to be loaded via JTAG first that will then allow a version to be loaded that will work with Win 10 and also allow debugging.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems that the mbed FRDM-K82F support is very half-hearted - the link on the boot loader leads to a non-existent ARM page - they don't even have anything on the official web site about the board (no new version that corrects the Win 10 issue, whereas FRDM-K22F and FRDM-K64F do) yet the FRDM-K82F, is a year or so old, is delivered with their loader which doesn't actually work (just to copy form Win 7) and doesn't allow corrections....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have installed a secondary boot loader with USB-MSD and CDC so that&amp;nbsp; can basically work but will probably need to fall-back on a HW Jtag method in case of specific debugging requirements - or use the TWR-K82F board instead.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There still seems to be be quite a mess with these tools - each time losing several hours to do a couple of simple checks ;-(&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Feb 2017 19:08:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K82-using-OpenSDA/m-p/660319#M40521</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2017-02-03T19:08:10Z</dc:date>
    </item>
  </channel>
</rss>