<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: KL8x: Universal Multilink: Breakpoints in QSPI</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL8x-Universal-Multilink-Breakpoints-in-QSPI/m-p/660192#M40506</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for your response.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I did ask P&amp;amp;E and&amp;nbsp;got the following response:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;The Cortex M0, M3, and M4 cannot set hardware breakpoints at addresses higher than 0x1000_0000.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;I guess that means, that they are not able to set breakpoints in the QSPI.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As for the J-Link OpenSDA: The paragraph you cited is a bullet point under&amp;nbsp;&lt;/P&gt;&lt;BLOCKQUOTE class="jive-quote"&gt;The firmware that makes the OpenSDA platform J-Link compatible has some limitations in contrast to an original, industry leading SEGGER J-Link:&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I know that the SEGGER J-Link&amp;nbsp;claims to be able to&amp;nbsp;&lt;SPAN&gt;set breakpoints in the QSPI, but as it's more expensive I&amp;nbsp;wanted to check-out the alternatives. However, it looks like&amp;nbsp;there are&amp;nbsp;none.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 28 Oct 2016 10:00:32 GMT</pubDate>
    <dc:creator>konradgräfe</dc:creator>
    <dc:date>2016-10-28T10:00:32Z</dc:date>
    <item>
      <title>KL8x: Universal Multilink: Breakpoints in QSPI</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL8x-Universal-Multilink-Breakpoints-in-QSPI/m-p/660190#M40504</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE&gt;I am on a project with the Freescale MKL82Z128VMC7 SDK. As my software grew,
I hit the limitations of the internal flash and therefore moved it to run
from external (QSPI) flash.

Currently I am using the OpenSDA with J-Link firmware which cannot set
breakpoints within the QSPI address space. Is the Universal Multilink (or Universal
Multilink FX) probe able to set breakpoints within the QSPI flash?

Regards,
Konrad Gräfe&lt;/PRE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Oct 2016 16:32:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL8x-Universal-Multilink-Breakpoints-in-QSPI/m-p/660190#M40504</guid>
      <dc:creator>konradgräfe</dc:creator>
      <dc:date>2016-10-21T16:32:39Z</dc:date>
    </item>
    <item>
      <title>Re: KL8x: Universal Multilink: Breakpoints in QSPI</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL8x-Universal-Multilink-Breakpoints-in-QSPI/m-p/660191#M40505</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regarding this issue, I had double checked the segger. See below:&lt;/P&gt;&lt;P&gt;&lt;A class="jivelink10" href="https://www.segger.com/opensda.html" title="https://www.segger.com/opensda.html"&gt;https://www.segger.com/opensda.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;It mentioned:&amp;nbsp; Unlimited breakpoints in flash available for evaluation only. But yes, I really not sure if this work for the QSPI flash. You may contact segger directly. Anyway, I am sure that the J-Link debug probe itself supporting the QSPI flash breakpoint: &lt;A class="jivelink12" href="https://www.segger.com/jlink-unlimited-flash-breakpoints.html" title="https://www.segger.com/jlink-unlimited-flash-breakpoints.html"&gt;https://www.segger.com/jlink-unlimited-flash-breakpoints.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As for the Multilink FX, yes, it is support the QSPI flash programming, and as for the breakpoint, you should contact them directly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;H1 style="vertical-align: middle;"&gt;&lt;/H1&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Oct 2016 07:28:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL8x-Universal-Multilink-Breakpoints-in-QSPI/m-p/660191#M40505</guid>
      <dc:creator>miduo</dc:creator>
      <dc:date>2016-10-28T07:28:38Z</dc:date>
    </item>
    <item>
      <title>Re: KL8x: Universal Multilink: Breakpoints in QSPI</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL8x-Universal-Multilink-Breakpoints-in-QSPI/m-p/660192#M40506</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for your response.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I did ask P&amp;amp;E and&amp;nbsp;got the following response:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;The Cortex M0, M3, and M4 cannot set hardware breakpoints at addresses higher than 0x1000_0000.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;I guess that means, that they are not able to set breakpoints in the QSPI.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As for the J-Link OpenSDA: The paragraph you cited is a bullet point under&amp;nbsp;&lt;/P&gt;&lt;BLOCKQUOTE class="jive-quote"&gt;The firmware that makes the OpenSDA platform J-Link compatible has some limitations in contrast to an original, industry leading SEGGER J-Link:&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I know that the SEGGER J-Link&amp;nbsp;claims to be able to&amp;nbsp;&lt;SPAN&gt;set breakpoints in the QSPI, but as it's more expensive I&amp;nbsp;wanted to check-out the alternatives. However, it looks like&amp;nbsp;there are&amp;nbsp;none.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Oct 2016 10:00:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL8x-Universal-Multilink-Breakpoints-in-QSPI/m-p/660192#M40506</guid>
      <dc:creator>konradgräfe</dc:creator>
      <dc:date>2016-10-28T10:00:32Z</dc:date>
    </item>
  </channel>
</rss>