<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic KEAZ64 muddle in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEAZ64-muddle/m-p/659396#M40440</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to the circuit diagram of the FRDM-KEAZ64Q64 the processor is an &lt;STRONG&gt;S9&lt;/STRONG&gt;KEAZ64AMLH, which is handled by the user's manual "9KEA64Z64M20SF0RM".&lt;BR /&gt;However the processor runs too quickly (FLL is faster than expected) and also the SIM_SCGC is not at the expected location.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If the user's manual "SKEA128Z80M48SF0RM" is however used as guide (would be correct for &lt;STRONG&gt;S&lt;/STRONG&gt;KEAZ64AMLH) all works as expected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Therefore, why is the chip in the circuit diagram and the marking on the chip on the board equal to the 40MHz S9KEAZ64AMLH, but behave as a 48MHz SKEAZ64AMLH ??? What is the source of this confusion?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 14 Nov 2016 18:37:55 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2016-11-14T18:37:55Z</dc:date>
    <item>
      <title>KEAZ64 muddle</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEAZ64-muddle/m-p/659396#M40440</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to the circuit diagram of the FRDM-KEAZ64Q64 the processor is an &lt;STRONG&gt;S9&lt;/STRONG&gt;KEAZ64AMLH, which is handled by the user's manual "9KEA64Z64M20SF0RM".&lt;BR /&gt;However the processor runs too quickly (FLL is faster than expected) and also the SIM_SCGC is not at the expected location.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If the user's manual "SKEA128Z80M48SF0RM" is however used as guide (would be correct for &lt;STRONG&gt;S&lt;/STRONG&gt;KEAZ64AMLH) all works as expected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Therefore, why is the chip in the circuit diagram and the marking on the chip on the board equal to the 40MHz S9KEAZ64AMLH, but behave as a 48MHz SKEAZ64AMLH ??? What is the source of this confusion?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Nov 2016 18:37:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEAZ64-muddle/m-p/659396#M40440</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2016-11-14T18:37:55Z</dc:date>
    </item>
    <item>
      <title>Re: KEAZ64 muddle</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEAZ64-muddle/m-p/659397#M40441</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mark,&lt;/P&gt;&lt;P&gt;The S9KEAZ64AMLH and S9KEAZN64AMLH are different chips. For the customer using FRDM-KEAZ64, the chip on that board is S9KEAZ64AMLH. So they need read the &lt;A href="http://www.nxp.com/files/microcontrollers/doc/ref_manual/KEA128RM.pdf?fasp=1&amp;amp;WT_TYPE=Reference%20Manuals&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;KEA128RM&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;The part numbers are very similar, sorry for this confusion.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="S9KEAZ64AMLH S9KEAZN64AMLH.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/9032iFBCB2C06B4FB4B54/image-size/large?v=v2&amp;amp;px=999" role="button" title="S9KEAZ64AMLH S9KEAZN64AMLH.png" alt="S9KEAZ64AMLH S9KEAZN64AMLH.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Nov 2016 07:12:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEAZ64-muddle/m-p/659397#M40441</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2016-11-15T07:12:38Z</dc:date>
    </item>
    <item>
      <title>Re: KEAZ64 muddle</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEAZ64-muddle/m-p/659398#M40442</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Robin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is the &lt;STRONG&gt;N&lt;/STRONG&gt; in the name that I was missing (thinking that the S&lt;STRONG&gt;9&lt;/STRONG&gt;KEA or SKEA may have been the difference).&lt;/P&gt;&lt;P&gt;Now all makes sense...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Nov 2016 10:29:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEAZ64-muddle/m-p/659398#M40442</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2016-11-15T10:29:55Z</dc:date>
    </item>
  </channel>
</rss>