<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Are FRDM-KW41Z drivers compatible with Windows 10? If not, when are they expected to be?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Are-FRDM-KW41Z-drivers-compatible-with-Windows-10-If-not-when/m-p/659115#M40421</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am thinking that what you mean " support" should be the IDE that the board used with. There are two IDEs we provide to support FRDM-KW41Z, IAR EWARM and NXP KDS. Both are work with Win 10.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 13 Apr 2017 07:20:57 GMT</pubDate>
    <dc:creator>miduo</dc:creator>
    <dc:date>2017-04-13T07:20:57Z</dc:date>
    <item>
      <title>Are FRDM-KW41Z drivers compatible with Windows 10? If not, when are they expected to be?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Are-FRDM-KW41Z-drivers-compatible-with-Windows-10-If-not-when/m-p/659114#M40420</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Same question applies for the other FRDM-KW boards (KW20Z, KW30Z, KW40Z).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Apr 2017 14:47:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Are-FRDM-KW41Z-drivers-compatible-with-Windows-10-If-not-when/m-p/659114#M40420</guid>
      <dc:creator>morechnikov</dc:creator>
      <dc:date>2017-04-07T14:47:43Z</dc:date>
    </item>
    <item>
      <title>Re: Are FRDM-KW41Z drivers compatible with Windows 10? If not, when are they expected to be?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Are-FRDM-KW41Z-drivers-compatible-with-Windows-10-If-not-when/m-p/659115#M40421</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am thinking that what you mean " support" should be the IDE that the board used with. There are two IDEs we provide to support FRDM-KW41Z, IAR EWARM and NXP KDS. Both are work with Win 10.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Apr 2017 07:20:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Are-FRDM-KW41Z-drivers-compatible-with-Windows-10-If-not-when/m-p/659115#M40421</guid>
      <dc:creator>miduo</dc:creator>
      <dc:date>2017-04-13T07:20:57Z</dc:date>
    </item>
    <item>
      <title>Re: Are FRDM-KW41Z drivers compatible with Windows 10? If not, when are they expected to be?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Are-FRDM-KW41Z-drivers-compatible-with-Windows-10-If-not-when/m-p/659116#M40422</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the response. Previously, I worked with the FRDM-KL25Z and KE02Z. Their main issue is that Windows 10 does not detect them, no USB storage for firmware and no COM port for programming. Even after OpenSDA and P&amp;amp;E Micro drivers are installed from the internet. The KDS IDE works fine, but it can't detect the COM Port&amp;nbsp;(OpenSDA) interface (neither can Device Manager). My question is in regards to the KW41Z's, and newer models', plug-and-play and/or P&amp;amp;E Micro/OpenSDA driver functionality, specifically in the Windows 10 environment. I apologize for any confusion.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Apr 2017 13:28:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Are-FRDM-KW41Z-drivers-compatible-with-Windows-10-If-not-when/m-p/659116#M40422</guid>
      <dc:creator>morechnikov</dc:creator>
      <dc:date>2017-04-13T13:28:03Z</dc:date>
    </item>
  </channel>
</rss>