<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: twrk20d50m   duplicate wire on J3 (TWRPI - tower plugin connector) mistake?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/twrk20d50m-duplicate-wire-on-J3-TWRPI-tower-plugin-connector/m-p/155767#M404</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I realize this is an incredibly old post, but surely the TWR-K20D50M J3 pin 11 was intended to be PTD0/DSPI0_PCS0, and not connected to pin 20?&amp;nbsp; Without access to DSPI0_PCS0 on the TWRPI connector, the TWR-K20D50M can't be configured as an SPI Slave can it?&amp;nbsp; If I have a TWRPI device that must be the SPI Master, please share (if there's a way) how I can configure the TWR-K20D50M to be an SPI Slave (using SPI over the TWRPI of course).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 Aug 2014 16:05:55 GMT</pubDate>
    <dc:creator>dhecker</dc:creator>
    <dc:date>2014-08-12T16:05:55Z</dc:date>
    <item>
      <title>twrk20d50m   duplicate wire on J3 (TWRPI - tower plugin connector) mistake?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/twrk20d50m-duplicate-wire-on-J3-TWRPI-tower-plugin-connector/m-p/155765#M402</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; I have just designed a new tower plug-in module to help prototype a zigbee design, and I noticed that in the TWRK20D50M_SCH.PDF schematic, connector J3 has pin 11 labeled as 'PTD4_EBI_AD2/DSPI0_PCS1/FTM0_CH4' and SPI0_CS1_B, and it also has pin 20 labelled as 'PTD4_EBI_AD2/DSPI0_PCS1/FTM0_CH4' and UART0_RTS.&amp;nbsp; (Yes the long names are the same!)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I checked my tower board (TWR-K20D50M) and pin11 is connected to pin 20. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This seems to be a mistake.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the pin-out listed in the TWRK20D72 user manual, and in other places, shows the following for the general purpose tower plug-in&lt;/P&gt;&lt;P&gt;(in the TWR schematic J10 and J3 are&amp;nbsp; the TWRPI, instead of J4 and J5 below)&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="General Purposes TWRPI Socket Pinout.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/38391iB3A971221490D772/image-size/large?v=v2&amp;amp;px=999" role="button" title="General Purposes TWRPI Socket Pinout.jpg" alt="General Purposes TWRPI Socket Pinout.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 28 Oct 2012 18:31:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/twrk20d50m-duplicate-wire-on-J3-TWRPI-tower-plugin-connector/m-p/155765#M402</guid>
      <dc:creator>Tonkabot</dc:creator>
      <dc:date>2012-10-28T18:31:13Z</dc:date>
    </item>
    <item>
      <title>Re: twrk20d50m   duplicate wire on J3 (TWRPI - tower plugin connector) mistake?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/twrk20d50m-duplicate-wire-on-J3-TWRPI-tower-plugin-connector/m-p/155766#M403</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The pin PTD4 on the MK20DX128VLH5 MCU can be configured as either a SPI Slave Select or a UART RTS signal (among other pin mux setting).&amp;nbsp; The connections are "technically" correct, but cause a limitaion that only one interface (SPI or UART w/ Flow Control) can be used on the TWRPI. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will discuss with the HW team responsible for the TWR-K20D50M to see if there is a more appropriate pin assignment for any future redesigns.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You will have to be careful that the shared pin is not being incorrection driven or sensed by the non-intended use case (for example, the SS signal being misintepreted when using the pin as a UART RTS).&lt;/P&gt;&lt;P&gt;If you are using a TWRPI that utilizes both the SPI SS and UART RTS (may be a GPIO) then I would recommend isolating the signal (assuming you don't actually need both pin functions) for the non-required use case.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Nov 2012 16:33:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/twrk20d50m-duplicate-wire-on-J3-TWRPI-tower-plugin-connector/m-p/155766#M403</guid>
      <dc:creator>CJarvis</dc:creator>
      <dc:date>2012-11-05T16:33:28Z</dc:date>
    </item>
    <item>
      <title>Re: twrk20d50m   duplicate wire on J3 (TWRPI - tower plugin connector) mistake?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/twrk20d50m-duplicate-wire-on-J3-TWRPI-tower-plugin-connector/m-p/155767#M404</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I realize this is an incredibly old post, but surely the TWR-K20D50M J3 pin 11 was intended to be PTD0/DSPI0_PCS0, and not connected to pin 20?&amp;nbsp; Without access to DSPI0_PCS0 on the TWRPI connector, the TWR-K20D50M can't be configured as an SPI Slave can it?&amp;nbsp; If I have a TWRPI device that must be the SPI Master, please share (if there's a way) how I can configure the TWR-K20D50M to be an SPI Slave (using SPI over the TWRPI of course).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Aug 2014 16:05:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/twrk20d50m-duplicate-wire-on-J3-TWRPI-tower-plugin-connector/m-p/155767#M404</guid>
      <dc:creator>dhecker</dc:creator>
      <dc:date>2014-08-12T16:05:55Z</dc:date>
    </item>
  </channel>
</rss>