<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 using external watchdog with MK64</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/using-external-watchdog-with-MK64/m-p/658181#M40358</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Although, not concerned &lt;STRONG&gt;directly&lt;/STRONG&gt; with the MK64, still, I have this question which I'm sure will help other users...&lt;/P&gt;&lt;P&gt;I'm using external &lt;A href="http://ww1.microchip.com/downloads/en/DeviceDoc/MIC1832.pdf"&gt;watchdog timer&lt;/A&gt; in my board to reset the MK64 in case no strobe is passed to it (I know there's also internal watchdog in the MK64).&lt;/P&gt;&lt;P&gt;What I don't understand is what should happen while burning the internal flash of the MK64. Since no strobe will pass to the watchdog timer, the watchdog will reset the board all the time (in loop).&lt;/P&gt;&lt;P&gt;Any idea how to avoid such scenario?&lt;/P&gt;&lt;P&gt;(I've placed pull up resistor on the PB_RST (pushbutton reset pin) but that will not help in case of burning the flash)&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;Roy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 31 Jan 2017 16:16:08 GMT</pubDate>
    <dc:creator>roymessinger</dc:creator>
    <dc:date>2017-01-31T16:16:08Z</dc:date>
    <item>
      <title>using external watchdog with MK64</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/using-external-watchdog-with-MK64/m-p/658181#M40358</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Although, not concerned &lt;STRONG&gt;directly&lt;/STRONG&gt; with the MK64, still, I have this question which I'm sure will help other users...&lt;/P&gt;&lt;P&gt;I'm using external &lt;A href="http://ww1.microchip.com/downloads/en/DeviceDoc/MIC1832.pdf"&gt;watchdog timer&lt;/A&gt; in my board to reset the MK64 in case no strobe is passed to it (I know there's also internal watchdog in the MK64).&lt;/P&gt;&lt;P&gt;What I don't understand is what should happen while burning the internal flash of the MK64. Since no strobe will pass to the watchdog timer, the watchdog will reset the board all the time (in loop).&lt;/P&gt;&lt;P&gt;Any idea how to avoid such scenario?&lt;/P&gt;&lt;P&gt;(I've placed pull up resistor on the PB_RST (pushbutton reset pin) but that will not help in case of burning the flash)&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;Roy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 31 Jan 2017 16:16:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/using-external-watchdog-with-MK64/m-p/658181#M40358</guid>
      <dc:creator>roymessinger</dc:creator>
      <dc:date>2017-01-31T16:16:08Z</dc:date>
    </item>
    <item>
      <title>Re: using external watchdog with MK64</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/using-external-watchdog-with-MK64/m-p/658182#M40359</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I do a search and there with &lt;A href="https://www.google.com/url?sa=t&amp;amp;rct=j&amp;amp;q=&amp;amp;esrc=s&amp;amp;source=web&amp;amp;cd=8&amp;amp;cad=rja&amp;amp;uact=8&amp;amp;ved=0ahUKEwiBmOGCwv3RAhVL-2MKHbmyB9IQFghTMAc&amp;amp;url=http%3A%2F%2Fwww.cs.ucf.edu%2F~lboloni%2FTeaching%2FEEL6897_2007%2Fpresentations%2FJeffreySchwentner-WatchdogTimers.ppt&amp;amp;usg=AFQjCNHyI00BYEjjCUNUhKLhOsU39Rax8A&amp;amp;sig2=o0pr99ezY-xmThDgxRaDpA"&gt;a ppt&lt;/A&gt; about external watchdog timers.&lt;/P&gt;&lt;P&gt;There with requirement to determine the proper watchdog timeout duration, the programmer must determine the amount of time it takes to execute the code, using worst case scenarios.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Feb 2017 08:18:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/using-external-watchdog-with-MK64/m-p/658182#M40359</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2017-02-07T08:18:44Z</dc:date>
    </item>
  </channel>
</rss>