<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Do not working ethernet with kinetis K64 with KSZ8081RNACA in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Do-not-working-ethernet-with-kinetis-K64-with-KSZ8081RNACA/m-p/657861#M40314</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I think the hardware connection is okay. But pls check that the pin24 of KSZ8081 is Reset pin, you should connect a RC circuit as the FRDM-K64. For the connector of Ethernet, Pls check if there should be serial resistor for the LEDG- and LEDG+.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 16 Nov 2016 07:05:05 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2016-11-16T07:05:05Z</dc:date>
    <item>
      <title>Do not working ethernet with kinetis K64 with KSZ8081RNACA</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Do-not-working-ethernet-with-kinetis-K64-with-KSZ8081RNACA/m-p/657860#M40313</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;I have working software on FRDM K64 and I tried make own hardware - I inspired from FRDM K64 schematic. Now, I have issue with connection ethernet. Schematic is on attachment.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried read registers from&amp;nbsp;KSZ8081RNACA - it is OK. When I connected cable, then it is not see any change. Any change on registers, any change on router.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please, could you help me, how can I debug it and find issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Vilem&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Nov 2016 12:31:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Do-not-working-ethernet-with-kinetis-K64-with-KSZ8081RNACA/m-p/657860#M40313</guid>
      <dc:creator>VilemZ</dc:creator>
      <dc:date>2016-11-14T12:31:50Z</dc:date>
    </item>
    <item>
      <title>Re: Do not working ethernet with kinetis K64 with KSZ8081RNACA</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Do-not-working-ethernet-with-kinetis-K64-with-KSZ8081RNACA/m-p/657861#M40314</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I think the hardware connection is okay. But pls check that the pin24 of KSZ8081 is Reset pin, you should connect a RC circuit as the FRDM-K64. For the connector of Ethernet, Pls check if there should be serial resistor for the LEDG- and LEDG+.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Nov 2016 07:05:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Do-not-working-ethernet-with-kinetis-K64-with-KSZ8081RNACA/m-p/657861#M40314</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2016-11-16T07:05:05Z</dc:date>
    </item>
    <item>
      <title>Re: Do not working ethernet with kinetis K64 with KSZ8081RNACA</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Do-not-working-ethernet-with-kinetis-K64-with-KSZ8081RNACA/m-p/657862#M40315</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #212121; background-color: #ffffff; font-size: 16px;"&gt;I was troubled because LAN was not stable. Thanks and it worked.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: #ffffff; color: #212121; font-size: 16px;"&gt;Thank you for your help!&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Nov 2016 11:12:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Do-not-working-ethernet-with-kinetis-K64-with-KSZ8081RNACA/m-p/657862#M40315</guid>
      <dc:creator>kazukiyamashita</dc:creator>
      <dc:date>2016-11-16T11:12:16Z</dc:date>
    </item>
    <item>
      <title>Re: Do not working ethernet with kinetis K64 with KSZ8081RNACA</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Do-not-working-ethernet-with-kinetis-K64-with-KSZ8081RNACA/m-p/657863#M40316</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;thanks for your reply. When I compare schematic with FRDM k64F, then I don't see any RC circuit on the pin24 of KSZ8081.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And serial resistor for the LEDG&amp;nbsp;can't affect detection of cable. And I think, that it is clear.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Vilem&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Nov 2016 11:18:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Do-not-working-ethernet-with-kinetis-K64-with-KSZ8081RNACA/m-p/657863#M40316</guid>
      <dc:creator>VilemZ</dc:creator>
      <dc:date>2016-11-16T11:18:02Z</dc:date>
    </item>
    <item>
      <title>Re: Do not working ethernet with kinetis K64 with KSZ8081RNACA</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Do-not-working-ethernet-with-kinetis-K64-with-KSZ8081RNACA/m-p/657864#M40317</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I tried change XTAL for PHY (25 MHz). It is OK. When xtal is not soldered on board, then kinetis not working too, because I am using 120 MHz clock for kinetis.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now, I don't know, what have I do? Please help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 20 Nov 2016 18:15:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Do-not-working-ethernet-with-kinetis-K64-with-KSZ8081RNACA/m-p/657864#M40317</guid>
      <dc:creator>VilemZ</dc:creator>
      <dc:date>2016-11-20T18:15:54Z</dc:date>
    </item>
  </channel>
</rss>