<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MKV31F128VLL10 sawtooth on reset pin in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKV31F128VLL10-sawtooth-on-reset-pin/m-p/657171#M40232</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, this if my first project with Kinetis, and I'm seeing a saw tooth waveform on the reset pin after a power up. I can connect to the target board and run/debug the application, however when I disconnect the probe (Jink) I see an oscillation on the reset_b pin.&lt;/P&gt;&lt;P&gt;First, I thought that this problem could be related to the fact that I was trying to use the NMI_b pin as GPIO. I changed the configuration on the board, so now the NMI_b is no longer a GPIO, but the problem still persists.&lt;/P&gt;&lt;P&gt;Any ideas what could be causing the problem or suggestions to fix it?&lt;/P&gt;&lt;P&gt;Any help appreciated. Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 27 Sep 2016 18:59:03 GMT</pubDate>
    <dc:creator>renatodutra</dc:creator>
    <dc:date>2016-09-27T18:59:03Z</dc:date>
    <item>
      <title>MKV31F128VLL10 sawtooth on reset pin</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKV31F128VLL10-sawtooth-on-reset-pin/m-p/657171#M40232</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, this if my first project with Kinetis, and I'm seeing a saw tooth waveform on the reset pin after a power up. I can connect to the target board and run/debug the application, however when I disconnect the probe (Jink) I see an oscillation on the reset_b pin.&lt;/P&gt;&lt;P&gt;First, I thought that this problem could be related to the fact that I was trying to use the NMI_b pin as GPIO. I changed the configuration on the board, so now the NMI_b is no longer a GPIO, but the problem still persists.&lt;/P&gt;&lt;P&gt;Any ideas what could be causing the problem or suggestions to fix it?&lt;/P&gt;&lt;P&gt;Any help appreciated. Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Sep 2016 18:59:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKV31F128VLL10-sawtooth-on-reset-pin/m-p/657171#M40232</guid>
      <dc:creator>renatodutra</dc:creator>
      <dc:date>2016-09-27T18:59:03Z</dc:date>
    </item>
    <item>
      <title>Re: MKV31F128VLL10 sawtooth on reset pin</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKV31F128VLL10-sawtooth-on-reset-pin/m-p/657172#M40233</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi renatodutra&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You were using NMI-b as GPIO, now that NMI-b is no longer GPIO I suggest you check that the NMI pin is high during reset. Also, the NMI_b pin, if enabled, must not have any capacitance connected to it and as its default function it has a weak internal pullup, but an external 4.7 kΩ to 10 kΩ pullup is recommended.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also I recommend you to check: &lt;A href="https://community.nxp.com/thread/383037"&gt;Reset signal of K64&lt;/A&gt;, This thread is something similar to your case, it can help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this information helps you.&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Jorge Alcala&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 01 Oct 2016 01:12:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKV31F128VLL10-sawtooth-on-reset-pin/m-p/657172#M40233</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2016-10-01T01:12:20Z</dc:date>
    </item>
    <item>
      <title>Re: MKV31F128VLL10 sawtooth on reset pin</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKV31F128VLL10-sawtooth-on-reset-pin/m-p/657173#M40234</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jorge,&lt;/P&gt;&lt;P&gt;Thanks for the reply.&lt;/P&gt;&lt;P&gt;In the end, the problem was related to an erroneous configuration.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Oct 2016 15:45:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKV31F128VLL10-sawtooth-on-reset-pin/m-p/657173#M40234</guid>
      <dc:creator>renatodutra</dc:creator>
      <dc:date>2016-10-07T15:45:27Z</dc:date>
    </item>
  </channel>
</rss>