<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MKW41Z512 DSPI PCS in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKW41Z512-DSPI-PCS/m-p/656905#M40205</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I figured it out, for now at least, I just select a CS pin that does not exist on the chip and use the gpio as a CS pin. Woks well so far.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 03 May 2017 13:28:11 GMT</pubDate>
    <dc:creator>ivaylomanushev</dc:creator>
    <dc:date>2017-05-03T13:28:11Z</dc:date>
    <item>
      <title>MKW41Z512 DSPI PCS</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKW41Z512-DSPI-PCS/m-p/656904#M40204</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Everyone,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a question about the pins I can use for the DSPI on the KW41z processor.&lt;/P&gt;&lt;P&gt;I am using a custom board and one of the pins that I have for the CS is just a regular GPIO pin instead of the SPI0_PCSx pin. Can I disable the PCS requirements on the drivers provided for the DSPI and use a manual toggle for the CS or do I have to use &amp;nbsp;a &lt;SPAN&gt;SPI0_PCSx &lt;/SPAN&gt;pin to be able to use the provided drivers?&lt;/P&gt;&lt;P&gt;If I am able to disable the PCS how do I go about doing so?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Ivaylo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 May 2017 16:10:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKW41Z512-DSPI-PCS/m-p/656904#M40204</guid>
      <dc:creator>ivaylomanushev</dc:creator>
      <dc:date>2017-05-02T16:10:29Z</dc:date>
    </item>
    <item>
      <title>Re: MKW41Z512 DSPI PCS</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKW41Z512-DSPI-PCS/m-p/656905#M40205</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I figured it out, for now at least, I just select a CS pin that does not exist on the chip and use the gpio as a CS pin. Woks well so far.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 May 2017 13:28:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKW41Z512-DSPI-PCS/m-p/656905#M40205</guid>
      <dc:creator>ivaylomanushev</dc:creator>
      <dc:date>2017-05-03T13:28:11Z</dc:date>
    </item>
  </channel>
</rss>