<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: KL81 tamper event cannot generate interrupt</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL81-tamper-event-cannot-generate-interrupt/m-p/656854#M40175</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I didn't enable the interrupt in NVIC module. After I added these code, interrupt works.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NVIC_SetPriority(Tamper_IRQn, 0);&amp;nbsp;&lt;BR /&gt; NVIC_EnableIRQ(Tamper_IRQn);&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 06 Feb 2017 01:18:42 GMT</pubDate>
    <dc:creator>daweiy</dc:creator>
    <dc:date>2017-02-06T01:18:42Z</dc:date>
    <item>
      <title>KL81 tamper event cannot generate interrupt</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL81-tamper-event-cannot-generate-interrupt/m-p/656853#M40174</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a hardware which has a tamper circuit loop. After I set up tamper pins, I trigger tamper event by switch on/off a physical switcher. When tamper event occurred, I can see DTF bit and tamper pin's TPF bit are both set.&amp;nbsp; I also set DTIE bit in IER register to enable interrupt when DTF sets. But tamper service routine,Tamper_IRQHandler, is not called.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the KL81 reference manual, it says "The DryIce Interrupt is asserted whenever a status flag and the corresponding interrupt enable bit are both set.". Obviously, it is not happening in my case.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone give me any clues on this issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Dawei&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Feb 2017 00:40:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL81-tamper-event-cannot-generate-interrupt/m-p/656853#M40174</guid>
      <dc:creator>daweiy</dc:creator>
      <dc:date>2017-02-01T00:40:19Z</dc:date>
    </item>
    <item>
      <title>Re: KL81 tamper event cannot generate interrupt</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL81-tamper-event-cannot-generate-interrupt/m-p/656854#M40175</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I didn't enable the interrupt in NVIC module. After I added these code, interrupt works.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NVIC_SetPriority(Tamper_IRQn, 0);&amp;nbsp;&lt;BR /&gt; NVIC_EnableIRQ(Tamper_IRQn);&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Feb 2017 01:18:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL81-tamper-event-cannot-generate-interrupt/m-p/656854#M40175</guid>
      <dc:creator>daweiy</dc:creator>
      <dc:date>2017-02-06T01:18:42Z</dc:date>
    </item>
  </channel>
</rss>