<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Keaz128 Bareboard Project can NOT boot  in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Keaz128-Bareboard-Project-can-NOT-boot/m-p/656110#M40085</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Dear Jorge,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Thanks for your reply.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;I found that issue was due to the __copy_rom_section.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;I remove most of the static variable into .rodata &amp;nbsp;memory section , the device can boot correctly .&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 05 May 2017 14:53:22 GMT</pubDate>
    <dc:creator>kigerzhang</dc:creator>
    <dc:date>2017-05-05T14:53:22Z</dc:date>
    <item>
      <title>Keaz128 Bareboard Project can NOT boot</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Keaz128-Bareboard-Project-can-NOT-boot/m-p/656108#M40083</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Now the Keaz128 was used to design a thermal control board .&amp;nbsp;&lt;/P&gt;&lt;P&gt;After the program was flash into the board , and power reset , the program can NOT run .&amp;nbsp;&lt;/P&gt;&lt;P&gt;If run debug , the program can run smoothly .&amp;nbsp;&lt;/P&gt;&lt;P&gt;What &amp;nbsp;can I do to find out the issue?&lt;/P&gt;&lt;P&gt;Please help me!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;IDE : CodeWarrior 10.7&amp;nbsp;&lt;/P&gt;&lt;P&gt;Flash Interface: Multilink Universal FX&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now , what I have done and found( I am not sure &amp;nbsp;whether this method is correct or not):&lt;/P&gt;&lt;P&gt;1. &amp;nbsp;Start debug &amp;nbsp;,the program is running well.&lt;/P&gt;&lt;P&gt;2. &amp;nbsp;Power reset the target board , the debugger lost the connection with target board .&lt;/P&gt;&lt;P&gt;3. &amp;nbsp;Let the debugger to re-connect to the board.&lt;/P&gt;&lt;P&gt;4. &amp;nbsp;Found the board halt &amp;nbsp;on&amp;nbsp;Unhandled_ivINT_NMI &amp;nbsp; interrupt&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;( in fact the NMI &amp;nbsp;was disable).&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The &amp;nbsp;call stack is as the &amp;nbsp;following:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/17506i87BF57A33601CFAC/image-size/large?v=v2&amp;amp;px=999" title="捕获1.JPG" alt="捕获1.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/17563i68E0BFDA34E7001A/image-size/large?v=v2&amp;amp;px=999" title="捕获2.JPG" alt="捕获2.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/17595i4C3A1FCD8D06140A/image-size/large?v=v2&amp;amp;px=999" title="捕获3.JPG" alt="捕获3.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/17644iC35A26E6B02190FC/image-size/large?v=v2&amp;amp;px=999" title="捕获4.JPG" alt="捕获4.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;By the way , there is a strange issue:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Once the the program was halt , the CodeWarrior &amp;nbsp;CAN NOT &amp;nbsp;erase/program the target board , even power reset the board. &amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;If &amp;nbsp;want to make the board&amp;nbsp;can be erase/program again , I must use &amp;nbsp;IAR to &amp;nbsp;erase the target . &amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is that CodeWarrior bug?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 May 2017 10:18:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Keaz128-Bareboard-Project-can-NOT-boot/m-p/656108#M40083</guid>
      <dc:creator>kigerzhang</dc:creator>
      <dc:date>2017-05-02T10:18:26Z</dc:date>
    </item>
    <item>
      <title>Re: Keaz128 Bareboard Project can NOT boot</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Keaz128-Bareboard-Project-can-NOT-boot/m-p/656109#M40084</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kiger Zhange&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are you using your custom hardware? Could you verify the status of your pin in all the process?&amp;nbsp; The NMI_b pin must not have any capacitance connected to it. Also, this pin has a weak internal pullup, but is a general recommendation an external 4.7 kΩ to 10 kΩ pullup. Also, could you clarify how you disable the NMI?, you mentioned that NMI was disable but you didn't tell us how you do it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Jorge Alcala&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 May 2017 00:53:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Keaz128-Bareboard-Project-can-NOT-boot/m-p/656109#M40084</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2017-05-05T00:53:16Z</dc:date>
    </item>
    <item>
      <title>Re: Keaz128 Bareboard Project can NOT boot</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Keaz128-Bareboard-Project-can-NOT-boot/m-p/656110#M40085</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Dear Jorge,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Thanks for your reply.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;I found that issue was due to the __copy_rom_section.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;I remove most of the static variable into .rodata &amp;nbsp;memory section , the device can boot correctly .&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 May 2017 14:53:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Keaz128-Bareboard-Project-can-NOT-boot/m-p/656110#M40085</guid>
      <dc:creator>kigerzhang</dc:creator>
      <dc:date>2017-05-05T14:53:22Z</dc:date>
    </item>
  </channel>
</rss>