<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic hardware multiply speed in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/hardware-multiply-speed/m-p/220854#M4004</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;can any one tells me is the speed of hardware multiply 1 cycle or 32 cycle version in Kinetis L type of MCUs?&amp;nbsp; I was reading on the internet that there are two hardware choices for multiply. The first is 1 cycle an the other is 32 cycle version for lower cost designs. Which of this versions is supported in Kinetis L MCUs?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Florijan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 18 Oct 2012 12:13:23 GMT</pubDate>
    <dc:creator>Florijan</dc:creator>
    <dc:date>2012-10-18T12:13:23Z</dc:date>
    <item>
      <title>hardware multiply speed</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/hardware-multiply-speed/m-p/220854#M4004</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;can any one tells me is the speed of hardware multiply 1 cycle or 32 cycle version in Kinetis L type of MCUs?&amp;nbsp; I was reading on the internet that there are two hardware choices for multiply. The first is 1 cycle an the other is 32 cycle version for lower cost designs. Which of this versions is supported in Kinetis L MCUs?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Florijan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Oct 2012 12:13:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/hardware-multiply-speed/m-p/220854#M4004</guid>
      <dc:creator>Florijan</dc:creator>
      <dc:date>2012-10-18T12:13:23Z</dc:date>
    </item>
    <item>
      <title>Re: hardware multiply speed</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/hardware-multiply-speed/m-p/220855#M4005</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kinetic - L supports : Single cycle 32 bits by 32 bits multiply&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can follow : KL04/KL05 Product Brief, Rev. 2, 6/2012&lt;/P&gt;&lt;P&gt;Page no : 12.&lt;/P&gt;&lt;P&gt;Link : &lt;A href="http://cache.freescale.com/files/32bit/doc/prod_brief/KL05PB.pdf?fpsp=1" title="http://cache.freescale.com/files/32bit/doc/prod_brief/KL05PB.pdf?fpsp=1"&gt;http://cache.freescale.com/files/32bit/doc/prod_brief/KL05PB.pdf?fpsp=1&lt;/A&gt;&lt;/P&gt;&lt;P&gt;----------------------------------------------------------&lt;/P&gt;&lt;P&gt;For more information on : Cortex-M multiply you can go through : &lt;A href="http://en.wikipedia.org/wiki/ARM_Cortex-M" title="http://en.wikipedia.org/wiki/ARM_Cortex-M"&gt;ARM Cortex-M - Wikipedia, the free encyclopedia&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Nilesh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 20 Oct 2012 09:46:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/hardware-multiply-speed/m-p/220855#M4005</guid>
      <dc:creator>sNilesh</dc:creator>
      <dc:date>2012-10-20T09:46:17Z</dc:date>
    </item>
  </channel>
</rss>