<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic FRDM-K66F does not enter in bootloader moder after a reset in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K66F-does-not-enter-in-bootloader-moder-after-a-reset/m-p/654977#M39984</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have received FRDM-K66F boards two days ago.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I was running the standard demo program "power_mode_switch_frdmk66" to set the board in high speed mode.&lt;/P&gt;&lt;P&gt;Suddenly, the board enter in "bootloader" mode ...&lt;/P&gt;&lt;P&gt;To go back in JLINK mode, I load the "OpenSDA_V2_1;bin file, and the operation probably failed because since this&amp;nbsp;&lt;/P&gt;&lt;P&gt;time,&amp;nbsp;the board does not seem to be power connected.&lt;/P&gt;&lt;P&gt;When, I connect the board to a PC using the micro-USB cable no LED is illuminated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you thing the board is broken or where the problem could come from ?&lt;/P&gt;&lt;P&gt;Thanks for your support.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Nadine&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 06 Apr 2017 08:06:42 GMT</pubDate>
    <dc:creator>nadine</dc:creator>
    <dc:date>2017-04-06T08:06:42Z</dc:date>
    <item>
      <title>FRDM-K66F does not enter in bootloader moder after a reset</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K66F-does-not-enter-in-bootloader-moder-after-a-reset/m-p/654977#M39984</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have received FRDM-K66F boards two days ago.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I was running the standard demo program "power_mode_switch_frdmk66" to set the board in high speed mode.&lt;/P&gt;&lt;P&gt;Suddenly, the board enter in "bootloader" mode ...&lt;/P&gt;&lt;P&gt;To go back in JLINK mode, I load the "OpenSDA_V2_1;bin file, and the operation probably failed because since this&amp;nbsp;&lt;/P&gt;&lt;P&gt;time,&amp;nbsp;the board does not seem to be power connected.&lt;/P&gt;&lt;P&gt;When, I connect the board to a PC using the micro-USB cable no LED is illuminated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you thing the board is broken or where the problem could come from ?&lt;/P&gt;&lt;P&gt;Thanks for your support.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Nadine&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Apr 2017 08:06:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K66F-does-not-enter-in-bootloader-moder-after-a-reset/m-p/654977#M39984</guid>
      <dc:creator>nadine</dc:creator>
      <dc:date>2017-04-06T08:06:42Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K66F does not enter in bootloader moder after a reset</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K66F-does-not-enter-in-bootloader-moder-after-a-reset/m-p/654978#M39985</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi again,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have made some measurements with a scope.&lt;/P&gt;&lt;P&gt;The J21 connector is not connected to the 5V by the PV5_K66_USB !!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Apr 2017 09:26:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K66F-does-not-enter-in-bootloader-moder-after-a-reset/m-p/654978#M39985</guid>
      <dc:creator>nadine</dc:creator>
      <dc:date>2017-04-06T09:26:36Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K66F does not enter in bootloader moder after a reset</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K66F-does-not-enter-in-bootloader-moder-after-a-reset/m-p/654979#M39986</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Nadline Sueur,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; What the PC OS you are using? win7 or others?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; About the J21, in default, there has a sub block short J21.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; If you are not using the win7, please find a win7, try to update the bootloader again.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; About the firmware, please use my attached firmware.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Any updated information, please let me know!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Apr 2017 09:45:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K66F-does-not-enter-in-bootloader-moder-after-a-reset/m-p/654979#M39986</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2017-04-07T09:45:22Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K66F does not enter in bootloader moder after a reset</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K66F-does-not-enter-in-bootloader-moder-after-a-reset/m-p/654980#M39987</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kerry,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have made the test under win7 as suggested in your email with no success.&amp;nbsp;&lt;/P&gt;&lt;P&gt;It looks like the board is definitively dead, it is not more possible to enter the bootloader mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have another board FRDM-K66F board which is working fine.&lt;/P&gt;&lt;P&gt;I'm a bit disappointed by the lifetime of this fisrt board ... Less than one day.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help.&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Nadine,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Apr 2017 12:36:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K66F-does-not-enter-in-bootloader-moder-after-a-reset/m-p/654980#M39987</guid>
      <dc:creator>nadine</dc:creator>
      <dc:date>2017-04-07T12:36:54Z</dc:date>
    </item>
  </channel>
</rss>