<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 wake up k70 from VLPS deep sleep by GPIO interrupt</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/wake-up-k70-from-VLPS-deep-sleep-by-GPIO-interrupt/m-p/654734#M39956</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can not wake up k70 (Kinetis) from VLPS deep sleep by GPIO interrupt.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is under uCLinux, where I enabled CONFIG_PM. After that, I can put K70 to deep sleep by "echo mem &amp;gt; /sys/power/state" and wake it up from UART debug console. But I can not wake up by triggering GPIO interrupt. I have confirmed that the interrupt works before and after the sleep by printing from the interrupt handler and I have also confirmed the GPIO pin value changes &amp;nbsp;from 0 to 1 during sleep after I triggered the GPIO interrupt.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to the K70 manual, I should be able to wake up VLPS by a GPIO interrupt. Does any have any insight why I could not?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 01 May 2017 22:00:10 GMT</pubDate>
    <dc:creator>minli</dc:creator>
    <dc:date>2017-05-01T22:00:10Z</dc:date>
    <item>
      <title>wake up k70 from VLPS deep sleep by GPIO interrupt</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/wake-up-k70-from-VLPS-deep-sleep-by-GPIO-interrupt/m-p/654734#M39956</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can not wake up k70 (Kinetis) from VLPS deep sleep by GPIO interrupt.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is under uCLinux, where I enabled CONFIG_PM. After that, I can put K70 to deep sleep by "echo mem &amp;gt; /sys/power/state" and wake it up from UART debug console. But I can not wake up by triggering GPIO interrupt. I have confirmed that the interrupt works before and after the sleep by printing from the interrupt handler and I have also confirmed the GPIO pin value changes &amp;nbsp;from 0 to 1 during sleep after I triggered the GPIO interrupt.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to the K70 manual, I should be able to wake up VLPS by a GPIO interrupt. Does any have any insight why I could not?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 May 2017 22:00:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/wake-up-k70-from-VLPS-deep-sleep-by-GPIO-interrupt/m-p/654734#M39956</guid>
      <dc:creator>minli</dc:creator>
      <dc:date>2017-05-01T22:00:10Z</dc:date>
    </item>
    <item>
      <title>Re: wake up k70 from VLPS deep sleep by GPIO interrupt</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/wake-up-k70-from-VLPS-deep-sleep-by-GPIO-interrupt/m-p/654735#M39957</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Min Li,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Please also post some code of entering VLPS mode, and the GPIO interrupt code on your side.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; I will help you to check it.&lt;/P&gt;&lt;P&gt;&amp;nbsp; If your K70 really enter VLPS mode, the GPIO must can wakeup it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 May 2017 08:16:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/wake-up-k70-from-VLPS-deep-sleep-by-GPIO-interrupt/m-p/654735#M39957</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2017-05-09T08:16:10Z</dc:date>
    </item>
  </channel>
</rss>