<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックWhy is eclipse neon not pausing debug in frdm-k64f board?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Why-is-eclipse-neon-not-pausing-debug-in-frdm-k64f-board/m-p/654252#M39926</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using eclipse neon and GCC ARM compiler for a project with the FRDM-K64F board and using JLink. I'm having problems debugging.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The debug session starts properly and it works fine but one of the problems is that if I try to set a breakpoint after clicking "Run" then the execution does not stop at the breakpoint and after a couple of seconds eclipse shows a little "warning" icon where the breakpoint is supposed to be. I hover over the warning icon and I get the message "&lt;STRONG&gt;Breakpoint installation failed: Suspend operation timeout"&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Another problem is that I can't pause the execution. If I click the "pause" button nothing happens, also nothing happens if I click "reset". The only way to stop the execution is clicking the "stop" button but that ends the debug session completely wich is very annoying.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I really don't have any idea about how to explain the issue better, this is what I'm experiencing and I'd like some guidance about knowing what is going on.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could somebody please help? what another kind&amp;nbsp;of information do I need to add to this question to help find out the problem?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 02 May 2017 01:28:16 GMT</pubDate>
    <dc:creator>m4l490n</dc:creator>
    <dc:date>2017-05-02T01:28:16Z</dc:date>
    <item>
      <title>Why is eclipse neon not pausing debug in frdm-k64f board?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Why-is-eclipse-neon-not-pausing-debug-in-frdm-k64f-board/m-p/654252#M39926</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using eclipse neon and GCC ARM compiler for a project with the FRDM-K64F board and using JLink. I'm having problems debugging.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The debug session starts properly and it works fine but one of the problems is that if I try to set a breakpoint after clicking "Run" then the execution does not stop at the breakpoint and after a couple of seconds eclipse shows a little "warning" icon where the breakpoint is supposed to be. I hover over the warning icon and I get the message "&lt;STRONG&gt;Breakpoint installation failed: Suspend operation timeout"&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Another problem is that I can't pause the execution. If I click the "pause" button nothing happens, also nothing happens if I click "reset". The only way to stop the execution is clicking the "stop" button but that ends the debug session completely wich is very annoying.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I really don't have any idea about how to explain the issue better, this is what I'm experiencing and I'd like some guidance about knowing what is going on.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could somebody please help? what another kind&amp;nbsp;of information do I need to add to this question to help find out the problem?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 May 2017 01:28:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Why-is-eclipse-neon-not-pausing-debug-in-frdm-k64f-board/m-p/654252#M39926</guid>
      <dc:creator>m4l490n</dc:creator>
      <dc:date>2017-05-02T01:28:16Z</dc:date>
    </item>
    <item>
      <title>Re: Why is eclipse neon not pausing debug in frdm-k64f board?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Why-is-eclipse-neon-not-pausing-debug-in-frdm-k64f-board/m-p/654253#M39927</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Manuel,&lt;/P&gt;&lt;P&gt;are you on Neon.3? See &lt;A class="link-titled" href="http://gnuarmeclipse.github.io/plugins/install/" title="http://gnuarmeclipse.github.io/plugins/install/"&gt;How to install the GNU ARM Eclipse plug-ins?&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;"&lt;STRONG&gt;Neon&lt;/STRONG&gt; initially had several problems, but starting with &lt;STRONG&gt;Neon.3&lt;/STRONG&gt; it finally seems fully functional. Avoid previous Neon versions, since they do not work properly. If you want to use GCC 6.x, you &lt;STRONG&gt;need&lt;/STRONG&gt; Neon.3 (the compiler itself has no problems working with Mar, but GDB 7.12 is not supported on versions before Neon.3)."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 May 2017 05:22:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Why-is-eclipse-neon-not-pausing-debug-in-frdm-k64f-board/m-p/654253#M39927</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2017-05-02T05:22:53Z</dc:date>
    </item>
    <item>
      <title>Re: Why is eclipse neon not pausing debug in frdm-k64f board?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Why-is-eclipse-neon-not-pausing-debug-in-frdm-k64f-board/m-p/654254#M39928</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This definitely helped. I have now Neon and the debugging is working correctly.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 May 2017 15:18:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Why-is-eclipse-neon-not-pausing-debug-in-frdm-k64f-board/m-p/654254#M39928</guid>
      <dc:creator>m4l490n</dc:creator>
      <dc:date>2017-05-02T15:18:48Z</dc:date>
    </item>
  </channel>
</rss>