<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Connection the USB typeC connector to K26 microcontroller in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Connection-the-USB-typeC-connector-to-K26-microcontroller/m-p/653043#M39794</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to connect this USB C connector &lt;A href="http://www.jae.com/z-en/pdf_download_exec.cfm?param=MB-0297-3E_0301-2E_DX07.pdf"&gt;JAE-DX07S024JJ3R1300&lt;/A&gt;&amp;nbsp; with the Kinetis K26.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/17329i5192368C1DC828EE/image-size/large?v=v2&amp;amp;px=999" title="usbc-1.jpg" alt="usbc-1.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/17371iF6B486B2B425122B/image-size/large?v=v2&amp;amp;px=999" title="usb-connection.png" alt="usb-connection.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I just want to use USB 2.0 interface. &amp;nbsp;If I don't use SuperSpeed Data Path (TXn+,TXn-, RXn-,RXn+) , Configuration Channel CC1 and CC2, Sideband Use SBU1 and SBU2, I have to leave the pins floating? &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/17412i957C6A4E0EC7E3B4/image-size/large?v=v2&amp;amp;px=999" title="usb.png" alt="usb.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;L4 and L5 are 330OHM or 330UH ? I'm confused by this&amp;nbsp; Is&amp;nbsp;not that an ferrite fixed inductor?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What New and Active &lt;A href="http://www.nexperia.com/products/esd-protection-tvs-filtering-and-signal-conditioning-esd-protection/transient-voltage-surge-suppressor-tvs/tvs-diodes-for-mobile-applications/#/p=1,s=0,f=,c=,rpp=,fs=0,sc=,so=,es="&gt;Nexperia TVS&lt;/A&gt; I can used to U15, U16 and U18 ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 29 Apr 2017 10:21:58 GMT</pubDate>
    <dc:creator>javierhernande1</dc:creator>
    <dc:date>2017-04-29T10:21:58Z</dc:date>
    <item>
      <title>Connection the USB typeC connector to K26 microcontroller</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Connection-the-USB-typeC-connector-to-K26-microcontroller/m-p/653043#M39794</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to connect this USB C connector &lt;A href="http://www.jae.com/z-en/pdf_download_exec.cfm?param=MB-0297-3E_0301-2E_DX07.pdf"&gt;JAE-DX07S024JJ3R1300&lt;/A&gt;&amp;nbsp; with the Kinetis K26.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/17329i5192368C1DC828EE/image-size/large?v=v2&amp;amp;px=999" title="usbc-1.jpg" alt="usbc-1.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/17371iF6B486B2B425122B/image-size/large?v=v2&amp;amp;px=999" title="usb-connection.png" alt="usb-connection.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I just want to use USB 2.0 interface. &amp;nbsp;If I don't use SuperSpeed Data Path (TXn+,TXn-, RXn-,RXn+) , Configuration Channel CC1 and CC2, Sideband Use SBU1 and SBU2, I have to leave the pins floating? &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/17412i957C6A4E0EC7E3B4/image-size/large?v=v2&amp;amp;px=999" title="usb.png" alt="usb.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;L4 and L5 are 330OHM or 330UH ? I'm confused by this&amp;nbsp; Is&amp;nbsp;not that an ferrite fixed inductor?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What New and Active &lt;A href="http://www.nexperia.com/products/esd-protection-tvs-filtering-and-signal-conditioning-esd-protection/transient-voltage-surge-suppressor-tvs/tvs-diodes-for-mobile-applications/#/p=1,s=0,f=,c=,rpp=,fs=0,sc=,so=,es="&gt;Nexperia TVS&lt;/A&gt; I can used to U15, U16 and U18 ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 29 Apr 2017 10:21:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Connection-the-USB-typeC-connector-to-K26-microcontroller/m-p/653043#M39794</guid>
      <dc:creator>javierhernande1</dc:creator>
      <dc:date>2017-04-29T10:21:58Z</dc:date>
    </item>
    <item>
      <title>Re: Connection the USB typeC connector to K26 microcontroller</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Connection-the-USB-typeC-connector-to-K26-microcontroller/m-p/653044#M39795</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Per USB Type-C spec 1.2, the unused pins can be left unconnected.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/18368i8129BADC2B2FB4ED/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;for the L4,L5 used in FRDM-K64F, please kindly refer to the attached BOM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope that helps,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 May 2017 08:33:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Connection-the-USB-typeC-connector-to-K26-microcontroller/m-p/653044#M39795</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2017-05-05T08:33:40Z</dc:date>
    </item>
  </channel>
</rss>