<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic K61 part internal flash size in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K61-part-internal-flash-size/m-p/652522#M39738</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a requirement to use the micro controller&amp;nbsp;MK61FX512VMJ12.&lt;/P&gt;&lt;P&gt;I'm bit confused with its part break up and memory size.&lt;/P&gt;&lt;P&gt;As per the part break up it says it has a program flash size of 512KB.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does it mean it has the Flex NVM and Flash memory as total size of 512KB or indivially there is 512KB of Flex NVM and 512KB of Flash memory ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is a mention of SRAM for this device. How do I find the size of this interanl SRAM for the given device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please help us at the earliest.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Nanjunda M&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 02 Jan 2017 16:15:18 GMT</pubDate>
    <dc:creator>nanjundam</dc:creator>
    <dc:date>2017-01-02T16:15:18Z</dc:date>
    <item>
      <title>K61 part internal flash size</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K61-part-internal-flash-size/m-p/652522#M39738</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a requirement to use the micro controller&amp;nbsp;MK61FX512VMJ12.&lt;/P&gt;&lt;P&gt;I'm bit confused with its part break up and memory size.&lt;/P&gt;&lt;P&gt;As per the part break up it says it has a program flash size of 512KB.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does it mean it has the Flex NVM and Flash memory as total size of 512KB or indivially there is 512KB of Flex NVM and 512KB of Flash memory ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is a mention of SRAM for this device. How do I find the size of this interanl SRAM for the given device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please help us at the earliest.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Nanjunda M&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Jan 2017 16:15:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K61-part-internal-flash-size/m-p/652522#M39738</guid>
      <dc:creator>nanjundam</dc:creator>
      <dc:date>2017-01-02T16:15:18Z</dc:date>
    </item>
    <item>
      <title>Re: K61 part internal flash size</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K61-part-internal-flash-size/m-p/652523#M39739</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear&amp;nbsp;&lt;A _jive_internal="true" data-content-finding="Community" data-userid="265435" data-username="nanjundam" href="https://community.nxp.com/people/nanjundam"&gt;Nanjunda M&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;This device have:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;512 KB of Flash&lt;/LI&gt;&lt;LI&gt;512 KB FlexMem&lt;/LI&gt;&lt;LI&gt;128 KB RAM&lt;/LI&gt;&lt;LI&gt;16 KB FlexRAM&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the&lt;A href="http://www.nxp.com/assets/documents/data/en/data-sheets/K61P256M120SF3.pdf"&gt; Data sheet&lt;/A&gt;&amp;nbsp;in the first page you will find the &amp;nbsp;Memories and memory interfaces.&lt;/P&gt;&lt;P&gt;you can have some information there about the size of the memories and there are specific sections for each one.&lt;/P&gt;&lt;P&gt;hope this helps.&lt;/P&gt;&lt;P&gt;have a great day&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jonathan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Jan 2017 23:29:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K61-part-internal-flash-size/m-p/652523#M39739</guid>
      <dc:creator>Jonathan_Iglesias</dc:creator>
      <dc:date>2017-01-03T23:29:45Z</dc:date>
    </item>
  </channel>
</rss>