<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: KL82 UART Code Example</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL82-UART-Code-Example/m-p/652185#M39725</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;thank you for your kind help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Well, I need to write and read string to/from the uart.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/3492iEA768837D96947CB/image-size/large?v=v2&amp;amp;px=999" title="code.png" alt="code.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can't see how I can write to the uart register. this would be interessting to know and which configurations are needed to get it working barebone. Or could you explain how I could use the functions from the libs?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 13 Oct 2016 08:01:15 GMT</pubDate>
    <dc:creator>us1</dc:creator>
    <dc:date>2016-10-13T08:01:15Z</dc:date>
    <item>
      <title>KL82 UART Code Example</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL82-UART-Code-Example/m-p/652177#M39717</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;is there some Examplecode for the KL82 Board to get the UART working?&lt;/P&gt;&lt;P&gt;Is there a direct example from someone which used the ESP8266 with it?&lt;/P&gt;&lt;P&gt;Would appreceate any help,&lt;/P&gt;&lt;P&gt;thank you very much&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Sep 2016 09:45:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL82-UART-Code-Example/m-p/652177#M39717</guid>
      <dc:creator>us1</dc:creator>
      <dc:date>2016-09-26T09:45:25Z</dc:date>
    </item>
    <item>
      <title>Re: KL82 UART Code Example</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL82-UART-Code-Example/m-p/652178#M39718</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" data-content-finding="Community" data-userid="277307" data-username="us1" href="https://community.nxp.com/people/us1"&gt;Ulrich Steinlehner&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;I'd highly recommend you to refer to the KSDK v2.0 which includes the some demos of the UART module.&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.nxp.com/products/software-and-tools/run-time-software/kinetis-software-and-tools/development-platforms-with-mbed/software-development-kit-for-kinetis-mcus:KINETIS-SDK?fsrch=1&amp;amp;sr=1&amp;amp;pageNum=1" title="http://www.nxp.com/products/software-and-tools/run-time-software/kinetis-software-and-tools/development-platforms-with-mbed/software-development-kit-for-kinetis-mcus:KINETIS-SDK?fsrch=1&amp;amp;sr=1&amp;amp;pageNum=1"&gt;Software Development Kit for Kinetis MCUs|NXP&lt;/A&gt; &lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Sep 2016 02:17:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL82-UART-Code-Example/m-p/652178#M39718</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2016-09-27T02:17:18Z</dc:date>
    </item>
    <item>
      <title>Re: KL82 UART Code Example</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL82-UART-Code-Example/m-p/652179#M39719</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;thank you.&lt;/P&gt;&lt;P&gt;I downloaded the SDK for the kl82 but what do I do with the *.zip! file? Extract or add in the Kinetis design studio, tried but it does somehow not work both ways...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Sep 2016 11:07:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL82-UART-Code-Example/m-p/652179#M39719</guid>
      <dc:creator>us1</dc:creator>
      <dc:date>2016-09-28T11:07:37Z</dc:date>
    </item>
    <item>
      <title>Re: KL82 UART Code Example</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL82-UART-Code-Example/m-p/652180#M39720</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ulrich,&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;Firstly, you should extract it, then get start with the KSDK V2.0 by referring to the attachment.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Sep 2016 01:42:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL82-UART-Code-Example/m-p/652180#M39720</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2016-09-29T01:42:04Z</dc:date>
    </item>
    <item>
      <title>Re: KL82 UART Code Example</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL82-UART-Code-Example/m-p/652181#M39721</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI,&lt;/P&gt;&lt;P&gt;thank you. where Can I find the uart example?&lt;/P&gt;&lt;P&gt;thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Sep 2016 10:11:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL82-UART-Code-Example/m-p/652181#M39721</guid>
      <dc:creator>us1</dc:creator>
      <dc:date>2016-09-29T10:11:47Z</dc:date>
    </item>
    <item>
      <title>Re: KL82 UART Code Example</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL82-UART-Code-Example/m-p/652182#M39722</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ulrich,&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;The LPUART demo resides in the \SDK_2.0_MKL82Z128xxx7\boards\frdmkl82z\driver_examples which as the Fig 1 shows.&lt;/P&gt;&lt;P style="text-align: center;"&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/2317iF9F3FFF6042B3632/image-size/large?v=v2&amp;amp;px=999" title="2016-09-29_20-34-45.jpg" alt="2016-09-29_20-34-45.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P style="text-align: center;"&gt;Fig 1&lt;/P&gt;&lt;P style="text-align: left;"&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Sep 2016 12:37:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL82-UART-Code-Example/m-p/652182#M39722</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2016-09-29T12:37:25Z</dc:date>
    </item>
    <item>
      <title>Re: KL82 UART Code Example</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL82-UART-Code-Example/m-p/652183#M39723</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you very much,&lt;/P&gt;&lt;P&gt;but I can't really understand this example, it's to hard to understand.&lt;/P&gt;&lt;P&gt;Is there some code for receiving strings?&lt;/P&gt;&lt;P&gt;Thank you a lot&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Oct 2016 18:05:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL82-UART-Code-Example/m-p/652183#M39723</guid>
      <dc:creator>us1</dc:creator>
      <dc:date>2016-10-12T18:05:30Z</dc:date>
    </item>
    <item>
      <title>Re: KL82 UART Code Example</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL82-UART-Code-Example/m-p/652184#M39724</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ulrich,&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;The SDK development kit is the first option for the customer to get start with the Kinetis MCU.&lt;/P&gt;&lt;P&gt;And I'd like to know what the codes confuse you, you can share them with the screenshot.&lt;/P&gt;&lt;P&gt;I'm looking forward to your reply.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Oct 2016 01:44:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL82-UART-Code-Example/m-p/652184#M39724</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2016-10-13T01:44:48Z</dc:date>
    </item>
    <item>
      <title>Re: KL82 UART Code Example</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL82-UART-Code-Example/m-p/652185#M39725</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;thank you for your kind help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Well, I need to write and read string to/from the uart.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/3492iEA768837D96947CB/image-size/large?v=v2&amp;amp;px=999" title="code.png" alt="code.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can't see how I can write to the uart register. this would be interessting to know and which configurations are needed to get it working barebone. Or could you explain how I could use the functions from the libs?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Oct 2016 08:01:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL82-UART-Code-Example/m-p/652185#M39725</guid>
      <dc:creator>us1</dc:creator>
      <dc:date>2016-10-13T08:01:15Z</dc:date>
    </item>
    <item>
      <title>Re: KL82 UART Code Example</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL82-UART-Code-Example/m-p/652186#M39726</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I created now two things:&lt;/P&gt;&lt;P&gt;I send a AT Command to UART via: &lt;EM&gt;LPUART_WriteBlocking(DEMO_LPUART, "AT\r\n", sizeof("AT\r\n")-1);&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;when I do the same with a function like this:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&lt;EM&gt; void uart_esp12_send_command (char* esp_command)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;{&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;LPUART_WriteBlocking(DEMO_LPUART, esp_command, sizeof(esp_command)-1);&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;}&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;and then&lt;/P&gt;&lt;P&gt;&lt;EM&gt;uart_esp12_send_command ("AT-Command");&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I only get with the function three letters displayed on the Serial Consol, but the normal Command ( &lt;EM&gt;LPUART_WriteBlocking(DEMO_LPUART, "AT\r\n", sizeof("AT\r\n")-1)) &lt;/EM&gt;gives back the full entered string. &lt;/P&gt;&lt;P&gt;How can I change this? I need to change the data type.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How could I receive data strings with: LPUART_ReadBlocking(LPUART_Type *base, uint8_t *data, size_t length);??&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Oct 2016 13:28:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL82-UART-Code-Example/m-p/652186#M39726</guid>
      <dc:creator>us1</dc:creator>
      <dc:date>2016-10-13T13:28:31Z</dc:date>
    </item>
  </channel>
</rss>