<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 TWR-KV58F220M</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-KV58F220M/m-p/650659#M39587</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am testing demo application for now. And have the following questions:&lt;/P&gt;&lt;P&gt;1) KV58F220M can work on 240Mhz as well? If not, what is the maximum frequency on this?&lt;/P&gt;&lt;P&gt;2) In the demo project, it is set to 235.7Mhz, is it any reason why not set to 240MHz?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Christie&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 26 Sep 2016 20:20:33 GMT</pubDate>
    <dc:creator>a8Chcx</dc:creator>
    <dc:date>2016-09-26T20:20:33Z</dc:date>
    <item>
      <title>TWR-KV58F220M</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-KV58F220M/m-p/650659#M39587</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am testing demo application for now. And have the following questions:&lt;/P&gt;&lt;P&gt;1) KV58F220M can work on 240Mhz as well? If not, what is the maximum frequency on this?&lt;/P&gt;&lt;P&gt;2) In the demo project, it is set to 235.7Mhz, is it any reason why not set to 240MHz?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Christie&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Sep 2016 20:20:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-KV58F220M/m-p/650659#M39587</guid>
      <dc:creator>a8Chcx</dc:creator>
      <dc:date>2016-09-26T20:20:33Z</dc:date>
    </item>
    <item>
      <title>Re: TWR-KV58F220M</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-KV58F220M/m-p/650660#M39588</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Christie,&lt;/P&gt;&lt;P&gt;Pls go to the website:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/kinetis-cortex-m-mcus/v-series-real-time-control-m0-plus-m4-m7/kinetis-kv5x-240-mhz-motor-control-and-power-conversion-ethernet-microcontrollers-mcus-based-on-arm-cortex-m7-core:KV5x?&amp;amp;cof=0&amp;amp;am=0&amp;amp;tab=Buy_Parametric_Tab&amp;amp;fromSearch=false" title="http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/kinetis-cortex-m-mcus/v-series-real-time-control-m0-plus-m4-m7/kinetis-kv5x-240-mhz-motor-control-and-power-conversion-ethernet-microcontrollers-mcus-based-on-arm-cortex-m7-core:KV5x?&amp;amp;cof=0&amp;amp;am=0&amp;amp;tab=Buy_Parametric_Tab&amp;amp;fromSearch=false"&gt;ARM Cortex-M7|Kinetis KV5x Real-time Control MCUs|NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;all of KV5x can work in 240mhz at most in high speed run mode.&lt;/P&gt;&lt;P&gt;Because the TWR-KV58 uses external 50MHz external clock source, and the PLL input clock frequency must range from 8mhz to 16MHz, so this is the PLL configuration&lt;/P&gt;&lt;P&gt;VCO output clock frequency=(50MHz/4)*19*2=475MHz, PLL output clock frequency is 475MHz/2=237.5MHz.&lt;/P&gt;&lt;P&gt;The external 50mhz clock source is populated on the TWR-KV58 board and it is the clcok souce for Ethernet.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Sep 2016 03:26:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-KV58F220M/m-p/650660#M39588</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2016-09-27T03:26:35Z</dc:date>
    </item>
  </channel>
</rss>