<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックNo Disable Option for some IO's</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/No-Disable-Option-for-some-IO-s/m-p/649904#M39545</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can specific IO can be configured as "DISABLED" if there is no option like this in it's datasheet ?&lt;/P&gt;&lt;P&gt;For example G8:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/6611i0DC6CAD62D6AEAE4/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If not - what is the preffered configuration for savig power (input PD/PU, Output) ?&lt;/P&gt;&lt;P&gt;Another thing - If pin configured as "DISABLED", it is enough for saving power ? or more configurations should be done (PD,PU) ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Edi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 26 Sep 2016 07:27:45 GMT</pubDate>
    <dc:creator>razumovskyeduar</dc:creator>
    <dc:date>2016-09-26T07:27:45Z</dc:date>
    <item>
      <title>No Disable Option for some IO's</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/No-Disable-Option-for-some-IO-s/m-p/649904#M39545</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can specific IO can be configured as "DISABLED" if there is no option like this in it's datasheet ?&lt;/P&gt;&lt;P&gt;For example G8:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/6611i0DC6CAD62D6AEAE4/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If not - what is the preffered configuration for savig power (input PD/PU, Output) ?&lt;/P&gt;&lt;P&gt;Another thing - If pin configured as "DISABLED", it is enough for saving power ? or more configurations should be done (PD,PU) ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Edi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Sep 2016 07:27:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/No-Disable-Option-for-some-IO-s/m-p/649904#M39545</guid>
      <dc:creator>razumovskyeduar</dc:creator>
      <dc:date>2016-09-26T07:27:45Z</dc:date>
    </item>
    <item>
      <title>Re: No Disable Option for some IO's</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/No-Disable-Option-for-some-IO-s/m-p/649905#M39546</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For the G8 pin default function is analog input pin, it could be left floating.&lt;/P&gt;&lt;P&gt;The digital IO pin with default "DISABLE"&amp;nbsp; will saving the power. There does not need to configure related pin, keep default "Disable" setting.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Sep 2016 06:12:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/No-Disable-Option-for-some-IO-s/m-p/649905#M39546</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2016-09-27T06:12:18Z</dc:date>
    </item>
  </channel>
</rss>