<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re:  FRDM-K22F core</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K22F-core/m-p/649446#M39510</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;The K22 on the FRDM-K22F has a single precision floating point unit present, is it is a ARM Cortex-M4F. You are right: M4F is sometimes not used consistently in the industry, as it is a Cortex M4 with an optional floating point unit. So the single precision floating point unit can be present or not. In any case, I would have a look at the data sheet to be sure as the device ID itself might not be enough to identify the architecture/core (M0+/M4/etc) and what features are implemented.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 27 Jan 2017 18:49:27 GMT</pubDate>
    <dc:creator>BlackNight</dc:creator>
    <dc:date>2017-01-27T18:49:27Z</dc:date>
    <item>
      <title>FRDM-K22F core</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K22F-core/m-p/649445#M39509</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm new to NXP MPUs and am having trouble figuring out the exact ARM Cortex core inside the FRDM-K22F dev board. Some of the descriptions I've seen around state its Cortex M4F, while others say its Cortex M4 (no FPU). Can someone clear this up for me?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A follow up: is there a common naming convention in the NXP world of MCUs (besides the flash size), like the 'F' referring to floating p. unit?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Jan 2017 15:11:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K22F-core/m-p/649445#M39509</guid>
      <dc:creator>alex_p</dc:creator>
      <dc:date>2017-01-27T15:11:06Z</dc:date>
    </item>
    <item>
      <title>Re:  FRDM-K22F core</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K22F-core/m-p/649446#M39510</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;The K22 on the FRDM-K22F has a single precision floating point unit present, is it is a ARM Cortex-M4F. You are right: M4F is sometimes not used consistently in the industry, as it is a Cortex M4 with an optional floating point unit. So the single precision floating point unit can be present or not. In any case, I would have a look at the data sheet to be sure as the device ID itself might not be enough to identify the architecture/core (M0+/M4/etc) and what features are implemented.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Jan 2017 18:49:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K22F-core/m-p/649446#M39510</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2017-01-27T18:49:27Z</dc:date>
    </item>
    <item>
      <title>Re:  FRDM-K22F core</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K22F-core/m-p/649447#M39511</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Erich's right about the core. &amp;nbsp;More generally on the topic of NXP's naming, watch out - I think the marketing people must win out over the engineers on this stuff sometimes. &amp;nbsp;The MK22FN512 and the MK22FN1M0, for example, sound like they'd be the same part with different memory configurations - that's been the convention for most parts I've used over the last 20+ years. &amp;nbsp;They're not, though. &amp;nbsp;They're different generations and the 1 meg part doesn't have HSRUN or the crystal-less USB oscillator, and the flash memory configuration is quite different from the 512k part. &amp;nbsp;It's actually part of the K21F120 line. &amp;nbsp;The only semi-obvious thing in the documentation to suggest that is the recommended development board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Scott&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 29 Jan 2017 02:37:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K22F-core/m-p/649447#M39511</guid>
      <dc:creator>scottm</dc:creator>
      <dc:date>2017-01-29T02:37:18Z</dc:date>
    </item>
  </channel>
</rss>