<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Kinetis K64F missing documentation?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64F-missing-documentation/m-p/648297#M39392</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Dave,&lt;/P&gt;&lt;P&gt;I am sorry for the delay. Regarding the GPIO toggling based on&amp;nbsp; DMA plus PIT, You have to use DMA channel0 if you use PIT0 to trigger, use DMA channel1 if you use PIT1. I attach the fig here.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/9204iEAB8801654ECC73A/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;For DGPIO configuration,&amp;nbsp;&amp;nbsp; you have to set the PORTx_PCRy as GPIO function and set the IRQC bits as 3(DMA request on either edge.). For example, if you use PIT0,&amp;nbsp; you have to use DMA channel0. Set the source bits of DMAMUX_CHCFG0 as 49(PORTA), 50(PORTB), 51 (PORTC)..., configure PIT0 registers and DMA registers, it is okay.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 16 Nov 2016 03:28:24 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2016-11-16T03:28:24Z</dc:date>
    <item>
      <title>Kinetis K64F missing documentation?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64F-missing-documentation/m-p/648293#M39388</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We're evaluating the K64F for a family of instrumentation products, but I'm having trouble finding all the required documentation. On the NXP web site, I find only two documents about this chip:&lt;BR /&gt;K64P144M120SF5RM.pdf: K64 Sub-Family Reference Manual, Rev. 2, January 2014&lt;BR /&gt;K64P144M120SF5.pdf: Kinetis K64F Sub-Family Data Sheet, Rev. 6, 08/2015&lt;/P&gt;&lt;P&gt;Questions:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;In the reference manual, in many places it says "&lt;EM&gt;Refer to chip configuration details&lt;/EM&gt;".&lt;BR /&gt;Where are "chip configuration details"?&lt;/LI&gt;&lt;LI&gt;Reference manual page 934, PDBx_SC field descriptions, Trigger Input Source Select, says:&lt;BR /&gt;"&lt;EM&gt;Refer to chip configuration details for the actual PDB input trigger connections.&lt;/EM&gt;"&lt;BR /&gt;Where is the table defining the values and possible PDB input triggers?&lt;/LI&gt;&lt;LI&gt;Reference manual page 459, DMAMUX_CHCFGn field descriptions DMA Channel Source, says:&lt;BR /&gt;"&lt;EM&gt;See your device's chip configuration details for information about the peripherals and their slot numbers.&lt;/EM&gt;"&lt;BR /&gt;Where is the table defining allowed values and corresponding peripherals?&lt;/LI&gt;&lt;LI&gt;Reference manual section 21.5.2, To enable a source with periodic triggering, step 5 says:&lt;BR /&gt;"&lt;EM&gt;Select the source to be routed to the DMA channel. Write to the corresponding&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;CHCFG register&lt;/EM&gt;" - This appears to be an error. &lt;BR /&gt;&lt;SPAN style="text-decoration: underline;"&gt;&lt;STRONG&gt;For periodic triggering, the source must be set to an "always on" source&lt;/STRONG&gt;&lt;/SPAN&gt;, right?&lt;/LI&gt;&lt;LI&gt;Where is the table of application notes, with links to the notes and associated source code, for Kinetis processors?&lt;BR /&gt;The last thing I find with google is a list without links last updated in 2012...&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Without this information, it is very hard for your customers to make use of these parts...&lt;BR /&gt;Any help would be much appreciated.&lt;/P&gt;&lt;P&gt;Thanks!&lt;BR /&gt;Best Regards, Dave&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Oct 2016 14:19:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64F-missing-documentation/m-p/648293#M39388</guid>
      <dc:creator>davenadler</dc:creator>
      <dc:date>2016-10-18T14:19:18Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis K64F missing documentation?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64F-missing-documentation/m-p/648294#M39389</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Pls refer to chapter 3 chip configuration in K64P144M120SF5RM.pdf.&lt;/P&gt;&lt;P&gt;For PDB triggering source, pls refer to section 3.8.1.1.2 PDB Input Trigger Connections.&lt;/P&gt;&lt;P&gt;For DMA requestion source, pls refer to section 3.3.9.1 DMA MUX request sources&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Oct 2016 02:31:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64F-missing-documentation/m-p/648294#M39389</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2016-10-19T02:31:12Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis K64F missing documentation?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64F-missing-documentation/m-p/648295#M39390</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks! To save other customers trouble, please consider updating the manual adding links in the PDF to the mentioned chapter, or at a very minimum say "&lt;EM&gt;Refer to chip configuration details chapter above&lt;/EM&gt;"... I was looking for a separate document (as have other customers asking this question on this forum).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you answer questions 4 and 5 above?&lt;BR /&gt;Also, another apparent documentation error:&lt;/P&gt;&lt;P&gt;6) In reference manual 21.4.1 DMA channels with periodic triggering capability: PIT 1 is shown connected to DMA trigger 0. In reality, PIT 0 is connected to DMA trigger 0, right? Here's the erroneous diagram (also repeated in the text)&lt;span class="lia-inline-image-display-wrapper" image-alt="K64F_wrong_trigger_connections.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/3917i341BCEB32CE4112D/image-size/large?v=v2&amp;amp;px=999" role="button" title="K64F_wrong_trigger_connections.png" alt="K64F_wrong_trigger_connections.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Best Regards, Dave&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Oct 2016 13:49:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64F-missing-documentation/m-p/648295#M39390</guid>
      <dc:creator>davenadler</dc:creator>
      <dc:date>2016-10-19T13:49:59Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis K64F missing documentation?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64F-missing-documentation/m-p/648296#M39391</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello XiangJun Rong - We are still waiting for answers to 4,5, and 6 above? It has been almost one month?&lt;BR /&gt;Answers would be much appreciated!&lt;BR /&gt;Thanks, Best Regards, Dave&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Nov 2016 15:18:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64F-missing-documentation/m-p/648296#M39391</guid>
      <dc:creator>davenadler</dc:creator>
      <dc:date>2016-11-15T15:18:43Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis K64F missing documentation?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64F-missing-documentation/m-p/648297#M39392</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Dave,&lt;/P&gt;&lt;P&gt;I am sorry for the delay. Regarding the GPIO toggling based on&amp;nbsp; DMA plus PIT, You have to use DMA channel0 if you use PIT0 to trigger, use DMA channel1 if you use PIT1. I attach the fig here.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/9204iEAB8801654ECC73A/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;For DGPIO configuration,&amp;nbsp;&amp;nbsp; you have to set the PORTx_PCRy as GPIO function and set the IRQC bits as 3(DMA request on either edge.). For example, if you use PIT0,&amp;nbsp; you have to use DMA channel0. Set the source bits of DMAMUX_CHCFG0 as 49(PORTA), 50(PORTB), 51 (PORTC)..., configure PIT0 registers and DMA registers, it is okay.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Nov 2016 03:28:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64F-missing-documentation/m-p/648297#M39392</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2016-11-16T03:28:24Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis K64F missing documentation?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64F-missing-documentation/m-p/648298#M39393</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Pls refer to an4419.pdf.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Nov 2016 03:32:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64F-missing-documentation/m-p/648298#M39393</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2016-11-16T03:32:47Z</dc:date>
    </item>
  </channel>
</rss>