<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: K82 Kinetics DAC Voltage reference</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-Kinetics-DAC-Voltage-reference/m-p/647681#M39345</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Fang Li,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your answer,&lt;/P&gt;&lt;P&gt;I thought the VREF_OUT pin is an output only, do you mean that I should connect my external reference to this pin?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Since my design only needs DAC and DAC IDDA current is 700uA I was connecting the 2.5V reference to VDDA directly.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Would you please clarify which is the preferred approach?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 06 Apr 2017 14:23:11 GMT</pubDate>
    <dc:creator>mhanuel</dc:creator>
    <dc:date>2017-04-06T14:23:11Z</dc:date>
    <item>
      <title>K82 Kinetics DAC Voltage reference</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-Kinetics-DAC-Voltage-reference/m-p/647679#M39343</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Will appreciate anyone that can clarify the following about K82 Voltage Reference for DAC module.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Datasheet page 52 Note 1 says:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;"The DAC reference can be selected to be VDDA or VREFH."&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But reference manual page 1429 (46.1.3 12-Bit DAC Reference) says:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;"For this device VREF_OUT and VDDA are selectable as the DAC reference.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;VREF_OUT is connected to the DACREF_1 input and VDDA is connected to the&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;DACREF_2 input. Use DACx_C0[DACRFS] control bit to select between these two&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;options."&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to use a precision 2.5V reference, should I then connect the Reference Output to VDDA? and leave VREFH floating, I cannot see how to select the VREFH for DAC, for ADC there is the SC register.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you in advance,&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Apr 2017 23:56:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-Kinetics-DAC-Voltage-reference/m-p/647679#M39343</guid>
      <dc:creator>mhanuel</dc:creator>
      <dc:date>2017-04-04T23:56:38Z</dc:date>
    </item>
    <item>
      <title>Re: K82 Kinetics DAC Voltage reference</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-Kinetics-DAC-Voltage-reference/m-p/647680#M39344</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please ignore the description of the datasheet. Make the reference manual as a correct that VREF_OUT and VDDA are selectable as the DAC reference&lt;EM&gt;.&amp;nbsp;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For your case, an external voltage reference can be used as the DAC voltage reference by connecting it to the VREF_OUT pin and selecting VREF_OUT as the DAC reference.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Apr 2017 07:47:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-Kinetics-DAC-Voltage-reference/m-p/647680#M39344</guid>
      <dc:creator>miduo</dc:creator>
      <dc:date>2017-04-06T07:47:30Z</dc:date>
    </item>
    <item>
      <title>Re: K82 Kinetics DAC Voltage reference</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-Kinetics-DAC-Voltage-reference/m-p/647681#M39345</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Fang Li,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your answer,&lt;/P&gt;&lt;P&gt;I thought the VREF_OUT pin is an output only, do you mean that I should connect my external reference to this pin?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Since my design only needs DAC and DAC IDDA current is 700uA I was connecting the 2.5V reference to VDDA directly.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Would you please clarify which is the preferred approach?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Apr 2017 14:23:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-Kinetics-DAC-Voltage-reference/m-p/647681#M39345</guid>
      <dc:creator>mhanuel</dc:creator>
      <dc:date>2017-04-06T14:23:11Z</dc:date>
    </item>
  </channel>
</rss>